|
MotorWare f2806x Driver API Documentation
|
Contains the various functions related to the watch dog (WDOG) object. More...
#include "sw/drivers/wdog/src/32b/f28x/f2806x/wdog.h"Go to the source code of this file.
Functions | |
| void | WDOG_clearCounter (WDOG_Handle wdogHandle) |
| Clears the watchdog (WDOG) counter. More... | |
| void | WDOG_disable (WDOG_Handle wdogHandle) |
| Disables the watchdog (WDOG) timer. More... | |
| void | WDOG_disableInt (WDOG_Handle wdogHandle) |
| Disables the watchdog (WDOG) timer interrupt. More... | |
| void | WDOG_disableOverRide (WDOG_Handle wdogHandle) |
| Disables the timer override. More... | |
| void | WDOG_enable (WDOG_Handle wdogHandle) |
| Enables the watchdog (WDOG) timer. More... | |
| void | WDOG_enableInt (WDOG_Handle wdogHandle) |
| Enables the watchdog (WDOG) timer interrupt. More... | |
| void | WDOG_enableOverRide (WDOG_Handle wdogHandle) |
| Enables the watchdog (WDOG) timer override. More... | |
| WDOG_IntStatus_e | WDOG_getIntStatus (WDOG_Handle wdogHandle) |
| Gets the watchdog (WDOG) interrupt status. More... | |
| WDOG_Handle | WDOG_init (void *pMemory, const size_t numBytes) |
| Initializes the watchdog (WDOG) object handle. More... | |
| void | WDOG_setCount (WDOG_Handle wdogHandle, const uint_least8_t count) |
| Sets the watchdog (WDOG) counter. More... | |
| void | WDOG_setPreScaler (WDOG_Handle wdogHandle, const WDOG_PreScaler_e preScaler) |
| Sets the watchdog (WDOG) timer clock prescaler. More... | |
Contains the various functions related to the watch dog (WDOG) object.
(C) Copyright 2015, Texas Instruments, Inc.
Definition in file wdog.c.
1.8.9.1