|
MotorWare f2806x Module API Documentation
|
Portable C fixed point code. These functions define the second-order filter (FILTER) module routines. More...
#include "sw/modules/filter/src/32b/filter_so.h"Go to the source code of this file.
Functions | |
| void | FILTER_SO_getDenCoeffs (FILTER_SO_Handle handle, _iq *pa1, _iq *pa2) |
| Gets the second-order filter denominator coefficients. More... | |
| void | FILTER_SO_getInitialConditions (FILTER_SO_Handle handle, _iq *px1, _iq *px2, _iq *py1, _iq *py2) |
| Gets the initial conditions of the second-order filter. More... | |
| void | FILTER_SO_getNumCoeffs (FILTER_SO_Handle handle, _iq *pb0, _iq *pb1, _iq *pb2) |
| Gets the second-order filter numerator coefficients. More... | |
| FILTER_SO_Handle | FILTER_SO_init (void *pMemory, const size_t numBytes) |
| Initializes the second-order filter. More... | |
| void | FILTER_SO_setDenCoeffs (FILTER_SO_Handle handle, const _iq a1, const _iq a2) |
| Sets the second-order filter denominator coefficients. More... | |
| void | FILTER_SO_setInitialConditions (FILTER_SO_Handle handle, const _iq x1, const _iq x2, const _iq y1, const _iq y2) |
| Sets the initial conditions of the second-order filter. More... | |
| void | FILTER_SO_setNumCoeffs (FILTER_SO_Handle handle, const _iq b0, const _iq b1, const _iq b2) |
| Sets the second-order filter numerator coefficients. More... | |
Portable C fixed point code. These functions define the second-order filter (FILTER) module routines.
(C) Copyright 2012, Texas Instruments, Inc.
Definition in file 32b/filter_so.c.
1.8.9.1