|
MotorWare f2806x Module API Documentation
|
Portable C fixed point code. These functions define the Park transform module routines. More...
#include "sw/modules/park/src/32b/park.h"Go to the source code of this file.
Functions | |
| PARK_Handle | PARK_init (void *pMemory, const size_t numBytes) |
| Initializes the Park transform module. More... | |
Portable C fixed point code. These functions define the Park transform module routines.
(C) Copyright 2011, Texas Instruments, Inc.
Definition in file 32b/park.c.
1.8.9.1