|
MotorWare f2806x Module API Documentation
|
Contains public interface to various functions related to the trajectory (TRAJ) object. More...
Go to the source code of this file.
Data Structures | |
| struct | _TRAJ_Obj_ |
| Defines the trajectory (TRAJ) object. More... | |
Typedefs | |
| typedef struct _TRAJ_Obj_ | TRAJ_Obj |
| Defines the trajectory (TRAJ) object. More... | |
| typedef struct _TRAJ_Obj_ * | TRAJ_Handle |
| Defines the TRAJ handle. More... | |
Functions | |
| static _iq | TRAJ_getIntValue (TRAJ_Handle handle) |
| Gets the intermediate value for the trajectory. More... | |
| static _iq | TRAJ_getMaxDelta (TRAJ_Handle handle) |
| Gets the maximum delta value for the trajectory. More... | |
| static _iq | TRAJ_getMaxValue (TRAJ_Handle handle) |
| Gets the maximum value for the trajectory. More... | |
| static _iq | TRAJ_getMinValue (TRAJ_Handle handle) |
| Gets the minimum value for the trajectory. More... | |
| static _iq | TRAJ_getTargetValue (TRAJ_Handle handle) |
| Gets the target value for the trajectory. More... | |
| TRAJ_Handle | TRAJ_init (void *pMemory, const size_t numBytes) |
| Initializes the trajectory (TRAJ) object. More... | |
| static void | TRAJ_setIntValue (TRAJ_Handle handle, const _iq intValue) |
| Sets the intermediate value for the trajectory. More... | |
| static void | TRAJ_setMaxDelta (TRAJ_Handle handle, const _iq maxDelta) |
| Sets the maximum delta value for the trajectory. More... | |
| static void | TRAJ_setMaxValue (TRAJ_Handle handle, const _iq maxValue) |
| Sets the maximum value for the trajectory. More... | |
| static void | TRAJ_setMinValue (TRAJ_Handle handle, const _iq minValue) |
| Sets the minimum value for the trajectory. More... | |
| static void | TRAJ_setTargetValue (TRAJ_Handle handle, const _iq targetValue) |
| Sets the target value for the trajectory. More... | |
| static void | TRAJ_run (TRAJ_Handle handle) |
| Runs the trajectory (TRAJ) object. More... | |
Contains public interface to various functions related to the trajectory (TRAJ) object.
(C) Copyright 2011, Texas Instruments, Inc.
Definition in file 32b/traj.h.
1.8.9.1