|
MotorWare f2806x Module API Documentation
|
| C_ANGLE_Obj_ | Defines the angle generator (ANGLE) object |
| C_CAL_Obj_ | Defines the calibrator (CAL) object |
| C_CLARKE_Obj_ | Defines the CLARKE object |
| C_cplx_int16_t_ | Define the complex data type for 16 bit signed real and imaginary components |
| C_cplx_int32_t | Define the complex data type for 32 bit signed real and imaginary components |
| C_cplx_int_least32_t_ | Define the complex data type for at least 32 bit signed real and imaginary components |
| C_cplx_int_least8_t | Define the complex data type for at least 8 bit signed real and imaginary components |
| C_cplx_least16_t | Define the complex data type for at least 16 bit signed real and imaginary components |
| C_cplx_uint16_t_ | Define the complex data type for 16 bit unsigned real and imaginary components |
| C_cplx_uint32_t | Define the complex data type for 32 bit unsigned real and imaginary components |
| C_cplx_uint_least32_t_ | Define the complex data type for at least 32 bit unsigned real and imaginary components |
| C_cplx_uint_least8_t | Define the complex data type for at least 8 bit unsigned real and imaginary components |
| C_cplx_uleast16_t | Define the complex data type for at least 16 bit unsigned real and imaginary components |
| C_CPU_USAGE_Obj_ | Defines the CPU usage (CPU_USAGE) object |
| C_CTRL_Obj_ | Defines the controller (CTRL) object |
| C_CTRL_Version_ | Defines the controller (CTRL) version number |
| C_DLOG_4CH_ | Defines the data logging (DLOG) object |
| C_ENC_Obj_ | Defines the encoder object |
| C_EST_InputData_ | Defines the estimator (EST) input data |
| C_EST_OutputData_ | Defines the estimator (EST) output data |
| C_EVENT_ArgList_ | Defines the event argument list |
| C_EVENT_Obj_ | Defines the event queue object |
| C_FEM_Obj_ | Defines the frequency of execution monitoring (FEM) object |
| C_FILTER_FO_ | Defines the first-order filter (FILTER_FO) object |
| C_FILTER_FO_Obj_ | Defines the first-order filter (FILTER_FO) object |
| C_FILTER_SO_ | Defines the second-order filter (FILTER_SO) object |
| C_FILTER_SO_Obj_ | Defines the second-order filter (FILTER_SO) object |
| C_FW_Obj_ | Defines the field weakening (FW) data |
| C_HAL_AdcData_t_ | Defines the ADC data |
| C_HAL_DacData_t_ | Defines the DAC data |
| C_HAL_Obj_ | Defines the hardware abstraction layer (HAL) data |
| C_HAL_PwmData_t_ | Defines the PWM data |
| C_IPARK_Obj_ | Defines the IPARK object |
| C_MATH_vec2_ | Defines a two element vector |
| C_MATH_vec3_ | Defines a three element vector |
| C_MOTOR_Params_ | Defines the motor parameters |
| C_OFFSET_ | Defines the offset (OFFSET) object |
| C_PARK_Obj_ | Defines the PARK object |
| C_PI_Obj_ | Defines the PI controller object |
| C_PID_Obj_ | Defines the PID controller object |
| C_QUEUE_Obj_ | Defines the queue object structure |
| C_SLIP_Obj_ | Defines the slip object |
| C_SVGEN_Obj_ | Defines the Space Vector Generator object |
| C_SVGENCURRENT_Obj_ | Defines the Svgen Current object |
| C_TRAJ_Obj_ | Defines the trajectory (TRAJ) object |
| C_USER_Params_ | Defines a structure for the user parameters |
| CST_PlanError_t | Defines the ST_PlanError_t data |
| CST_PosConv_t | Defines the ST_PosConv_t data |
| CST_PosConvCfg_t | Defines the ST_PosConvCfg_t data |
| CST_PosCtl_t | Defines the ST_PosCtl_t data |
| CST_PosCtlCfg_t | Defines the ST_PosCtlCfg_t data |
| CST_PosMove_t | Defines the ST_PosMove_t data |
| CST_PosMoveCfg_t | Defines the ST_PosMoveCfg_t data |
| CST_PosMoveMsg_t | Defines the ST_PosMoveMsg_t data |
| CST_PosPlan_t | Defines the ST_PosPlan_t data |
| CST_VelCtl_t | Defines the ST_VelCtl_t data |
| CST_VelCtlCfg_t | Defines the ST_VelCtlCfg_t data |
| CST_VelId_t | Defines the ST_VelId_t data |
| CST_VelIdCfg_t | Defines the ST_VelIdCfg_t data |
| CST_VelMove_t | Defines the ST_VelMove_t data |
| CST_VelMoveCfg_t | Defines the ST_VelMoveCfg_t data |
| CST_VelMoveMsg_t | Defines the ST_VelMoveMsg_t message data |
| CST_VelPlan_t | Defines the ST_VelPlan_t data |
| CST_Ver_t | Defines the version data |
1.8.9.1