MotorWare f2806x Module API Documentation
Functions
cpu_usage.c File Reference

Portable C fixed point code. These functions define the CPU usage (CPU_USAGE) module routines. More...

#include "sw/modules/cpu_usage/src/32b/cpu_usage.h"

Go to the source code of this file.

Functions

CPU_USAGE_Handle CPU_USAGE_init (void *pMemory, const size_t numBytes)
 Initializes the CPU usage (CPU_USAGE) object. More...
 
void CPU_USAGE_setParams (CPU_USAGE_Handle handle, const uint32_t timerPeriod_cnts, const uint32_t numDeltaCntsAvg)
 Sets the CPU usage module parameters. More...
 

Detailed Description

Portable C fixed point code. These functions define the CPU usage (CPU_USAGE) module routines.

(C) Copyright 2013, Texas Instruments, Inc.

Definition in file cpu_usage.c.