|
MotorWare f2806x Module API Documentation
|
#include <math.h>#include "sw/modules/dlog/src/32b/dlog4ch.h"#include "sw/modules/math/src/32b/math.h"#include "ctrlQEP.h"#include "hal.h"#include "user.h"Go to the source code of this file.
Functions | |
| void | CTRL_getGains (CTRL_Handle handle, const CTRL_Type_e ctrlType, _iq *pKp, _iq *pKi, _iq *pKd) |
| Gets the gain values for the specified controller. More... | |
| void | CTRL_getIab_filt_pu (CTRL_Handle handle, MATH_vec2 *pIab_filt_pu) |
| Gets the alpha/beta filtered current vector values from the controller. More... | |
| void | CTRL_getIab_in_pu (CTRL_Handle handle, MATH_vec2 *pIab_in_pu) |
| Gets the alpha/beta current input vector values from the controller. More... | |
| void | CTRL_getIdq_in_pu (CTRL_Handle handle, MATH_vec2 *pIdq_in_pu) |
| Gets the direct/quadrature current input vector values from the controller. More... | |
| void | CTRL_getIdq_ref_pu (CTRL_Handle handle, MATH_vec2 *pIdq_ref_pu) |
| Gets the direct/quadrature current reference vector values from the controller. More... | |
| _iq | CTRL_getMagCurrent_pu (CTRL_Handle handle) |
| Gets the magnetizing current value from the controller. More... | |
| _iq | CTRL_getMaximumSpeed_pu (CTRL_Handle handle) |
| Gets the maximum speed value from the controller. More... | |
| void | CTRL_getVab_in_pu (CTRL_Handle handle, MATH_vec2 *pVab_in_pu) |
| Gets the alpha/beta voltage input vector values from the controller. More... | |
| void | CTRL_getVab_out_pu (CTRL_Handle handle, MATH_vec2 *pVab_out_pu) |
| Gets the alpha/beta voltage output vector values from the controller. More... | |
| void | CTRL_getVdq_out_pu (CTRL_Handle handle, MATH_vec2 *pVdq_out_pu) |
| Gets the direct/quadrature voltage output vector values from the controller. More... | |
| void | CTRL_getWaitTimes (CTRL_Handle handle, uint_least32_t *pWaitTimes) |
| Gets the wait times from the estimator. More... | |
| void | CTRL_run (CTRL_Handle handle, HAL_Handle halHandle, const HAL_AdcData_t *pAdcData, HAL_PwmData_t *pPwmData, uint32_t electricalAngle) |
| Runs the controller. More... | |
| void | CTRL_setGains (CTRL_Handle handle, const CTRL_Type_e ctrlType, const _iq Kp, const _iq Ki, const _iq Kd) |
| Sets the gain values for the specified controller. More... | |
| void | CTRL_setMagCurrent_pu (CTRL_Handle handle, const _iq magCurrent_pu) |
| Sets the magnetizing current value in the controller. More... | |
| void | CTRL_setMaximumSpeed_pu (CTRL_Handle handle, const _iq maxSpeed_pu) |
| Sets the maximum speed value in the controller. More... | |
| void | CTRL_setParams (CTRL_Handle handle, USER_Params *pUserParams) |
| Sets the controller parameters. More... | |
| void | CTRL_setSpd_ref_pu (CTRL_Handle handle, const _iq spd_ref_pu) |
| Sets the output speed reference value in the controller. More... | |
| void | CTRL_setSpd_ref_krpm (CTRL_Handle handle, const _iq spd_ref_krpm) |
| Sets the output speed reference value in the controller. More... | |
| void | CTRL_setup (CTRL_Handle handle) |
| Sets up the controller (CTRL) object and all of the subordinate objects. More... | |
| void | CTRL_setupClarke_I (CTRL_Handle handle, uint_least8_t numCurrentSensors) |
| Sets the number of current sensors. More... | |
| void | CTRL_setupClarke_V (CTRL_Handle handle, uint_least8_t numVoltageSensors) |
| Sets the number of voltage sensors. More... | |
| void | CTRL_setWaitTimes (CTRL_Handle handle, const uint_least32_t *pWaitTimes) |
| Sets the wait times for the controller states. More... | |
| bool | CTRL_updateState (CTRL_Handle handle) |
| Updates the controller state. More... | |
1.8.9.1