|
MotorWare f2806x Module API Documentation
|
Files | |
| file | 32b/svgen.c [code] |
| Portable C fixed point code. These functions define the Space Vector Generator (SVGEN) module routines. | |
| file | 32b/svgen.h [code] |
| Contains the public interface to the Space Vector Generator (SVGEN) module routines. | |
| file | svgen_current.c [code] |
| Contains the various functions related to the svgen current object. | |
| file | svgen_current.h [code] |
| Contains the public interface to the Svgen Current module routines. | |
1.8.9.1