|
MotorWare f2806x Module API Documentation
|
Directories | |
| directory | 32b |
| directory | float |
Files | |
| file | est_Flux_states.h [code] |
| Contains the states for the flux estimator (EST_Flux) module routines. | |
| file | est_Ls_states.h [code] |
| Contains the states for the stator inductance estimator (EST_Ls) module routines. | |
| file | est_Rr_states.h [code] |
| Contains the public interface to the rotor resistance estimator (EST_Rr) module routines. | |
| file | est_Rs_states.h [code] |
| Contains the public interface to the stator resistance estimator (EST_Rs) module routines. | |
| file | est_states.h [code] |
| Contains the states for the estimator (EST) module routines. | |
| file | est_Traj_states.h [code] |
| Contains the states for the flux estimator (EST_Flux) module routines. | |
1.8.9.1