|
MotorWare f2806x Module API Documentation
|
Files | |
| file | 32b/filter_fo.c [code] |
| Portable C fixed point code. These functions define the first-order filter (FILTER) module routines. | |
| file | 32b/filter_fo.h [code] |
| Contains the public interface to the first-order filter (FILTER_FO) module routines. | |
| file | 32b/filter_so.c [code] |
| Portable C fixed point code. These functions define the second-order filter (FILTER) module routines. | |
| file | 32b/filter_so.h [code] |
| Contains the public interface to the second-order filter (FILTER_SO) module routines. | |
1.8.9.1