|
MotorWare f2806x Module API Documentation
|
Contains the states for the flux estimator (EST_Flux) module routines. More...
Go to the source code of this file.
Enumerations | |
| enum | EST_Flux_ErrorCode_e { EST_Flux_ErrorCode_NoError =0, EST_Flux_ErrorCode_ShiftOverFlow, EST_Flux_ErrorCode_Clip, EST_Flux_numErrorCodes } |
| Enumeration for the estimator error codes. More... | |
| enum | EST_Flux_State_e { EST_Flux_State_Error =0, EST_Flux_State_Idle, EST_Flux_State_CL1, EST_Flux_State_CL2, EST_Flux_State_Fine, EST_Flux_State_Done, EST_Flux_numStates } |
| Enumeration for the estimator states. More... | |
Contains the states for the flux estimator (EST_Flux) module routines.
(C) Copyright 2012, Texas Instruments, Inc.
Definition in file est_Flux_states.h.
1.8.9.1