1 #ifndef _EST_FLUX_STATES_H_
2 #define _EST_FLUX_STATES_H_
71 #endif // end of _EST_FLUX_STATES_H_ definition
flux shift overflow error code
EST_Flux_State_e
Enumeration for the estimator states.
closed loop control stage 2
EST_Flux_ErrorCode_e
Enumeration for the estimator error codes.
the number of estimator error codes
closed loop control stage 1
the number of flux estimator states