|
MotorWare f2806x Module API Documentation
|
Contains the public interface to the second-order filter (FILTER_SO) module routines. More...
#include "sw/modules/types/src/types.h"Go to the source code of this file.
Data Structures | |
| struct | _FILTER_SO_Obj_ |
| Defines the second-order filter (FILTER_SO) object. More... | |
Typedefs | |
| typedef struct _FILTER_SO_Obj_ | FILTER_SO_Obj |
| Defines the second-order filter (FILTER_SO) object. More... | |
| typedef struct _FILTER_SO_Obj_ * | FILTER_SO_Handle |
| Defines the second-order filter (FILTER_SO) handle. More... | |
Functions | |
| static float_t | FILTER_SO_get_a1 (FILTER_SO_Handle handle) |
| Gets the second-order filter denominator coefficient a1. More... | |
| static float_t | FILTER_SO_get_a2 (FILTER_SO_Handle handle) |
| Gets the second-order filter denominator coefficient a2. More... | |
| static float_t | FILTER_SO_get_b0 (FILTER_SO_Handle handle) |
| Gets the second-order filter numerator coefficient b0. More... | |
| static float_t | FILTER_SO_get_b1 (FILTER_SO_Handle handle) |
| Gets the second-order filter numerator coefficient b1. More... | |
| static float_t | FILTER_SO_get_b2 (FILTER_SO_Handle handle) |
| Gets the second-order filter numerator coefficient b2. More... | |
| static float_t | FILTER_SO_get_x1 (FILTER_SO_Handle handle) |
| Gets the second-order filter input value at time sample n=-1. More... | |
| static float_t | FILTER_SO_get_x2 (FILTER_SO_Handle handle) |
| Gets the second-order filter input value at time sample n=-2. More... | |
| static float_t | FILTER_SO_get_y1 (FILTER_SO_Handle handle) |
| Gets the second-order filter output value at time sample n=-1. More... | |
| static float_t | FILTER_SO_get_y2 (FILTER_SO_Handle handle) |
| Gets the second-order filter output value at time sample n=-2. More... | |
| void | FILTER_SO_getDenCoeffs (FILTER_SO_Handle handle, float_t *pa1, float_t *pa2) |
| Gets the second-order filter denominator coefficients. More... | |
| void | FILTER_SO_getInitialConditions (FILTER_SO_Handle handle, float_t *px1, float_t *px2, float_t *py1, float_t *py2) |
| Gets the initial conditions of the second-order filter. More... | |
| void | FILTER_SO_getNumCoeffs (FILTER_SO_Handle handle, float_t *pb0, float_t *pb1, float_t *pb2) |
| Gets the second-order filter numerator coefficients. More... | |
| FILTER_SO_Handle | FILTER_SO_init (void *pMemory, const size_t numBytes) |
| Initializes the second-order filter. More... | |
| static float_t | FILTER_SO_run (FILTER_SO_Handle handle, const float_t inputValue) |
| Runs a second-order filter of the form y[n] = b0*x[n] + b1*x[n-1] + b2*x[n-2] - a1*y[n-1] - a2*y[n-2]. More... | |
| static float_t | FILTER_SO_run_form_0 (FILTER_SO_Handle handle, const float_t inputValue) |
| Runs a simplified second-order filter of the form y[n] = b0*x[n] - a1*y[n-1] - a2*y[n-2]. More... | |
| static float_t | FILTER_SO_run_form_1 (FILTER_SO_Handle handle, const float_t inputValue) |
| Runs a second-order filter of the form y[n] = b0*x[n] + b1*x[n-1] - a1*y[n-1] - a2*y[n-2]. More... | |
| static void | FILTER_SO_set_a1 (FILTER_SO_Handle handle, const float_t a1) |
| Sets the second-order filter denominator coefficient a1. More... | |
| static void | FILTER_SO_set_a2 (FILTER_SO_Handle handle, const float_t a2) |
| Sets the second-order filter denominator coefficient a2. More... | |
| static void | FILTER_SO_set_b0 (FILTER_SO_Handle handle, const float_t b0) |
| Sets the second-order filter numerator coefficient b0. More... | |
| static void | FILTER_SO_set_b1 (FILTER_SO_Handle handle, const float_t b1) |
| Sets the second-order filter numerator coefficient b1. More... | |
| static void | FILTER_SO_set_b2 (FILTER_SO_Handle handle, const float_t b2) |
| Sets the second-order filter numerator coefficient b2. More... | |
| static void | FILTER_SO_set_x1 (FILTER_SO_Handle handle, const float_t x1) |
| Sets the second-order filter input value at time sample n=-1. More... | |
| static void | FILTER_SO_set_x2 (FILTER_SO_Handle handle, const float_t x2) |
| Sets the second-order filter input value at time sample n=-2. More... | |
| static void | FILTER_SO_set_y1 (FILTER_SO_Handle handle, const float_t y1) |
| Sets the second-order filter output value at time sample n=-1. More... | |
| static void | FILTER_SO_set_y2 (FILTER_SO_Handle handle, const float_t y2) |
| Sets the second-order filter output value at time sample n=-2. More... | |
| void | FILTER_SO_setDenCoeffs (FILTER_SO_Handle handle, const float_t a1, const float_t a2) |
| Sets the second-order filter denominator coefficients. More... | |
| void | FILTER_SO_setInitialConditions (FILTER_SO_Handle handle, const float_t x1, const float_t x2, const float_t y1, const float_t y2) |
| Sets the initial conditions of the second-order filter. More... | |
| void | FILTER_SO_setNumCoeffs (FILTER_SO_Handle handle, const float_t b0, const float_t b1, const float_t b2) |
| Sets the second-order filter numerator coefficients. More... | |
Contains the public interface to the second-order filter (FILTER_SO) module routines.
(C) Copyright 2014, Texas Instruments, Inc.
Definition in file float/filter_so.h.
|
inlinestatic |
Gets the second-order filter denominator coefficient a1.
| [in] | handle | The filter handle |
Definition at line 105 of file float/filter_so.h.
References _FILTER_SO_::a1.
|
inlinestatic |
Gets the second-order filter denominator coefficient a2.
| [in] | handle | The filter handle |
Definition at line 116 of file float/filter_so.h.
References _FILTER_SO_::a2.
|
inlinestatic |
Gets the second-order filter numerator coefficient b0.
| [in] | handle | The filter handle |
Definition at line 127 of file float/filter_so.h.
References _FILTER_SO_::b0.
|
inlinestatic |
Gets the second-order filter numerator coefficient b1.
| [in] | handle | The filter handle |
Definition at line 138 of file float/filter_so.h.
References _FILTER_SO_::b1.
|
inlinestatic |
Gets the second-order filter numerator coefficient b2.
| [in] | handle | The filter handle |
Definition at line 149 of file float/filter_so.h.
References _FILTER_SO_::b2.
|
inlinestatic |
Gets the second-order filter input value at time sample n=-1.
| [in] | handle | The filter handle |
Definition at line 160 of file float/filter_so.h.
References _FILTER_SO_::x1.
|
inlinestatic |
Gets the second-order filter input value at time sample n=-2.
| [in] | handle | The filter handle |
Definition at line 171 of file float/filter_so.h.
References _FILTER_SO_::x2.
|
inlinestatic |
Gets the second-order filter output value at time sample n=-1.
| [in] | handle | The filter handle |
Definition at line 182 of file float/filter_so.h.
References _FILTER_SO_::y1.
|
inlinestatic |
Gets the second-order filter output value at time sample n=-2.
| [in] | handle | The filter handle |
Definition at line 193 of file float/filter_so.h.
References _FILTER_SO_::y2.
1.8.9.1