MotorWare f2806x Module API Documentation
Data Structures | Typedefs | Enumerations
float/motor.h File Reference
#include "sw/modules/types/src/types.h"

Go to the source code of this file.

Data Structures

struct  _MOTOR_Params_
 Defines the motor parameters. More...
 

Typedefs

typedef struct _MOTOR_Params_ MOTOR_Params
 Defines the motor parameters. More...
 

Enumerations

enum  MOTOR_Type_e { MOTOR_Type_Induction =0, MOTOR_Type_Pm, MOTOR_Type_Induction =0, MOTOR_Type_Pm }
 Enumeration for the motor types. More...