|
MotorWare f2806x Module API Documentation
|
Portable C fixed point code. These functions define the offset (OFFSET) module routines. More...
#include "sw/modules/offset/src/float/offset.h"Go to the source code of this file.
Functions | |
| float_t | OFFSET_getBeta (OFFSET_Handle handle) |
| Gets the beta offset filter coefficient. More... | |
| OFFSET_Handle | OFFSET_init (void *pMemory, const size_t numBytes) |
| Initializes the offset. More... | |
| void | OFFSET_setBeta (OFFSET_Handle handle, const float_t beta_rad) |
| Sets the beta offset filter coefficient. More... | |
| void | OFFSET_setInitCond (OFFSET_Handle handle, const float_t initCond) |
| Set the initial condition of the integrator or the value of y[n-1]. More... | |
| void | OFFSET_setOffset (OFFSET_Handle handle, float_t offsetValue) |
| Sets the offset value. More... | |
Portable C fixed point code. These functions define the offset (OFFSET) module routines.
(C) Copyright 2014, Texas Instruments, Inc.
Definition in file float/offset.c.
1.8.9.1