|
MotorWare f2806x Module API Documentation
|
Contains the public interface to the Proportional-Integral-Derivative (PID) controller module routines. More...
#include "sw/modules/types/src/types.h"#include "sw/modules/filter/src/float/filter_fo.h"#include "sw/modules/math/src/float/math.h"Go to the source code of this file.
Data Structures | |
| struct | _PID_Obj_ |
| Defines the PID controller object. More... | |
Typedefs | |
| typedef struct _PID_Obj_ | PID_Obj |
| Defines the PID controller object. More... | |
| typedef struct _PID_Obj_ * | PID_Handle |
| Defines the PID handle. More... | |
Functions | |
| void | PID_getDerFilterParams (PID_Handle handle, float_t *b0, float_t *b1, float_t *a1, float_t *x1, float_t *y1) |
| Gets the derivative filter parameters. More... | |
| static float_t | PID_getFbackValue (PID_Handle handle) |
| Gets the feedback value in the PID controller. More... | |
| static float_t | PID_getFfwdValue (PID_Handle handle) |
| Gets the feedforward value in the PID controller. More... | |
| static void | PID_getGains (PID_Handle handle, float_t *pKp, float_t *pKi, float_t *pKd) |
| Gets the gains in the PID controller. More... | |
| static float_t | PID_getKd (PID_Handle handle) |
| Gets the derivative gain in the PID controller. More... | |
| static float_t | PID_getKi (PID_Handle handle) |
| Gets the integral gain in the PID controller. More... | |
| static float_t | PID_getKp (PID_Handle handle) |
| Gets the proportional gain in the PID controller. More... | |
| static void | PID_getMinMax (PID_Handle handle, float_t *pOutMin, float_t *pOutMax) |
| Gets the minimum and maximum output value allowed in the PID controller. More... | |
| static float_t | PID_getOutMax (PID_Handle handle) |
| Gets the maximum output value allowed in the PID controller. More... | |
| static float_t | PID_getOutMin (PID_Handle handle) |
| Gets the minimum output value allowed in the PID controller. More... | |
| static float_t | PID_getRefValue (PID_Handle handle) |
| Gets the reference value in the PID controller. More... | |
| static float_t | PID_getUi (PID_Handle handle) |
| Gets the integrator start value in the PID controller. More... | |
| PID_Handle | PID_init (void *pMemory, const size_t numBytes) |
| Initializes the PID controller. More... | |
| void | PID_setDerFilterParams (PID_Handle handle, const float_t b0, const float_t b1, const float_t a1, const float_t x1, const float_t y1) |
| Sets the derivative filter parameters. More... | |
| static void | PID_setFbackValue (PID_Handle handle, const float_t fbackValue) |
| Sets the feedback value in the PID controller. More... | |
| static void | PID_setFfwdValue (PID_Handle handle, const float_t ffwdValue) |
| Sets the feedforward value in the PID controller. More... | |
| static void | PID_setGains (PID_Handle handle, const float_t Kp, const float_t Ki, const float_t Kd) |
| Sets the gains in the PID controller. More... | |
| static void | PID_setKd (PID_Handle handle, const float_t Kd) |
| Sets the derivative gain in the PID controller. More... | |
| static void | PID_setKi (PID_Handle handle, const float_t Ki) |
| Sets the integral gain in the PID controller. More... | |
| static void | PID_setKp (PID_Handle handle, const float_t Kp) |
| Sets the proportional gain in the PID controller. More... | |
| static void | PID_setMinMax (PID_Handle handle, const float_t outMin, const float_t outMax) |
| Sets the minimum and maximum output value allowed in the PID controller. More... | |
| static void | PID_setOutMax (PID_Handle handle, const float_t outMax) |
| Sets the maximum output value allowed in the PID controller. More... | |
| static void | PID_setOutMin (PID_Handle handle, const float_t outMin) |
| Sets the minimum output value allowed in the PID controller. More... | |
| static void | PID_setRefValue (PID_Handle handle, const float_t refValue) |
| Sets the reference value in the PID controller. More... | |
| static void | PID_setUi (PID_Handle handle, const float_t Ui) |
| Sets the integrator start value in the PID controller. More... | |
| static void | PID_run_parallel (PID_Handle handle, const float_t refValue, const float_t fbackValue, const float_t ffwdValue, float_t *pOutValue) |
| Runs the parallel form of the PID controller. More... | |
| static void | PID_run_series (PID_Handle handle, const float_t refValue, const float_t fbackValue, const float_t ffwdValue, float_t *pOutValue) |
| Runs the series form of the PID controller. More... | |
Contains the public interface to the Proportional-Integral-Derivative (PID) controller module routines.
(C) Copyright 2014, Texas Instruments, Inc.
Definition in file float/pid.h.
|
inlinestatic |
Gets the feedback value in the PID controller.
| [in] | handle | The PID controller handle |
Definition at line 121 of file float/pid.h.
References _PID_Obj_::fbackValue.
|
inlinestatic |
Gets the derivative gain in the PID controller.
| [in] | handle | The PID controller handle |
Definition at line 160 of file float/pid.h.
References _PID_Obj_::Kd.
Referenced by PID_run_parallel(), and PID_run_series().
|
inlinestatic |
Gets the integral gain in the PID controller.
| [in] | handle | The PID controller handle |
Definition at line 171 of file float/pid.h.
References _PID_Obj_::Ki.
Referenced by PID_run_parallel(), and PID_run_series().
|
inlinestatic |
Gets the proportional gain in the PID controller.
| [in] | handle | The PID controller handle |
Definition at line 182 of file float/pid.h.
References _PID_Obj_::Kp.
Referenced by PID_run_parallel(), and PID_run_series().
|
inlinestatic |
Gets the maximum output value allowed in the PID controller.
| [in] | handle | The PID controller handle |
Definition at line 208 of file float/pid.h.
References _PID_Obj_::outMax.
Referenced by PID_run_parallel(), and PID_run_series().
|
inlinestatic |
Gets the minimum output value allowed in the PID controller.
| [in] | handle | The PID controller handle |
Definition at line 219 of file float/pid.h.
References _PID_Obj_::outMin.
Referenced by PID_run_parallel(), and PID_run_series().
|
inlinestatic |
Gets the reference value in the PID controller.
| [in] | handle | The PID controller handle |
Definition at line 230 of file float/pid.h.
References _PID_Obj_::refValue.
|
inlinestatic |
Gets the integrator start value in the PID controller.
| [in] | handle | The PID controller handle |
Definition at line 241 of file float/pid.h.
References _PID_Obj_::Ui.
Referenced by PID_run_parallel(), and PID_run_series().
1.8.9.1