49 #ifdef __TMS320C28XX_CLA__
50 #pragma CODE_SECTION(SVGEN_init,"Cla1Prog2");
67 if((int16_t)numBytes < (int16_t)
sizeof(
SVGEN_Obj))
Contains the public interface to the Space Vector Generator (SVGEN) module routines.
Defines the Space Vector Generator object.
struct _SVGEN_Obj_ * SVGEN_Handle
Defines the SVGEN handle.
SVGEN_Handle SVGEN_init(void *pMemory, const size_t numBytes)
Initializes the space vector generator module.