|
MotorWare f2806x Module API Documentation
|
Portable C fixed point code. These functions define the field weakening module routines. More...
#include "sw/modules/fw/src/32b/fw.h"Go to the source code of this file.
Functions | |
| FW_Handle | FW_init (void *pMemory, const size_t numBytes) |
| Initializes the field weakening (FW) object. More... | |
Portable C fixed point code. These functions define the field weakening module routines.
(C) Copyright 2011, Texas Instruments, Inc.
Definition in file fw.c.
1.8.9.1