MotorWare f2806x Module API Documentation
Macros | Enumerations | Functions
hvkit_rev1p1/f28x/f2806x/src/float/hal.h File Reference
#include "hal_obj.h"

Go to the source code of this file.

Macros

#define Device_cal   (void (*)(void))0x3D7C80
 
#define FP_SCALE   32768
 Defines used in oscillator calibration functions. More...
 
#define FP_ROUND   FP_SCALE/2
 Defines the quantity added to Q15 numbers before converting to integer to round the number. More...
 
#define OSC_POSTRIM   32
 Defines the amount to add to Q16.15 fixed point number to shift from a fine trim range of. More...
 
#define OSC_POSTRIM_OFF   FP_SCALE*OSC_POSTRIM
 
#define getOsc1FineTrimSlope()   (*(int16_t (*)(void))0x3D7E90)()
 The following functions return reference values stored in OTP. More...
 
#define getOsc1FineTrimOffset()   (*(int16_t (*)(void))0x3D7E93)()
 Defines the oscillator 1 fine trim at high temp. More...
 
#define getOsc1CoarseTrim()   (*(int16_t (*)(void))0x3D7E96)()
 Defines the oscillator 1 coarse trim. More...
 
#define getOsc2FineTrimSlope()   (*(int16_t (*)(void))0x3D7E99)()
 Defines the slope used to compensate oscillator 2 (fine trim steps / ADC code). Stored. More...
 
#define getOsc2FineTrimOffset()   (*(int16_t (*)(void))0x3D7E9C)()
 Defines the oscillator 2 fine trim at high temp. More...
 
#define getOsc2CoarseTrim()   (*(int16_t (*)(void))0x3D7E9F)()
 Defines the oscillator 2 coarse trim. More...
 
#define getRefTempOffset()   (*(int16_t (*)(void))0x3D7EA2)()
 Defines the ADC reading of temperature sensor at reference temperature for compensation. More...
 
#define HAL_PWM_DBFED_CNT   (uint16_t)(2.0 * (float_t)USER_SYSTEM_FREQ_MHz)
 Defines the PWM deadband falling edge delay count (system clocks) More...
 
#define HAL_PWM_DBRED_CNT   (uint16_t)(2.0 * (float_t)USER_SYSTEM_FREQ_MHz)
 Defines the PWM deadband rising edge delay count (system clocks) More...
 
#define HAL_readSW   HAL_readGpio
 Defines the function to read pushbuttons. More...
 
#define HAL_turnLedOff   HAL_setGpioLow
 Defines the function to turn LEDs off. More...
 
#define HAL_turnLedOn   HAL_setGpioHigh
 Defines the function to turn LEDs on. More...
 
#define HAL_toggleLed   HAL_toggleGpio
 Defines the function to turn LEDs on. More...
 

Enumerations

enum  HAL_LedNumber_e {
  HAL_Gpio_LED2 =GPIO_Number_34, HAL_Gpio_LED3 =GPIO_Number_39, HAL_Gpio_LED2 =GPIO_Number_34, HAL_Gpio_LED3 =GPIO_Number_39,
  HAL_Gpio_LED2 =GPIO_Number_31, HAL_Gpio_LED3 =GPIO_Number_34, HAL_Gpio_LED2 =GPIO_Number_31, HAL_Gpio_LED3 =GPIO_Number_34,
  HAL_Gpio_LED2 =GPIO_Number_31, HAL_Gpio_LED3 =GPIO_Number_34, HAL_Gpio_LED2 =GPIO_Number_31, HAL_Gpio_LED3 =GPIO_Number_34,
  HAL_Gpio_LED2 =GPIO_Number_31, HAL_Gpio_LED3 =GPIO_Number_34, HAL_Gpio_LED2 =GPIO_Number_31, HAL_Gpio_LED3 =GPIO_Number_34
}
 Enumeration for the LED numbers. More...
 
enum  HAL_PwmFreq_e {
  HAL_PwmFreq_2_kHz = 22500, HAL_PwmFreq_3_kHz = 15000, HAL_PwmFreq_4_kHz = 11250, HAL_PwmFreq_5_kHz = 9000,
  HAL_PwmFreq_6_kHz = 7500, HAL_PwmFreq_8_kHz = 5625, HAL_PwmFreq_9_kHz = 5000, HAL_PwmFreq_10_kHz = 4500,
  HAL_PwmFreq_12_kHz = 3750, HAL_PwmFreq_15_kHz = 3000, HAL_PwmFreq_18_kHz = 2500, HAL_PwmFreq_20_kHz = 2250,
  HAL_PwmFreq_24_kHz = 1875, HAL_PwmFreq_25_kHz = 1800, HAL_PwmFreq_30_kHz = 1500, HAL_PwmFreq_36_kHz = 1250,
  HAL_PwmFreq_40_kHz = 1125, HAL_PwmFreq_45_kHz = 1000, HAL_PwmFreq_50_kHz = 900, HAL_PwmFreq_60_kHz = 750,
  HAL_PwmFreq_75_kHz = 600, HAL_PwmFreq_90_kHz = 500, HAL_PwmFreq_100_kHz = 450, HAL_PwmFreq_120_kHz = 375,
  HAL_PwmFreq_125_kHz = 360, HAL_PwmFreq_150_kHz = 300, HAL_PwmFreq_2_kHz = 22500, HAL_PwmFreq_3_kHz = 15000,
  HAL_PwmFreq_4_kHz = 11250, HAL_PwmFreq_5_kHz = 9000, HAL_PwmFreq_6_kHz = 7500, HAL_PwmFreq_8_kHz = 5625,
  HAL_PwmFreq_9_kHz = 5000, HAL_PwmFreq_10_kHz = 4500, HAL_PwmFreq_12_kHz = 3750, HAL_PwmFreq_15_kHz = 3000,
  HAL_PwmFreq_18_kHz = 2500, HAL_PwmFreq_20_kHz = 2250, HAL_PwmFreq_24_kHz = 1875, HAL_PwmFreq_25_kHz = 1800,
  HAL_PwmFreq_30_kHz = 1500, HAL_PwmFreq_36_kHz = 1250, HAL_PwmFreq_40_kHz = 1125, HAL_PwmFreq_45_kHz = 1000,
  HAL_PwmFreq_50_kHz = 900, HAL_PwmFreq_60_kHz = 750, HAL_PwmFreq_75_kHz = 600, HAL_PwmFreq_90_kHz = 500,
  HAL_PwmFreq_100_kHz = 450, HAL_PwmFreq_120_kHz = 375, HAL_PwmFreq_125_kHz = 360, HAL_PwmFreq_150_kHz = 300,
  HAL_PwmFreq_2_kHz = 22500, HAL_PwmFreq_3_kHz = 15000, HAL_PwmFreq_4_kHz = 11250, HAL_PwmFreq_5_kHz = 9000,
  HAL_PwmFreq_6_kHz = 7500, HAL_PwmFreq_8_kHz = 5625, HAL_PwmFreq_9_kHz = 5000, HAL_PwmFreq_10_kHz = 4500,
  HAL_PwmFreq_12_kHz = 3750, HAL_PwmFreq_15_kHz = 3000, HAL_PwmFreq_18_kHz = 2500, HAL_PwmFreq_20_kHz = 2250,
  HAL_PwmFreq_24_kHz = 1875, HAL_PwmFreq_25_kHz = 1800, HAL_PwmFreq_30_kHz = 1500, HAL_PwmFreq_36_kHz = 1250,
  HAL_PwmFreq_40_kHz = 1125, HAL_PwmFreq_45_kHz = 1000, HAL_PwmFreq_50_kHz = 900, HAL_PwmFreq_60_kHz = 750,
  HAL_PwmFreq_75_kHz = 600, HAL_PwmFreq_90_kHz = 500, HAL_PwmFreq_100_kHz = 450, HAL_PwmFreq_120_kHz = 375,
  HAL_PwmFreq_125_kHz = 360, HAL_PwmFreq_150_kHz = 300
}
 Enumeration for the PWM frequencies. More...
 
enum  HAL_SensorType_e {
  HAL_SensorType_Current =0, HAL_SensorType_Voltage, HAL_SensorType_Current =0, HAL_SensorType_Voltage,
  HAL_SensorType_Current =0, HAL_SensorType_Voltage, HAL_SensorType_Current =0, HAL_SensorType_Voltage,
  HAL_SensorType_Current =0, HAL_SensorType_Voltage, HAL_SensorType_Current =0, HAL_SensorType_Voltage,
  HAL_SensorType_Current =0, HAL_SensorType_Voltage, HAL_SensorType_Current =0, HAL_SensorType_Voltage
}
 Enumeration for the sensor types. More...
 

Functions

interrupt void led2ISR (void)
 
interrupt void led3OffISR (void)
 
interrupt void led3OnISR (void)
 
interrupt void mainISR (void)
 
void HAL_AdcCalChanSelect (HAL_Handle handle, const ADC_SocChanNumber_e chanNumber)
 Selects the analog channel used for calibration. More...
 
uint16_t HAL_AdcCalConversion (HAL_Handle handle)
 Reads the converted value from the selected calibration channel. More...
 
void HAL_AdcOffsetSelfCal (HAL_Handle handle)
 Executes the offset calibration of the ADC. More...
 
static void HAL_acqAdcInt (HAL_Handle handle, const ADC_IntNumber_e intNumber)
 Acknowledges an interrupt from the ADC so that another ADC interrupt can happen again. More...
 
static void HAL_acqPwmInt (HAL_Handle handle, const PWM_Number_e pwmNumber)
 Acknowledges an interrupt from the PWM so that another PWM interrupt can happen again. More...
 
void HAL_cal (HAL_Handle handle)
 Executes calibration routines. More...
 
void HAL_disableGlobalInts (HAL_Handle handle)
 Disables global interrupts. More...
 
static void HAL_disablePwm (HAL_Handle handle)
 Disables the PWM device. More...
 
static void HAL_disableTbClockSync (HAL_Handle handle)
 Disables the ePWM module time base clock sync signal. More...
 
void HAL_enableAdcInts (HAL_Handle handle)
 Enables the ADC interrupts. More...
 
void HAL_enableDebugInt (HAL_Handle handle)
 Enables the debug interrupt. More...
 
void HAL_enableGlobalInts (HAL_Handle handle)
 Enables global interrupts. More...
 
static void HAL_enablePwm (HAL_Handle handle)
 Enables the PWM devices. More...
 
void HAL_enablePwmInt (HAL_Handle handle)
 Enables the PWM interrupt. More...
 
static void HAL_enableTbClockSync (HAL_Handle handle)
 Enables the ePWM module time base clock sync signal. More...
 
static ADC_SocSampleDelay_e HAL_getAdcSocSampleDelay (HAL_Handle handle, const ADC_SocNumber_e socNumber)
 Gets the ADC delay value. More...
 
static float_t HAL_getBias (HAL_Handle handle, const HAL_SensorType_e sensorType, uint_least8_t sensorNumber)
 Gets the ADC bias value. More...
 
static float_t HAL_getCurrentScaleFactor (HAL_Handle handle)
 Gets the current scale factor. More...
 
static void HAL_getDutyCycles (HAL_Handle handle, uint16_t *pDutyCycles)
 Gets the PWM duty cycle times. More...
 
static uint_least8_t HAL_getNumCurrentSensors (HAL_Handle handle)
 Gets the number of current sensors. More...
 
static uint_least8_t HAL_getNumVoltageSensors (HAL_Handle handle)
 Gets the number of voltage sensors. More...
 
static float_t HAL_getVoltageScaleFactor (HAL_Handle handle)
 Gets the voltage scale factor. More...
 
void HAL_setupFaults (HAL_Handle handle)
 Configures the fault protection logic. More...
 
HAL_Handle HAL_init (void *pMemory, const size_t numBytes)
 Initializes the hardware abstraction layer (HAL) object. More...
 
void HAL_OscTempComp (HAL_Handle handle)
 Executes the oscillator 1 and 2 calibration functions. More...
 
void HAL_osc1Comp (HAL_Handle handle, const int16_t sensorSample)
 Executes the oscillator 1 calibration based on input sample. More...
 
void HAL_osc2Comp (HAL_Handle handle, const int16_t sensorSample)
 Executes the oscillator 2 calibration based on input sample. More...
 
uint16_t HAL_computeOscTrimValue (int16_t coarse, int16_t fine)
 
static void HAL_initIntVectorTable (HAL_Handle handle)
 Initializes the interrupt vector table. More...
 
static void HAL_readAdcData (HAL_Handle handle, HAL_AdcData_t *pAdcData)
 Reads the ADC data. More...
 
static void HAL_readAdcDataWithOffsets (HAL_Handle handle, HAL_AdcData_t *pAdcData)
 
static uint32_t HAL_readTimerCnt (HAL_Handle handle, const uint_least8_t timerNumber)
 Reads the timer count. More...
 
static void HAL_resetPwmCount (HAL_Handle handle, PWM_Number_e pwmNumber)
 Resets the PWM count. More...
 
static void HAL_setAdcSocSampleDelay (HAL_Handle handle, const ADC_SocNumber_e socNumber, const ADC_SocSampleDelay_e sampleDelay)
 Sets the ADC SOC sample delay value. More...
 
static void HAL_setBias (HAL_Handle handle, const HAL_SensorType_e sensorType, uint_least8_t sensorNumber, const float_t bias)
 Sets the ADC bias value. More...
 
static void HAL_setCurrentScaleFactor (HAL_Handle handle, const float_t current_sf)
 Sets the current scale factor in the hal. More...
 
static void HAL_setGpioHigh (HAL_Handle handle, const GPIO_Number_e gpioNumber)
 Sets the GPIO pin high. More...
 
static void HAL_setGpioLow (HAL_Handle handle, const GPIO_Number_e gpioNumber)
 Sets the GPIO pin low. More...
 
static void HAL_setNumCurrentSensors (HAL_Handle handle, const uint_least8_t numCurrentSensors)
 Sets the number of current sensors. More...
 
static void HAL_setNumVoltageSensors (HAL_Handle handle, const uint_least8_t numVoltageSensors)
 Sets the number of voltage sensors. More...
 
static void HAL_setPwmFreq_kHz (HAL_Handle handle, PWM_Number_e pwmNumber, HAL_PwmFreq_e pwmFreq_kHz)
 Sets the PWM frequency. More...
 
static void HAL_setVoltageScaleFactor (HAL_Handle handle, const float_t voltage_sf)
 Sets the voltage scale factor in the hal. More...
 
void HAL_setParams (HAL_Handle handle, const USER_Params *pUserParams)
 Sets the hardware abstraction layer parameters. More...
 
void HAL_setupAdcs (HAL_Handle handle)
 Sets up the ADCs (Analog to Digital Converters) More...
 
void HAL_setupClks (HAL_Handle handle)
 Sets up the clocks. More...
 
void HAL_setupGpios (HAL_Handle handle)
 Sets up the GPIO (General Purpose I/O) pins. More...
 
void HAL_setupFlash (HAL_Handle handle)
 Sets up the FLASH. More...
 
void HAL_setupPeripheralClks (HAL_Handle handle)
 Sets up the peripheral clocks. More...
 
void HAL_setupPie (HAL_Handle handle)
 Sets up the PIE (Peripheral Interrupt Expansion) More...
 
void HAL_setupPll (HAL_Handle handle, const PLL_ClkFreq_e clkFreq)
 Sets up the PLL (Phase Lock Loop) More...
 
void HAL_setupPwms (HAL_Handle handle, const float_t systemFreq_MHz, const float_t pwmPeriod_usec, const uint_least16_t numPwmTicksPerIsrTick)
 Sets up the PWMs (Pulse Width Modulators) More...
 
void HAL_setupPwmDacs (HAL_Handle handle, const float_t systemFreq_MHz, const float_t dacFreq_kHz)
 Sets up the PWM DACs (Pulse Width Modulator Digital to Analof Converters) More...
 
void HAL_setupTimers (HAL_Handle handle, const float_t systemFreq_MHz)
 Sets up the timers. More...
 
static void HAL_toggleGpio (HAL_Handle handle, const GPIO_Number_e gpioNumber)
 Toggles the GPIO pin. More...
 
static void HAL_updateAdcBias (HAL_Handle handle, OFFSET_Handle *pOffsetHandle_I, OFFSET_Handle *pOffsetHandle_V)
 Updates the ADC bias values. More...
 
static void HAL_writeDacData (HAL_Handle handle, const HAL_DacData_t *pDacData)
 Writes DAC data to the PWM comparators for DAC (digital-to-analog conversion) output. More...
 
static void HAL_writePwmData (HAL_Handle handle, const HAL_PwmData_t *pPwmData)
 Writes PWM data to the PWM comparators for motor control. More...
 
static uint16_t HAL_readPwmPeriod (HAL_Handle handle, const PWM_Number_e pwmNumber)
 Reads PWM period register. More...
 

Function Documentation

static void HAL_acqAdcInt ( HAL_Handle  handle,
const ADC_IntNumber_e  intNumber 
)
inlinestatic

Acknowledges an interrupt from the ADC so that another ADC interrupt can happen again.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
[in]intNumberThe interrupt number

Definition at line 217 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::adcHandle, and _HAL_Obj_::pieHandle.

static void HAL_acqPwmInt ( HAL_Handle  handle,
const PWM_Number_e  pwmNumber 
)
inlinestatic

Acknowledges an interrupt from the PWM so that another PWM interrupt can happen again.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
[in]pwmNumberThe PWM number

Definition at line 237 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::pieHandle, and _HAL_Obj_::pwmHandle.

static void HAL_disablePwm ( HAL_Handle  handle)
inlinestatic

Disables the PWM device.

Turns off the outputs of the EPWM peripherals which will put the power switches into a high impedance state.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle

Definition at line 274 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::pwmHandle.

static void HAL_disableTbClockSync ( HAL_Handle  handle)
inlinestatic

Disables the ePWM module time base clock sync signal.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle

Definition at line 288 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::clkHandle.

static void HAL_enablePwm ( HAL_Handle  handle)
inlinestatic

Enables the PWM devices.

Turns on the outputs of the EPWM peripheral which will allow the power switches to be controlled.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle

Definition at line 322 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::pwmHandle.

static void HAL_enableTbClockSync ( HAL_Handle  handle)
inlinestatic

Enables the ePWM module time base clock sync signal.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle

Definition at line 341 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::clkHandle.

static ADC_SocSampleDelay_e HAL_getAdcSocSampleDelay ( HAL_Handle  handle,
const ADC_SocNumber_e  socNumber 
)
inlinestatic

Gets the ADC delay value.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
[in]socNumberThe ADC SOC number
Returns
The ADC delay value

Definition at line 355 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::adcHandle.

static float_t HAL_getBias ( HAL_Handle  handle,
const HAL_SensorType_e  sensorType,
uint_least8_t  sensorNumber 
)
inlinestatic

Gets the ADC bias value.

The ADC bias contains the feedback circuit's offset and bias. Bias is the mathematical offset used when a bi-polar signal is read into a uni-polar ADC.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
[in]sensorTypeThe sensor type
[in]sensorNumberThe sensor number
Returns
The ADC bias value

Definition at line 372 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::adcBias, HAL_SensorType_Current, HAL_SensorType_Voltage, _HAL_AdcData_t_::I_A, _HAL_AdcData_t_::V_V, and _MATH_vec3_::value.

Referenced by HAL_updateAdcBias().

static float_t HAL_getCurrentScaleFactor ( HAL_Handle  handle)
inlinestatic

Gets the current scale factor.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
Returns
The current scale factor

Definition at line 395 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::current_sf.

Referenced by HAL_readAdcData(), and HAL_readAdcDataWithOffsets().

static void HAL_getDutyCycles ( HAL_Handle  handle,
uint16_t *  pDutyCycles 
)
inlinestatic

Gets the PWM duty cycle times.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
[in]pDutyCyclesA pointer to memory for the duty cycle durations

Definition at line 406 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::pwmHandle.

static uint_least8_t HAL_getNumCurrentSensors ( HAL_Handle  handle)
inlinestatic

Gets the number of current sensors.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
Returns
The number of current sensors

Definition at line 421 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::numCurrentSensors.

Referenced by HAL_updateAdcBias().

static uint_least8_t HAL_getNumVoltageSensors ( HAL_Handle  handle)
inlinestatic

Gets the number of voltage sensors.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
Returns
The number of voltage sensors

Definition at line 433 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::numVoltageSensors.

Referenced by HAL_updateAdcBias().

static float_t HAL_getVoltageScaleFactor ( HAL_Handle  handle)
inlinestatic

Gets the voltage scale factor.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
Returns
The voltage scale factor

Definition at line 445 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::voltage_sf.

Referenced by HAL_readAdcData(), and HAL_readAdcDataWithOffsets().

static void HAL_initIntVectorTable ( HAL_Handle  handle)
inlinestatic

Initializes the interrupt vector table.

Points the ISR to the function mainISR.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle

Definition at line 486 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References mainISR(), and _HAL_Obj_::pieHandle.

static void HAL_readAdcData ( HAL_Handle  handle,
HAL_AdcData_t pAdcData 
)
inlinestatic

Reads the ADC data.

Reads in the ADC result registers, adjusts for offsets, and scales the values according to the settings in user.h. The structure gAdcData holds three phase voltages, three line currents, and one DC bus voltage.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
[in]pAdcDataA pointer to the ADC data buffer

Definition at line 512 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::adcBias, _HAL_Obj_::adcHandle, _HAL_AdcData_t_::dcBus_V, HAL_getCurrentScaleFactor(), HAL_getVoltageScaleFactor(), _HAL_AdcData_t_::I_A, _HAL_AdcData_t_::V_V, and _MATH_vec3_::value.

static void HAL_readAdcDataWithOffsets ( HAL_Handle  handle,
HAL_AdcData_t pAdcData 
)
inlinestatic
static uint16_t HAL_readPwmPeriod ( HAL_Handle  handle,
const PWM_Number_e  pwmNumber 
)
inlinestatic

Reads PWM period register.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
[in]pwmNumberThe PWM number
Returns
The PWM period value

Definition at line 975 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::pwmHandle.

static uint32_t HAL_readTimerCnt ( HAL_Handle  handle,
const uint_least8_t  timerNumber 
)
inlinestatic

Reads the timer count.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
[in]timerNumberThe timer number, 0,1 or 2
Returns
The timer count

Definition at line 607 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::timerHandle.

static void HAL_resetPwmCount ( HAL_Handle  handle,
PWM_Number_e  pwmNumber 
)
inlinestatic

Resets the PWM count.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
[in]pwmNumberThe PWM number

Definition at line 619 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::pwmHandle.

static void HAL_setAdcSocSampleDelay ( HAL_Handle  handle,
const ADC_SocNumber_e  socNumber,
const ADC_SocSampleDelay_e  sampleDelay 
)
inlinestatic

Sets the ADC SOC sample delay value.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
[in]socNumberThe SOC number
[in]sampleDelayThe delay value for the ADC

Definition at line 634 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::adcHandle.

static void HAL_setBias ( HAL_Handle  handle,
const HAL_SensorType_e  sensorType,
uint_least8_t  sensorNumber,
const float_t  bias 
)
inlinestatic

Sets the ADC bias value.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
[in]sensorTypeThe sensor type
[in]sensorNumberThe sensor number
[in]biasThe ADC bias value

Definition at line 651 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::adcBias, HAL_SensorType_Current, HAL_SensorType_Voltage, _HAL_AdcData_t_::I_A, _HAL_AdcData_t_::V_V, and _MATH_vec3_::value.

Referenced by HAL_updateAdcBias().

static void HAL_setCurrentScaleFactor ( HAL_Handle  handle,
const float_t  current_sf 
)
inlinestatic

Sets the current scale factor in the hal.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
[in]current_sfThe current scale factor

Definition at line 675 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::current_sf.

static void HAL_setGpioHigh ( HAL_Handle  handle,
const GPIO_Number_e  gpioNumber 
)
inlinestatic

Sets the GPIO pin high.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
[in]gpioNumberThe GPIO number

Definition at line 689 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::gpioHandle.

static void HAL_setGpioLow ( HAL_Handle  handle,
const GPIO_Number_e  gpioNumber 
)
inlinestatic

Sets the GPIO pin low.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
[in]gpioNumberThe GPIO number

Definition at line 704 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::gpioHandle.

static void HAL_setNumCurrentSensors ( HAL_Handle  handle,
const uint_least8_t  numCurrentSensors 
)
inlinestatic

Sets the number of current sensors.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
[in]numCurrentSensorsThe number of current sensors

Definition at line 719 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::numCurrentSensors.

static void HAL_setNumVoltageSensors ( HAL_Handle  handle,
const uint_least8_t  numVoltageSensors 
)
inlinestatic

Sets the number of voltage sensors.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
[in]numVoltageSensorsThe number of voltage sensors

Definition at line 733 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::numVoltageSensors.

static void HAL_setPwmFreq_kHz ( HAL_Handle  handle,
PWM_Number_e  pwmNumber,
HAL_PwmFreq_e  pwmFreq_kHz 
)
inlinestatic

Sets the PWM frequency.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
[in]pwmNumberThe PWM number
[in]pwmFreq_kHzThe PWM frequency, kHz

Definition at line 748 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::pwmHandle.

static void HAL_setVoltageScaleFactor ( HAL_Handle  handle,
const float_t  voltage_sf 
)
inlinestatic

Sets the voltage scale factor in the hal.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
[in]voltage_sfThe voltage scale factor

Definition at line 763 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::voltage_sf.

static void HAL_toggleGpio ( HAL_Handle  handle,
const GPIO_Number_e  gpioNumber 
)
inlinestatic

Toggles the GPIO pin.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
[in]gpioNumberThe GPIO number

Definition at line 852 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References _HAL_Obj_::gpioHandle.

static void HAL_updateAdcBias ( HAL_Handle  handle,
OFFSET_Handle pOffsetHandle_I,
OFFSET_Handle pOffsetHandle_V 
)
inlinestatic

Updates the ADC bias values.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
[in]pOffsetHandle_IThe pointer to the the current offset handles
[in]pOffsetHandle_VThe pointer to the the voltage offset handles

Definition at line 868 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References HAL_getBias(), HAL_getNumCurrentSensors(), HAL_getNumVoltageSensors(), HAL_SensorType_Current, HAL_SensorType_Voltage, HAL_setBias(), and OFFSET_getOffset().

static void HAL_writeDacData ( HAL_Handle  handle,
const HAL_DacData_t pDacData 
)
inlinestatic

Writes DAC data to the PWM comparators for DAC (digital-to-analog conversion) output.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
[in]pDacDataThe pointer to the DAC data

Definition at line 903 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References MATH_sat(), _HAL_Obj_::pwmDacHandle, and _HAL_DacData_t_::value.

static void HAL_writePwmData ( HAL_Handle  handle,
const HAL_PwmData_t pPwmData 
)
inlinestatic

Writes PWM data to the PWM comparators for motor control.

Parameters
[in]handleThe hardware abstraction layer (HAL) handle
[in]pPwmDataThe pointer to the PWM data

Definition at line 948 of file hvkit_rev1p1/f28x/f2806x/src/float/hal.h.

References MATH_sat(), _HAL_Obj_::pwmHandle, _HAL_PwmData_t_::Vabc_pu, and _MATH_vec3_::value.