|
MotorWare f2806x Module API Documentation
|
#include "sw/modules/types/src/types.h"#include "sw/modules/iqmath/src/32b/IQmathLib.h"#include "sw/modules/filter/src/32b/filter_fo.h"#include "sw/modules/math/src/32b/math.h"#include "sw/modules/park/src/32b/park.h"#include "sw/modules/pid/src/32b/pid.h"Go to the source code of this file.
Typedefs | |
| typedef struct IPD_HFI_Obj * | IPD_HFI_Handle |
| Defines the IPD_HFI handle. More... | |
Enumerations | |
| enum | IPD_HFI_State_e { IPD_HFI_State_Error = 0, IPD_HFI_State_Idle = 1, IPD_HFI_State_Coarse = 2, IPD_HFI_State_Fine = 3, IPD_HFI_State_OnLine = 4, IPD_HFI_State_NumStates = 5 } |
| Defines the initial position detection, high frequency injection (IPD_HFI) states. More... | |
| enum | IPD_HFI_TRAJ_State_e { IPD_HFI_TRAJ_State_Idle = 0, IPD_HFI_TRAJ_State_Coarse = 1, IPD_HFI_TRAJ_State_Fine = 2, IPD_HFI_TRAJ_State_NumStates = 3 } |
| Defines the trajectory states. More... | |
Functions | |
| static void | IPD_HFI_computePhasor (const _iq angle_pu, MATH_vec2 *pPhasor) |
| Computes a phasor for a given angle. More... | |
| void | IPD_HFI_disable (IPD_HFI_Handle handle) |
| Disables the initial position detection, high frequency injection (IPD_HFI) module. More... | |
| void | IPD_HFI_enable (IPD_HFI_Handle handle) |
| Enables the initial position detection, high frequency injection (IPD_HFI) module. More... | |
| _iq | IPD_HFI_getAngle_pu (IPD_HFI_Handle handle) |
| Gets the angle value from the estimator. More... | |
| _iq | IPD_HFI_getKspd_pu (IPD_HFI_Handle handle) |
| Gets the speed gain value. More... | |
| _iq | IPD_HFI_getSpeed_pu (IPD_HFI_Handle handle) |
| Gets the speed value from the estimator. More... | |
| _iq | IPD_HFI_getSpeed_lp_pu (IPD_HFI_Handle handle) |
| Gets the low pass filtered speed value from the estimator. More... | |
| IPD_HFI_State_e | IPD_HFI_getState (IPD_HFI_Handle handle) |
| Gets the estimator state. More... | |
| _iq | IPD_HFI_getVdValue (IPD_HFI_Handle handle) |
| Gets the current trajectory magnitude value. More... | |
| IPD_HFI_Handle | IPD_HFI_init (void) |
| Initializes the initial position detection, high frequency injection (IPD_HFI) module. More... | |
| bool | IPD_HFI_isEnabled (IPD_HFI_Handle handle) |
| Returns a boolean value denoting if the module is enabled (true) or not (false) More... | |
| bool | IPD_HFI_isOnLine (IPD_HFI_Handle handle) |
| Denotes whether the module is online (true) or not (false) More... | |
| void | IPD_HFI_run (IPD_HFI_Handle handle, const MATH_vec2 *pIab_pu) |
| Runs the initial position detection, high frequency injection (IPD_HFI) algorithm. More... | |
| void | IPD_HFI_setAngle_pu (IPD_HFI_Handle handle, const _iq angle_pu) |
| Sets the angle value in the module. More... | |
| void | IPD_HFI_setFlag_motorSpinning (IPD_HFI_Handle handle, const bool value) |
| Sets the value of the motor spinning flag. More... | |
| void | IPD_HFI_setHpf_Idq_Params (IPD_HFI_Handle handle, const _iq b0, const _iq b1, const _iq a1, const _iq x1, const _iq y1) |
| Sets the Idq high pass filter parameters. More... | |
| void | IPD_HFI_setId_sum (IPD_HFI_Handle handle, const _iq Id_sum_pu) |
| Sets the integral value for the direct current in the estimator. More... | |
| void | IPD_HFI_setKspd_pu (IPD_HFI_Handle handle, const _iq Kspd_pu) |
| Sets the speed gain value. More... | |
| void | IPD_HFI_setLpf_spd_Params (IPD_HFI_Handle handle, const _iq b0, const _iq b1, const _iq a1, const _iq x1, const _iq y1) |
| Sets the speed low pass filter parameters. More... | |
| void | IPD_HFI_setParams (IPD_HFI_Handle handle, float_t estFreq_Hz, float_t excFreq_Hz, float_t lpFilterCutOffFreq_Hz, float_t hpFilterCutOffFreq_Hz, float_t iqFullScaleFreq_Hz, float_t Kspd, float_t excMag_coarse_pu, float_t excMag_fine_pu, float_t waitTime_coarse_sec, float_t waitTime_fine_sec) |
| Sets the initial position detection, high frequency injection (IPD_HFI) parameters. More... | |
| void | IPD_HFI_setSpeed_pu (IPD_HFI_Handle handle, const _iq speed_pu) |
| Sets the speed value in the estimator. More... | |
| void | IPD_HFI_setSpeed_lp_pu (IPD_HFI_Handle handle, const _iq speed_lp_pu) |
| Sets the low pass filtered speed value in the estimator. More... | |
| void | IPD_HFI_setTrajMags (IPD_HFI_Handle handle, const _iq *pMags) |
| Sets the trajectory magnitudes in the estimator. More... | |
| void | IPD_HFI_setTrajParams (IPD_HFI_Handle handle, const uint_least32_t period, const uint_least32_t targetPeriod, const _iq *pTrajMags, const uint_least32_t *pTrajPeriods) |
| Sets the trajectory parameters in the estimator. More... | |
| void | IPD_HFI_setTrajPeriods (IPD_HFI_Handle handle, const uint_least32_t *pPeriods) |
| Sets the periods for each trajectory state. More... | |
| void | IPD_HFI_setWaitTimes (IPD_HFI_Handle handle, const uint_least32_t *pWaitTimes) |
| Sets the wait times for each estimator state. More... | |
| void | IPD_HFI_updateState (IPD_HFI_Handle handle) |
| Updates the state. More... | |
1.8.9.1