|
MotorWare f2806x Module API Documentation
|
Contains the public interface to the types definitions. More...
#include "stdbool.h"#include "string.h"#include "stdint.h"Go to the source code of this file.
Data Structures | |
| struct | _cplx_int_least8_t |
| Define the complex data type for at least 8 bit signed real and imaginary components. More... | |
| struct | _cplx_uint_least8_t |
| Define the complex data type for at least 8 bit unsigned real and imaginary components. More... | |
| struct | _cplx_least16_t |
| Define the complex data type for at least 16 bit signed real and imaginary components. More... | |
| struct | _cplx_uleast16_t |
| Define the complex data type for at least 16 bit unsigned real and imaginary components. More... | |
| struct | _cplx_int_least32_t_ |
| Define the complex data type for at least 32 bit signed real and imaginary components. More... | |
| struct | _cplx_uint_least32_t_ |
| Define the complex data type for at least 32 bit unsigned real and imaginary components. More... | |
| struct | _cplx_int16_t_ |
| Define the complex data type for 16 bit signed real and imaginary components. More... | |
| struct | _cplx_uint16_t_ |
| Define the complex data type for 16 bit unsigned real and imaginary components. More... | |
| struct | _cplx_int32_t |
| Define the complex data type for 32 bit signed real and imaginary components. More... | |
| struct | _cplx_uint32_t |
| Define the complex data type for 32 bit unsigned real and imaginary components. More... | |
Macros | |
| #define | HIGH 1 |
| Defines high. More... | |
| #define | LOW 0 |
| Defines low. More... | |
| #define | OFF 0 |
| Defines off. More... | |
| #define | OK 0 |
| Defines ok. More... | |
| #define | ON 1 |
| Defines on. More... | |
| #define | ERROR 1 |
| Defines generic error. More... | |
| #define | PASS 1 |
| Defines pass. More... | |
| #define | FAIL 0 |
| Defines fails. More... | |
Typedefs | |
| typedef unsigned int | status |
| Defines the portable data type for a status result. More... | |
| typedef float | float_t |
| Defines the portable data type for 32 bit, signed floating-point data. More... | |
| typedef long double | double_t |
| Defines the portable data type for 64 bit, signed floating-point data. More... | |
| typedef struct _cplx_int_least8_t | cplx_int_least8_t |
| Define the complex data type for at least 8 bit signed real and imaginary components. More... | |
| typedef struct _cplx_uint_least8_t | cplx_uint_least8_t |
| Define the complex data type for at least 8 bit unsigned real and imaginary components. More... | |
| typedef struct _cplx_least16_t | cplx_int_least16_t |
| Define the complex data type for at least 16 bit signed real and imaginary components. More... | |
| typedef struct _cplx_uleast16_t | cplx_uint_least16_t |
| Define the complex data type for at least 16 bit unsigned real and imaginary components. More... | |
| typedef struct _cplx_int_least32_t_ | cplx_int_least32_t |
| Define the complex data type for at least 32 bit signed real and imaginary components. More... | |
| typedef struct _cplx_uint_least32_t_ | cplx_uint_least32_t |
| Define the complex data type for at least 32 bit unsigned real and imaginary components. More... | |
| typedef struct _cplx_int16_t_ | cplx_int16_t |
| Define the complex data type for 16 bit signed real and imaginary components. More... | |
| typedef struct _cplx_uint16_t_ | cplx_uint16_t |
| Define the complex data type for 16 bit unsigned real and imaginary components. More... | |
| typedef struct _cplx_int32_t | cplx_int32_t |
| Define the complex data type for 32 bit signed real and imaginary components. More... | |
| typedef struct _cplx_uint32_t | cplx_uint32_t |
| Define the complex data type for 32 bit unsigned real and imaginary components. More... | |
Contains the public interface to the types definitions.
(C) Copyright 2013, Texas Instruments, Inc.
Definition in file types.h.
1.8.9.1