/********************************************************************/
/* f2808.gel                                                        */
/* Version 4.00.1                                                   */
/*                                                                  */
/* This GEL file is to be used with the TMS320F2808 DSP.            */
/* Changes may be required to support specific hardware designs.    */
/*                                                                  */
/* Code Composer Studio supports six reserved GEL functions that    */
/* automatically get executed if they are defined. They are:        */
/*                                                                  */
/* StartUp()              - Executed whenever CCS is invoked        */
/* OnReset()              - Executed after Debug->Reset CPU         */
/* OnRestart()            - Executed after Debug->Restart           */
/* OnPreFileLoaded()      - Executed before File->Load Program      */
/* OnFileLoaded()         - Executed after File->Load Program       */
/* OnTargetConnect()      - Executed after Debug->Connect           */
/*                                                                  */
/********************************************************************/

StartUp()
{

/* The next line automatically loads the .gel file that comes   */
/* with the DSP280x Peripheral Header Files download.  To use,  */
/* uncomment, and copy the peripheral header .gel file to       */
/* same directory as device .gel file.                          */
//  GEL_LoadGel("$(GEL_file_dir)\\DSP280x_Peripheral.gel");
}

OnReset(int nErrorCode)
{
    if (GEL_IsInRealtimeMode())   /* If in real-time-mode */
    {
    }
    else    /* Put device in C28x mode */
    {
         C28x_Mode();
    }
    Unlock_CSM();
}

OnRestart(int nErrorCode)
{
/* CCS will call OnRestart() when you do a Debug->Restart and   */
/* after you load a new file.  Between running interrupt based  */
/* programs, this function will clear interrupts and help keep  */
/* the processor from going off into invalid memory.            */
     if (GEL_IsInRealtimeMode())   /* If in real-time-mode */
    {
    }
    else    /* Put device in C28x mode */
    {
         C28x_Mode();
    }
     IER = 0;
     IFR = 0;
}

OnPreFileLoaded()
{
    GEL_Reset();
}

OnFileLoaded(int nErrorCode, int bSymbolsOnly)
{
}

OnTargetConnect()
{

    if (GEL_IsInRealtimeMode())   /* If in real-time-mode */
    {
    }
    else    /* Put device in C28x mode */
    {
         C28x_Mode();
    }
    F2808_Memory_Map();        /* Initialize the CCS memory map */

/* Check to see if CCS has been started-up with the DSP already */
/* running in real-time mode.  The user can add whatever        */
/* custom initialization stuff they want to each case.          */

    if (GEL_IsInRealtimeMode())     /* Do real-time mode target initialization */
    {

    }
    else                            /* Do stop-mode target initialization */
    {
        GEL_Reset();                /* Reset DSP */
    }
}


/********************************************************************/
/* These functions are useful to engage/disengage realtime          */
/* emulation mode during debug.  They save the user from having to  */
/* manually perform these steps in CCS.                             */
/********************************************************************/
menuitem "Realtime Emulation Control";

hotmenu Run_Realtime_with_Reset()
{
    GEL_Reset();                /* Reset the DSP */
    ST1 = ST1 & 0xFFFD;         /* clear DBGM bit in ST1 */
    GEL_EnableRealtime();       /* Enable Realtime mode */
    GEL_Run();                  /* Run the DSP */
}
hotmenu Run_Realtime_with_Restart()
{
    GEL_Restart();              /* Reset the DSP */
    ST1 = ST1 & 0xFFFD;         /* clear DBGM bit in ST1 */
    GEL_EnableRealtime();       /* Enable Realtime mode */
    GEL_Run();                  /* Run the DSP */
}
hotmenu Full_Halt()
{
    GEL_DisableRealtime();      /* Disable Realtime mode */
    GEL_Halt();                 /* Halt the DSP */
}
hotmenu Full_Halt_with_Reset()
{
    GEL_DisableRealtime();      /* Disable Realtime mode */
    GEL_Halt();                 /* Halt the DSP */
    GEL_Reset();                /* Reset the DSP */
}

/********************************************************************/
/* These functions are launched by the GEL_Toolbar button plugin    */
/********************************************************************/
GEL_Toolbar1()
{
    Run_Realtime_with_Reset();
}
GEL_Toolbar2()
{
    Run_Realtime_with_Restart();
}
GEL_Toolbar3()
{
    Full_Halt();
}
GEL_Toolbar4()
{
    Full_Halt_with_Reset();
}

GEL_Toolbar5()
{
    Full_Halt_with_Reset();
    GEL_Restart();
}

/********************************************************************/
/*                         F2808 Memory Map                         */
/*                                                                  */
/*   Note: M0M1MAP and VMAP signals tied high on F2808 core         */
/*                                                                  */
/*   0x000000 - 0x0003ff   M0 SARAM                (Prog and Data)  */
/*   0x000400 - 0x0007ff   M1 SARAM                (Prog and Data)  */
/*   0x000800 - 0x000fff   Peripheral Frame0 (PF0) (Data only)      */
/*   0x006000 - 0x006fff   Peripheral Frame1 (PF1) (Data only)      */
/*   0x007000 - 0x007fff   Peripheral Frame2 (PF2) (Data only)      */
/*   0x008000 - 0x008fff   L0 SARAM                (Prog and Data)  */
/*   0x009000 - 0x009fff   L1 SARAM                (Prog and Data)  */
/*   0x00a000 - 0x00bfff   H0 SARAM Mirror         (Prog and Data)  */
/*   0x3d7800 - 0x3d7fff   OTP                     (Prog and Data)  */
/*   0x3e8000 - 0x3f7fff   FLASH                   (Prog and Data)  */
/*   0x3f8000 - 0x3f8fff   L0 SARAM Mirror         (Prog and Data)  */
/*   0x3f9000 - 0x3f9fff   L1 SARAM Mirror         (Prog and Data)  */
/*   0x3fa000 - 0x3fbfff   H0 SARAM                (Prog and Data)  */
/*   0x3ff000 - 0x3fffff   BOOT ROM                (Prog and Data)  */
/********************************************************************/
menuitem "Initialize Memory Map";

hotmenu F2808_Memory_Map()
{
    GEL_MapReset();
    GEL_MapOn();

    /* Program memory maps */
    GEL_MapAdd(0x0,0,0x400,1,1);                 /* M0 SARAM        */
    GEL_MapAdd(0x400,0,0x400,1,1);               /* M1 SARAM        */
    GEL_MapAdd(0x8000,0,0x1000,1,1);             /* L0 SARAM        */
    GEL_MapAdd(0x9000,0,0x1000,1,1);             /* L1 SARAM        */
    GEL_MapAdd(0xa000,0,0x2000,1,1);             /* H0 SARAM Mirror */
    GEL_MapAdd(0x3d7800,0,0x400,1,0);            /* OTP             */
    GEL_MapAdd(0x3e8000,0,0x10000,1,0);          /* FLASH           */
    GEL_MapAdd(0x3f8000,0,0x1000,1,1);           /* L0 SARAM Mirror */
    GEL_MapAdd(0x3f9000,0,0x1000,1,1);           /* L1 SARAM Mirror */
    GEL_MapAdd(0x3fa000,0,0x2000,1,1);           /* H0 SARAM        */
    GEL_MapAdd(0x3ff000,0,0x1000,1,0);           /* BOOT ROM        */


    /* Data memory maps */
    GEL_MapAdd(0x0,1,0x400,1,1);                 /* M0 SARAM        */
    GEL_MapAdd(0x400,1,0x400,1,1);               /* M1 SARAM        */
    GEL_MapAdd(0x800,1,0x800,1,1);               /* PF0             */
    GEL_MapAdd(0x6000,1,0x1000,1,1);             /* PF1             */
    GEL_MapAddStr(0x7000,1,0x1000,"R|W|AS2",0);  /* PF2             */
    GEL_MapAdd(0x8000,1,0x1000,1,1);             /* L0 SARAM        */
    GEL_MapAdd(0x9000,1,0x1000,1,1);             /* L1 SARAM        */
    GEL_MapAdd(0xa000,1,0x2000,1,1);             /* H0 SARAM Mirror */
    GEL_MapAdd(0x3d7800,1,0x800,1,0);            /* OTP             */
    GEL_MapAdd(0x3e8000,1,0x10000,1,0);          /* FLASH           */
    GEL_MapAdd(0x3f8000,1,0x1000,1,1);           /* L0 SARAM Mirror */
    GEL_MapAdd(0x3f9000,1,0x1000,1,1);           /* L1 SARAM Mirror */
    GEL_MapAdd(0x3fa000,1,0x2000,1,1);           /* H0 SARAM        */
    GEL_MapAdd(0x3ff000,1,0x1000,1,0);           /* BOOT ROM        */
}


/********************************************************************/
/* The ESTOP0 fill functions are useful for debug.  They fill the   */
/* RAM with software breakpoints that will trap runaway code.       */
/********************************************************************/
hotmenu Fill_F2808_RAM_with_ESTOP0()
{
    GEL_MemoryFill(0x000000,1,0x000800,0x7625);      /* Fill M0/M1  */
    GEL_MemoryFill(0x008000,1,0x002000,0x7625);      /* Fill L0/L1  */
    GEL_MemoryFill(0x3FA000,1,0x002000,0x7625);      /* Fill H0     */
}


/********************************************************************/
menuitem "Watchdog";
hotmenu Disable_WD()
{
    *0x7029 = *0x7029 | 0x0068;                /* Set the WDDIS bit */
    *0x7025 = 0x0055;                          /* Service the WD    */
    *0x7025 = 0x00AA;                          /*  once to be safe. */
    GEL_TextOut("\nWatchdog Timer Disabled");
}


/********************************************************************/
menuitem "Code Security Module"
hotmenu Unlock_CSM()
{
    /* Perform dummy reads of the password locations */
    XAR0 = *0x3F7FF8;
    XAR0 = *0x3F7FF9;
    XAR0 = *0x3F7FFA;
    XAR0 = *0x3F7FFB;
    XAR0 = *0x3F7FFC;
    XAR0 = *0x3F7FFD;
    XAR0 = *0x3F7FFE;
    XAR0 = *0x3F7FFF;

    /* Write passwords to the KEY registers.  0xFFFF's are dummy passwords.
       User should replace them with the correct password for their DSP */
    *0xAE0 = 0xFFFF;
    *0xAE1 = 0xFFFF;
    *0xAE2 = 0xFFFF;
    *0xAE3 = 0xFFFF;
    *0xAE4 = 0xFFFF;
    *0xAE5 = 0xFFFF;
    *0xAE6 = 0xFFFF;
    *0xAE7 = 0xFFFF;
}


/********************************************************************/
menuitem "Addressing Modes";

hotmenu C28x_Mode()
{
    ST1 = ST1 & (~0x0100);      /*   AMODE = 0  */
    ST1 = ST1 | 0x0200;         /* OBJMODE = 1  */
}

hotmenu C24x_Mode()
{
    ST1 = ST1 | 0x0100;         /*   AMODE = 1  */
    ST1 = ST1 | 0x0200;         /* OBJMODE = 1  */
}

hotmenu C27x_Mode()
{
    ST1 = ST1 & (~0x0100);      /*   AMODE = 0  */
    ST1 = ST1 & (~0x0200);      /* OBJMODE = 0  */
}


/********************************************************************/
/*                            PLL Ratios                            */
/*                                                                  */
/* The following table describes the PLL clocking ratios (0..10)    */
/*                                                                  */
/*   Ratio        CLKIN         Description                         */
/*   -----    --------------    ------------                        */
/*     0      OSCCLK/2          PLL bypassed                        */
/*     1      (OSCCLK * 1)/2    10 Mhz for 20 Mhz CLKIN             */
/*     2      (OSCCLK * 2)/2    20 Mhz for 20 Mhz CLKIN             */
/*     3      (OSCCLK * 3)/2    30 Mhz for 20 Mhz CLKIN             */
/*     4      (OSCCLK * 4)/2    40 Mhz for 20 Mhz CLKIN             */
/*     5      (OSCCLK * 5)/2    50 Mhz for 20 Mhz CLKIN             */
/*     6      (OSCCLK * 6)/2    60 Mhz for 20 Mhz CLKIN             */
/*     7      (OSCCLK * 7)/2    70 Mhz for 20 Mhz CLKIN             */
/*     8      (OSCCLK * 8)/2    80 Mhz for 20 Mhz CLKIN             */
/*     9      (OSCCLK * 9)/2    90 Mhz for 20 Mhz CLKIN             */
/*    10      (OSCCLK * 10)/2  100 Mhz for 20 Mhz CLKIN             */
/********************************************************************/
menuitem "Set PLL Ratio";

hotmenu Bypass()
{
    *0x7021 = 0;    /* CLKIN = OSCCLK/2, PLL is bypassed */
    PLL_Wait();
}
hotmenu OSCCLK_x1_divided_by_2()
{
    *0x7021 = 1;    /* CLKIN = (OSCCLK * 1)/2 */
    PLL_Wait();
}
hotmenu OSCCLK_x2_divided_by_2()
{
    *0x7021 = 2;    /* CLKIN = (OSCCLK * 2)/2 */
    PLL_Wait();
}
hotmenu OSCCLK_x3_divided_by_2()
{
    *0x7021 = 3;    /* CLKIN = (OSCCLK * 3)/2 */
    PLL_Wait();
}
hotmenu OSCCLK_x4_divided_by_2()
{
    *0x7021 = 4;    /* CLKIN = (OSCCLK * 4)/2 */
    PLL_Wait();
}
hotmenu OSCCLK_x5_divided_by_2()
{
    *0x7021 = 5;    /* CLKIN = (OSCCLK * 5)/2 */
    PLL_Wait();
}
hotmenu OSCCLK_x6_divided_by_2()
{
    *0x7021 = 6;    /* CLKIN = (OSCCLK * 6)/2 */
    PLL_Wait();
}
hotmenu OSCCLK_x7_divided_by_2()
{
    *0x7021 = 7;    /* CLKIN = (OSCCLK * 7)/2 */
    PLL_Wait();
}
hotmenu OSCCLK_x8_divided_by_2()
{
    *0x7021 = 8;    /* CLKIN = (OSCCLK * 8)/2 */
    PLL_Wait();
}
hotmenu OSCCLK_x9_divided_by_2()
{
    *0x7021 = 9;    /* CLKIN = (OSCCLK * 9)/2 */
    PLL_Wait();
}
hotmenu OSCCLK_x10_divided_by_2()
{
    *0x7021 = 10;    /* CLKIN = (OSCCLK * 10)/2 */
    PLL_Wait();
}

/********************************************************************/
/* For F280x devices, check the PLLOCKS bit for PLL lock.           */
/********************************************************************/
PLL_Wait()
{
    int PLLSTS;
    int delay = 0;

    PLLSTS = 0x7011;


    while ( ( (unsigned int)*PLLSTS & 0x0001) != 0x0001)
    {
        delay++;
        GEL_TextOut("Waiting for PLL Lock, PLLSTS = %x\n",,,,,(unsigned int)*PLLSTS);
    }
    GEL_TextOut("\nPLL lock complete, PLLSTS = %x\n",,,,,(unsigned int)*PLLSTS);
}

/********************************************************************/
/*** End of file ***/