MotorWare f2806x Driver API Documentation
Functions
clk.c File Reference

Contains the various functions related to the clock object. More...

#include "sw/drivers/clk/src/32b/f28x/f2806x/clk.h"

Go to the source code of this file.

Functions

void CLK_disableAdcClock (CLK_Handle clkHandle)
 Disables the ADC clock. More...
 
void CLK_disableClaClock (CLK_Handle clkHandle)
 Disables the CLA clock. More...
 
void CLK_disableClkIn (CLK_Handle clkHandle)
 Disables the XCLKIN oscillator input. More...
 
void CLK_disableCompClock (CLK_Handle clkHandle, const CLK_CompNumber_e compNumber)
 Disables the comparator clock. More...
 
void CLK_disableCpuTimerClock (CLK_Handle clkHandle, const CLK_CpuTimerNumber_e cpuTimerNumber)
 Disables the CPU timer clock. More...
 
void CLK_disableCrystalOsc (CLK_Handle clkHandle)
 Disables the crystal oscillator. More...
 
void CLK_disableEcanaClock (CLK_Handle clkHandle)
 Disables the ECANA clock. More...
 
void CLK_disableEcap1Clock (CLK_Handle clkHandle)
 Disables the ECAP1 clock. More...
 
void CLK_disableEqep1Clock (CLK_Handle clkHandle)
 Disables the EQEP1 clock. More...
 
void CLK_disableEqep2Clock (CLK_Handle clkHandle)
 Disables the EQEP2 clock. More...
 
void CLK_disableGpioInputClock (CLK_Handle clkHandle)
 Disables the GPIO input clock. More...
 
void CLK_disableHrPwmClock (CLK_Handle clkHandle)
 Disables the HRPWM clock. More...
 
void CLK_disableI2cClock (CLK_Handle clkHandle)
 Disables the I2C clock. More...
 
void CLK_disableLinAClock (CLK_Handle clkHandle)
 Disables the LIN-A clock. More...
 
void CLK_disableOsc1 (CLK_Handle clkHandle)
 Disables internal oscillator 1. More...
 
void CLK_disableOsc1HaltMode (CLK_Handle clkHandle)
 Disables internal oscillator 1 halt mode ignore. More...
 
void CLK_disableOsc2 (CLK_Handle clkHandle)
 Disables internal oscillator 2. More...
 
void CLK_disableOsc2HaltMode (CLK_Handle clkHandle)
 Disables internal oscillator 2 halt mode ignore. More...
 
void CLK_disablePwmClock (CLK_Handle clkHandle, const PWM_Number_e pwmNumber)
 Disables the pwm clock. More...
 
void CLK_disableSciaClock (CLK_Handle clkHandle)
 Disables the SCI-A clock. More...
 
void CLK_disableScibClock (CLK_Handle clkHandle)
 Disables the SCI-B clock. More...
 
void CLK_disableSpiaClock (CLK_Handle clkHandle)
 Disables the SPI-A clock. More...
 
void CLK_disableSpibClock (CLK_Handle clkHandle)
 Disables the SPI-B clock. More...
 
void CLK_disableTbClockSync (CLK_Handle clkHandle)
 Disables the ePWM module time base clock sync signal. More...
 
void CLK_disableWatchDogHaltMode (CLK_Handle clkHandle)
 Disables the watchdog halt mode ignore. More...
 
void CLK_enableAdcClock (CLK_Handle clkHandle)
 Enables the ADC clock. More...
 
void CLK_enableClaClock (CLK_Handle clkHandle)
 Enables the CLA clock. More...
 
void CLK_enableCompClock (CLK_Handle clkHandle, const CLK_CompNumber_e compNumber)
 Enables the comparator clock. More...
 
void CLK_enableCpuTimerClock (CLK_Handle clkHandle, const CLK_CpuTimerNumber_e cpuTimerNumber)
 Enables the CPU timer clock. More...
 
void CLK_enableCrystalOsc (CLK_Handle clkHandle)
 Enables the crystal oscillator. More...
 
void CLK_enableEcanaClock (CLK_Handle clkHandle)
 Enables the ECANA clock. More...
 
void CLK_enableEqep1Clock (CLK_Handle clkHandle)
 Enables the EQEP1 clock. More...
 
void CLK_enableEqep2Clock (CLK_Handle clkHandle)
 Enables the EQEP2 clock. More...
 
void CLK_enableEcap1Clock (CLK_Handle clkHandle)
 Enables the ECAP1 clock. More...
 
void CLK_enableClkIn (CLK_Handle clkHandle)
 Enables the XCLKIN oscillator input. More...
 
void CLK_enableGpioInputClock (CLK_Handle clkHandle)
 Enables the GPIO input clock. More...
 
void CLK_enableHrPwmClock (CLK_Handle clkHandle)
 Enables the HRPWM clock. More...
 
void CLK_enableI2cClock (CLK_Handle clkHandle)
 Enables the I2C clock. More...
 
void CLK_enableLinAClock (CLK_Handle clkHandle)
 Enables the LIN-A clock. More...
 
void CLK_enableOsc1 (CLK_Handle clkHandle)
 Enables internal oscillator 1. More...
 
void CLK_enableOsc1HaltMode (CLK_Handle clkHandle)
 Enables internal oscillator 1 halt mode ignore. More...
 
void CLK_enableOsc2 (CLK_Handle clkHandle)
 Enables internal oscillator 2. More...
 
void CLK_enableOsc2HaltMode (CLK_Handle clkHandle)
 Enables internal oscillator 2 halt mode ignore. More...
 
void CLK_enablePwmClock (CLK_Handle clkHandle, const PWM_Number_e pwmNumber)
 Enables the pwm clock. More...
 
void CLK_enableSciaClock (CLK_Handle clkHandle)
 Enables the SCI-A clock. More...
 
void CLK_enableScibClock (CLK_Handle clkHandle)
 Enables the SCI-B clock. More...
 
void CLK_enableSpiaClock (CLK_Handle clkHandle)
 Enables the SPI-A clock. More...
 
void CLK_enableSpibClock (CLK_Handle clkHandle)
 Enables the SPI-B clock. More...
 
void CLK_enableTbClockSync (CLK_Handle clkHandle)
 Enables the ePWM module time base clock sync signal. More...
 
void CLK_enableWatchDogHaltMode (CLK_Handle clkHandle)
 Enables the watchdog halt mode ignore. More...
 
CLK_Handle CLK_init (void *pMemory, const size_t numBytes)
 Initializes the clock (CLK) object handle. More...
 
void CLK_setClkOutPreScaler (CLK_Handle clkHandle, const CLK_ClkOutPreScaler_e preScaler)
 Sets the external clock out prescaler. More...
 
void CLK_setLowSpdPreScaler (CLK_Handle clkHandle, const CLK_LowSpdPreScaler_e preScaler)
 Sets the low speed peripheral clock prescaler. More...
 
void CLK_setOscSrc (CLK_Handle clkHandle, const CLK_OscSrc_e src)
 Sets the oscillator clock source. More...
 
void CLK_setOsc2Src (CLK_Handle clkHandle, const CLK_Osc2Src_e src)
 Sets the oscillator 2 clock source. More...
 
void CLK_setXClkInSrc (CLK_Handle clkHandle, const CLK_XClkInSrc_e src)
 Sets the XCLKIN Clock Source. More...
 
void CLK_setTimer2PreScale (CLK_Handle clkHandle, const CLK_Timer2PreScaler_e preScaler)
 
void CLK_setTimer2Src (CLK_Handle clkHandle, const CLK_Timer2Src_e src)
 Sets the timer 2 clock source. More...
 
void CLK_setWatchDogSrc (CLK_Handle clkHandle, const CLK_WdClkSrc_e src)
 Sets the watchdog clock source. More...
 

Detailed Description

Contains the various functions related to the clock object.

(C) Copyright 2015, Texas Instruments, Inc.

Definition in file clk.c.

Function Documentation

void CLK_setTimer2PreScale ( CLK_Handle  clkHandle,
const CLK_Timer2PreScaler_e  preScaler 
)