| adc.c | Contains the various functions related to the analog-to-digital converter (ADC) object |
| adc.h | Contains public interface to various functions related to the analog-to-digital converter (ADC) object |
| adc_obj.h | Contains public interface to various functions related to the analog-to-digital converter (ADC) object |
| can.h | Contains public interface to various functions related to the CAN object |
| cap.c | Contains the various functions related to the Enhanced Capture (CAP) object |
| cap.h | Contains public interface to various functions related to the Enhanced Capture (CAP) object |
| cla.h | Contains public interface to various functions related to the CLA object |
| clk.c | Contains the various functions related to the clock object |
| clk.h | Contains public interface to various functions related to the clock (CLK) object |
| comp.c | Contains the various functions related to the comparator (COMP) object |
| comp.h | Contains public interface to various functions related to the comparator (COMP) object |
| cpu.c | Contains the various functions related to the central processing unit (CPU) object |
| cpu.h | Contains public interface to various functions related to the central processing unit (CPU) object |
| doxygen.h | |
| drv8301.c | Contains the various functions related to the DRV8301 object |
| drv8301.h | Contains public interface to various functions related to the DRV8301 object |
| emu.h | Contains public interface to various functions related to the EMU object |
| flash.c | Contains the various functions related to the flash object |
| flash.h | Contains public interface to various functions related to the flash (FLASH) object |
| gpio.c | The functions in this file are used to configure the general purpose I/O (GPIO) registers |
| gpio.h | Contains public interface to general purpose I/O (GPIO) methods |
| i2c.h | Contains public interface to various functions related to the I2C object |
| lin.h | |
| osc.c | Contains the various functions related to the oscillator object |
| osc.h | Contains public interface to various functions related to the oscillator (OSC) object |
| pie.c | Contains the various functions related to the peripheral interrupt expansion (PIE) object |
| pie.h | Contains public interface to various functions related to the peripheral interrupt expansion (PIE) object |
| pll.c | Contains the various functions related to the phase-locked loop (PLL) object |
| pll.h | Contains public interface to various functions related to the phase-locked loop (PLL) object |
| pwm.c | Contains the various functions related to the pulse width modulation (PWM) object |
| pwm.h | Contains public interface to various functions related to the pulse width modulation (PWM) object |
| pwmdac.h | Contains public interface to various functions related to the pulse width modulation digital-to-analog converter (PWMDAC) object |
| pwr.c | Contains the various functions related to the power (PWR) object |
| pwr.h | Contains public interface to various functions related to the power (PWR) object |
| qep.c | Contains the various functions related to the Quadrature Encoder Pulse (QEP) object |
| qep.h | Contains public interface to various functions related to the quadrature pulse encoder (QEP) object |
| sci.c | Contains the various functions related to the serial communications interface (SCI) object |
| sci.h | Contains public interface to various functions related to the serial communications interface (SCI) object |
| spi.c | Contains the various functions related to the serial peripheral interface (SPI) object |
| spi.h | Contains public interface to various functions related to the serial peripheral interface (SPI) object |
| timer.c | Contains the various functions related to the timer (TIMER) object |
| timer.h | Contains public interface to various functions related to the timer (TIMER) object |
| wdog.c | Contains the various functions related to the watch dog (WDOG) object |
| wdog.h | Contains public interface to various functions related to the watchdog (WDOG) timer object |