|
MotorWare f2806x Driver API Documentation
|
Data Structures | |
| struct | _CAP_Obj_ |
| Defines the capture (CAP) object. More... | |
Macros | |
| #define | CAP1_BASE_ADDR (0x00006A00) |
| Defines the base address of the capture (CAP) 1 registers. More... | |
| #define | CAP2_BASE_ADDR (0x00006A20) |
| Defines the base address of the capture (CAP) 2 registers. More... | |
| #define | CAP3_BASE_ADDR (0x00006A40) |
| Defines the base address of the capture (CAP) 3 registers. More... | |
| #define | CAP_ECCTL1_FREESOFT_BITS (3 << 14) |
| Defines the location of the FREE/SOFT bits in the ECCTL1 register. More... | |
| #define | CAP_ECCTL1_PRESCALE_BITS (31 << 9) |
| Defines the location of the PRESCALE bits in the ECCTL1 register. More... | |
| #define | CAP_ECCTL1_CAPLDEN_BITS (1 << 8) |
| Defines the location of the CAPLDEN bits in the ECCTL1 register. More... | |
| #define | CAP_ECCTL1_CTRRST4_BITS (1 << 7) |
| Defines the location of the CTRRST4 bits in the ECCTL1 register. More... | |
| #define | CAP_ECCTL1_CAP4POL_BITS (1 << 6) |
| Defines the location of the CAP4POL bits in the ECCTL1 register. More... | |
| #define | CAP_ECCTL1_CTRRST3_BITS (1 << 5) |
| Defines the location of the CTRRST3 bits in the ECCTL1 register. More... | |
| #define | CAP_ECCTL1_CAP3POL_BITS (1 << 4) |
| Defines the location of the CAP3POL bits in the ECCTL1 register. More... | |
| #define | CAP_ECCTL1_CTRRST2_BITS (1 << 3) |
| Defines the location of the CTRRST2 bits in the ECCTL1 register. More... | |
| #define | CAP_ECCTL1_CAP2POL_BITS (1 << 2) |
| Defines the location of the CAP2POL bits in the ECCTL1 register. More... | |
| #define | CAP_ECCTL1_CTRRST1_BITS (1 << 1) |
| Defines the location of the CTRRST1 bits in the ECCTL1 register. More... | |
| #define | CAP_ECCTL1_CAP1POL_BITS (1 << 0) |
| Defines the location of the CAP1POL bits in the ECCTL1 register. More... | |
| #define | CAP_ECCTL2_APWMPOL_BITS (1 << 10) |
| Defines the location of the APWMPOL bits in the ECCTL2 register. More... | |
| #define | CAP_ECCTL2_CAPAPWM_BITS (1 << 9) |
| Defines the location of the CAP/APWM bits in the ECCTL2 register. More... | |
| #define | CAP_ECCTL2_SWSYNC_BITS (1 << 8) |
| Defines the location of the SWSYNC bits in the ECCTL2 register. More... | |
| #define | CAP_ECCTL2_SYNCOSEL_BITS (3 << 6) |
| Defines the location of the SYNCO_SEL bits in the ECCTL2 register. More... | |
| #define | CAP_ECCTL2_SYNCIEN_BITS (1 << 5) |
| Defines the location of the SYNCI_EN bits in the ECCTL2 register. More... | |
| #define | CAP_ECCTL2_TSCTRSTOP_BITS (1 << 4) |
| Defines the location of the TSCTRSTOP bits in the ECCTL2 register. More... | |
| #define | CAP_ECCTL2_REARM_BITS (1 << 3) |
| Defines the location of the REARM bits in the ECCTL2 register. More... | |
| #define | CAP_ECCTL2_STOP_WRAP_BITS (3 << 1) |
| Defines the location of the STOP_WRAP bits in the ECCTL2 register. More... | |
| #define | CAP_ECCTL2_CONTONESHOT_BITS (1 << 0) |
| Defines the location of the CONT/ONESHOT bits in the ECCTL2 register. More... | |
| #define | CAP_ECCxxx_CTRCOMP_BITS (1 << 7) |
| Defines the location of the CTR=COMP bits in the ECCxxx register. More... | |
| #define | CAP_ECCxxx_CTRPRD_BITS (1 << 6) |
| Defines the location of the CTR=PRD bits in the ECCxxx register. More... | |
| #define | CAP_ECCxxx_CTROVF_BITS (1 << 5) |
| Defines the location of the CTROVF bits in the ECCxxx register. More... | |
| #define | CAP_ECCxxx_CEVT4_BITS (1 << 4) |
| Defines the location of the CEVT4 bits in the ECCxxx register. More... | |
| #define | CAP_ECCxxx_CEVT3_BITS (1 << 3) |
| Defines the location of the CEVT4 bits in the ECCxxx register. More... | |
| #define | CAP_ECCxxx_CEVT2_BITS (1 << 2) |
| Defines the location of the CEVT4 bits in the ECCxxx register. More... | |
| #define | CAP_ECCxxx_CEVT1_BITS (1 << 1) |
| Defines the location of the CEVT4 bits in the ECCxxx register. More... | |
| #define | CAP_ECCxxx_INT_BITS (1 << 0) |
| Defines the location of the INT bits in the ECCxxx register. More... | |
Typedefs | |
| typedef struct _CAP_Obj_ | CAP_Obj |
| Defines the capture (CAP) object. More... | |
| typedef struct _CAP_Obj_ * | CAP_Handle |
| Defines the capture (CAP) handle. More... | |
Enumerations | |
| enum | CAP_Int_Type_e { CAP_Int_Type_CTR_CMP = (1 << 7), CAP_Int_Type_CTR_PRD = (1 << 6), CAP_Int_Type_CTR_OVF = (1 << 5), CAP_Int_Type_CEVT4 = (1 << 4), CAP_Int_Type_CEVT3 = (1 << 3), CAP_Int_Type_CEVT2 = (1 << 2), CAP_Int_Type_CEVT1 = (1 << 1), CAP_Int_Type_Global = (1 << 0), CAP_Int_Type_All = 0x00FF } |
| Enumeration to define the capture (CAP) interrupts. More... | |
| enum | CAP_Prescale_e { CAP_Prescale_By_1 = (0 << 9), CAP_Prescale_By_2 = (1 << 9), CAP_Prescale_By_4 = (2 << 9), CAP_Prescale_By_6 = (3 << 9), CAP_Prescale_By_8 = (4 << 9), CAP_Prescale_By_10 = (5 << 9), CAP_Prescale_By_12 = (6 << 9), CAP_Prescale_By_14 = (7 << 9), CAP_Prescale_By_16 = (8 << 9), CAP_Prescale_By_18 = (9 << 9), CAP_Prescale_By_20 = (10 << 9), CAP_Prescale_By_22 = (11 << 9), CAP_Prescale_By_24 = (12 << 9), CAP_Prescale_By_26 = (13 << 9), CAP_Prescale_By_28 = (14 << 9), CAP_Prescale_By_30 = (15 << 9), CAP_Prescale_By_32 = (16 << 9), CAP_Prescale_By_34 = (17 << 9), CAP_Prescale_By_36 = (18 << 9), CAP_Prescale_By_38 = (19 << 9), CAP_Prescale_By_40 = (20 << 9), CAP_Prescale_By_42 = (21 << 9), CAP_Prescale_By_44 = (22 << 9), CAP_Prescale_By_46 = (23 << 9), CAP_Prescale_By_48 = (24 << 9), CAP_Prescale_By_50 = (25 << 9), CAP_Prescale_By_52 = (26 << 9), CAP_Prescale_By_54 = (27 << 9), CAP_Prescale_By_56 = (28 << 9), CAP_Prescale_By_58 = (29 << 9), CAP_Prescale_By_60 = (30 << 9), CAP_Prescale_By_62 = (31 << 9) } |
| Enumeration to define the capture (CAP) prescaler values. More... | |
| enum | CAP_RunMode_e { CAP_RunMode_HardStop = (0 << 14), CAP_RunMode_SoftStopAfterCycle = (1 << 14), CAP_RunMode_FreeRun = (2 << 14) } |
| Enumeration to define the pulse width modulation (PWM) run modes. More... | |
| enum | CAP_Stop_Wrap_e { CAP_Stop_Wrap_CEVT1 = (0 << 1), CAP_Stop_Wrap_CEVT2 = (1 << 1), CAP_Stop_Wrap_CEVT3 = (2 << 1), CAP_Stop_Wrap_CEVT4 = (3 << 1) } |
| Enumeration to define the capture (CAP) Stop/Wrap modes. More... | |
| enum | CAP_Event_e { CAP_Event_1 = 0, CAP_Event_2, CAP_Event_3, CAP_Event_4 } |
| Enumeration to define the capture (CAP) events. More... | |
| enum | CAP_Polarity_e { CAP_Polarity_Rising = 0, CAP_Polarity_Falling } |
| Enumeration to define the capture (CAP) event polarities. More... | |
| enum | CAP_Reset_e { CAP_Reset_Disable = 0, CAP_Reset_Enable } |
| Enumeration to define the capture (CAP) event resets. More... | |
| enum | CAP_SyncOut_e { CAP_SyncOut_SyncIn = (0 << 6), CAP_SyncOut_CTRPRD = (1 << 6), CAP_SyncOut_Disable = (2 << 6) } |
| Enumeration to define the Sync Out options. More... | |
Functions | |
| void | CAP_setModeCap (CAP_Handle capHandle) |
| Sets capture peripheral up for capture mode. More... | |
| void | CAP_setModeApwm (CAP_Handle capHandle) |
| Sets capture peripheral up for APWM mode. More... | |
| static void | CAP_clearInt (CAP_Handle capHandle, const CAP_Int_Type_e intType) |
| Clears capture (CAP) interrupt flag. More... | |
| void | CAP_disableCaptureLoad (CAP_Handle capHandle) |
| Disables loading of CAP1-4 on capture event. More... | |
| void | CAP_disableInt (CAP_Handle capHandle, const CAP_Int_Type_e intType) |
| Disables capture (CAP) interrupt source. More... | |
| void | CAP_disableSyncIn (CAP_Handle capHandle) |
| Disables counter synchronization. More... | |
| void | CAP_disableTimestampCounter (CAP_Handle capHandle) |
| Disables Time Stamp counter from running. More... | |
| void | CAP_enableCaptureLoad (CAP_Handle capHandle) |
| Enables loading of CAP1-4 on capture event. More... | |
| void | CAP_enableInt (CAP_Handle capHandle, const CAP_Int_Type_e intType) |
| Enables capture (CAP) interrupt source. More... | |
| void | CAP_enableSyncIn (CAP_Handle capHandle) |
| Enables counter synchronization. More... | |
| void | CAP_enableTimestampCounter (CAP_Handle capHandle) |
| Enables Time Stamp counter to running. More... | |
| static uint32_t | CAP_getCap1 (CAP_Handle capHandle) |
| Gets the CAP1 register value. More... | |
| static uint32_t | CAP_getCap2 (CAP_Handle capHandle) |
| Gets the CAP2 register value. More... | |
| static uint32_t | CAP_getCap3 (CAP_Handle capHandle) |
| Gets the CAP3 register value. More... | |
| static uint32_t | CAP_getCap4 (CAP_Handle capHandle) |
| Gets the CAP4 register value. More... | |
| static void | CAP_rearm (CAP_Handle capHandle) |
| (Re-)Arm the capture module More... | |
| void | CAP_setCapEvtPolarity (CAP_Handle capHandle, const CAP_Event_e event, const CAP_Polarity_e polarity) |
| Sets the capture event polarity. More... | |
| void | CAP_setCapEvtReset (CAP_Handle capHandle, const CAP_Event_e event, const CAP_Reset_e reset) |
| Sets the capture event counter reset configuration. More... | |
| void | CAP_setCapContinuous (CAP_Handle capHandle) |
| Sets up for continuous Capture. More... | |
| void | CAP_setCapOneShot (CAP_Handle capHandle) |
| Sets up for one-shot Capture. More... | |
| static void | CAP_setApwmPeriod (CAP_Handle capHandle, const uint32_t period) |
| Sets the APWM period. More... | |
| static void | CAP_setApwmCompare (CAP_Handle capHandle, const uint32_t compare) |
| Sets the APWM compare value. More... | |
| static void | CAP_setApwmShadowPeriod (CAP_Handle capHandle, const uint32_t shadowPeriod) |
| Sets the APWM shadow period. More... | |
| void | CAP_setStopWrap (CAP_Handle capHandle, const CAP_Stop_Wrap_e stopWrap) |
| Set the stop/wrap mode. More... | |
| void | CAP_setSyncOut (CAP_Handle capHandle, const CAP_SyncOut_e syncOut) |
| Set the sync out mode. More... | |
| CAP_Handle | CAP_init (void *pMemory, const size_t numBytes) |
| Initializes the capture (CAP) object handle. More... | |
| struct _CAP_Obj_ |
| #define CAP1_BASE_ADDR (0x00006A00) |
| #define CAP2_BASE_ADDR (0x00006A20) |
| #define CAP3_BASE_ADDR (0x00006A40) |
| #define CAP_ECCTL1_CAP1POL_BITS (1 << 0) |
| #define CAP_ECCTL1_CAP2POL_BITS (1 << 2) |
| #define CAP_ECCTL1_CAP3POL_BITS (1 << 4) |
| #define CAP_ECCTL1_CAP4POL_BITS (1 << 6) |
| #define CAP_ECCTL1_CAPLDEN_BITS (1 << 8) |
Defines the location of the CAPLDEN bits in the ECCTL1 register.
Definition at line 91 of file cap.h.
Referenced by CAP_disableCaptureLoad(), and CAP_enableCaptureLoad().
| #define CAP_ECCTL1_CTRRST1_BITS (1 << 1) |
| #define CAP_ECCTL1_CTRRST2_BITS (1 << 3) |
| #define CAP_ECCTL1_CTRRST3_BITS (1 << 5) |
| #define CAP_ECCTL1_CTRRST4_BITS (1 << 7) |
| #define CAP_ECCTL1_FREESOFT_BITS (3 << 14) |
| #define CAP_ECCTL1_PRESCALE_BITS (31 << 9) |
| #define CAP_ECCTL2_APWMPOL_BITS (1 << 10) |
| #define CAP_ECCTL2_CAPAPWM_BITS (1 << 9) |
Defines the location of the CAP/APWM bits in the ECCTL2 register.
Definition at line 132 of file cap.h.
Referenced by CAP_setModeApwm(), and CAP_setModeCap().
| #define CAP_ECCTL2_CONTONESHOT_BITS (1 << 0) |
Defines the location of the CONT/ONESHOT bits in the ECCTL2 register.
Definition at line 160 of file cap.h.
Referenced by CAP_setCapContinuous(), and CAP_setCapOneShot().
| #define CAP_ECCTL2_REARM_BITS (1 << 3) |
Defines the location of the REARM bits in the ECCTL2 register.
Definition at line 152 of file cap.h.
Referenced by CAP_rearm().
| #define CAP_ECCTL2_STOP_WRAP_BITS (3 << 1) |
Defines the location of the STOP_WRAP bits in the ECCTL2 register.
Definition at line 156 of file cap.h.
Referenced by CAP_setStopWrap().
| #define CAP_ECCTL2_SWSYNC_BITS (1 << 8) |
| #define CAP_ECCTL2_SYNCIEN_BITS (1 << 5) |
Defines the location of the SYNCI_EN bits in the ECCTL2 register.
Definition at line 144 of file cap.h.
Referenced by CAP_disableSyncIn(), and CAP_enableSyncIn().
| #define CAP_ECCTL2_SYNCOSEL_BITS (3 << 6) |
Defines the location of the SYNCO_SEL bits in the ECCTL2 register.
Definition at line 140 of file cap.h.
Referenced by CAP_setSyncOut().
| #define CAP_ECCTL2_TSCTRSTOP_BITS (1 << 4) |
Defines the location of the TSCTRSTOP bits in the ECCTL2 register.
Definition at line 148 of file cap.h.
Referenced by CAP_disableTimestampCounter(), and CAP_enableTimestampCounter().
| #define CAP_ECCxxx_CEVT1_BITS (1 << 1) |
| #define CAP_ECCxxx_CEVT2_BITS (1 << 2) |
| #define CAP_ECCxxx_CEVT3_BITS (1 << 3) |
| #define CAP_ECCxxx_CEVT4_BITS (1 << 4) |
| #define CAP_ECCxxx_CTRCOMP_BITS (1 << 7) |
| #define CAP_ECCxxx_CTROVF_BITS (1 << 5) |
| #define CAP_ECCxxx_CTRPRD_BITS (1 << 6) |
| #define CAP_ECCxxx_INT_BITS (1 << 0) |
| typedef struct _CAP_Obj_* CAP_Handle |
| enum CAP_Event_e |
| enum CAP_Int_Type_e |
Enumeration to define the capture (CAP) interrupts.
| enum CAP_Polarity_e |
| enum CAP_Prescale_e |
Enumeration to define the capture (CAP) prescaler values.
| enum CAP_Reset_e |
| enum CAP_RunMode_e |
| enum CAP_Stop_Wrap_e |
| enum CAP_SyncOut_e |
|
inlinestatic |
Clears capture (CAP) interrupt flag.
| [in] | capHandle | The capture (CAP) object handle |
| [in] | intType | The capture interrupt to be cleared |
Definition at line 356 of file cap.h.
References _CAP_Obj_::ECECLR.
| void CAP_disableCaptureLoad | ( | CAP_Handle | capHandle | ) |
Disables loading of CAP1-4 on capture event.
| [in] | capHandle | The capture (CAP) object handle |
Definition at line 70 of file cap.c.
References CAP_ECCTL1_CAPLDEN_BITS, and _CAP_Obj_::ECCTL1.
| void CAP_disableInt | ( | CAP_Handle | capHandle, |
| const CAP_Int_Type_e | intType | ||
| ) |
Disables capture (CAP) interrupt source.
| [in] | capHandle | The capture (CAP) object handle |
| [in] | intType | The capture interrupt type to be disabled |
Definition at line 91 of file cap.c.
References _CAP_Obj_::ECEINT.
| void CAP_disableSyncIn | ( | CAP_Handle | capHandle | ) |
Disables counter synchronization.
| [in] | capHandle | The capture (CAP) object handle |
Definition at line 80 of file cap.c.
References CAP_ECCTL2_SYNCIEN_BITS, and _CAP_Obj_::ECCTL2.
| void CAP_disableTimestampCounter | ( | CAP_Handle | capHandle | ) |
Disables Time Stamp counter from running.
| [in] | capHandle | The capture (CAP) object handle |
Definition at line 102 of file cap.c.
References CAP_ECCTL2_TSCTRSTOP_BITS, and _CAP_Obj_::ECCTL2.
| void CAP_enableCaptureLoad | ( | CAP_Handle | capHandle | ) |
Enables loading of CAP1-4 on capture event.
| [in] | capHandle | The capture (CAP) object handle |
Definition at line 112 of file cap.c.
References CAP_ECCTL1_CAPLDEN_BITS, and _CAP_Obj_::ECCTL1.
| void CAP_enableInt | ( | CAP_Handle | capHandle, |
| const CAP_Int_Type_e | intType | ||
| ) |
Enables capture (CAP) interrupt source.
| [in] | capHandle | The capture (CAP) object handle |
| [in] | intType | The capture interrupt type to be enabled |
Definition at line 122 of file cap.c.
References _CAP_Obj_::ECEINT.
| void CAP_enableSyncIn | ( | CAP_Handle | capHandle | ) |
Enables counter synchronization.
| [in] | capHandle | The capture (CAP) object handle |
Definition at line 133 of file cap.c.
References CAP_ECCTL2_SYNCIEN_BITS, and _CAP_Obj_::ECCTL2.
| void CAP_enableTimestampCounter | ( | CAP_Handle | capHandle | ) |
Enables Time Stamp counter to running.
| [in] | capHandle | The capture (CAP) object handle |
Definition at line 144 of file cap.c.
References CAP_ECCTL2_TSCTRSTOP_BITS, and _CAP_Obj_::ECCTL2.
|
inlinestatic |
Gets the CAP1 register value.
| [in] | capHandle | The capture (CAP) object handle |
Definition at line 401 of file cap.h.
References _CAP_Obj_::CAP1.
|
inlinestatic |
Gets the CAP2 register value.
| [in] | capHandle | The capture (CAP) object handle |
Definition at line 410 of file cap.h.
References _CAP_Obj_::CAP2.
|
inlinestatic |
Gets the CAP3 register value.
| [in] | capHandle | The capture (CAP) object handle |
Definition at line 419 of file cap.h.
References _CAP_Obj_::CAP3.
|
inlinestatic |
Gets the CAP4 register value.
| [in] | capHandle | The capture (CAP) object handle |
Definition at line 428 of file cap.h.
References _CAP_Obj_::CAP4.
| CAP_Handle CAP_init | ( | void * | pMemory, |
| const size_t | numBytes | ||
| ) |
|
inlinestatic |
(Re-)Arm the capture module
| [in] | capHandle | The capture (CAP) object handle |
Definition at line 437 of file cap.h.
References CAP_ECCTL2_REARM_BITS, and _CAP_Obj_::ECCTL2.
|
inlinestatic |
Sets the APWM compare value.
| [in] | capHandle | The capture (CAP) object handle |
| [in] | compare | The APWM compare value |
Definition at line 481 of file cap.h.
References _CAP_Obj_::CAP2.
|
inlinestatic |
Sets the APWM period.
| [in] | capHandle | The capture (CAP) object handle |
| [in] | period | The APWM period |
Definition at line 469 of file cap.h.
References _CAP_Obj_::CAP1.
|
inlinestatic |
Sets the APWM shadow period.
| [in] | capHandle | The capture (CAP) object handle |
| [in] | shadowPeriod | The APWM shadow period |
Definition at line 493 of file cap.h.
References _CAP_Obj_::CAP3.
| void CAP_setCapContinuous | ( | CAP_Handle | capHandle | ) |
Sets up for continuous Capture.
| [in] | capHandle | The capture (CAP) object handle |
Definition at line 180 of file cap.c.
References CAP_ECCTL2_CONTONESHOT_BITS, and _CAP_Obj_::ECCTL2.
| void CAP_setCapEvtPolarity | ( | CAP_Handle | capHandle, |
| const CAP_Event_e | event, | ||
| const CAP_Polarity_e | polarity | ||
| ) |
Sets the capture event polarity.
| [in] | capHandle | The capture (CAP) object handle |
| [in] | event | The event to configure |
| [in] | polarity | The polarity to configure the event for |
Definition at line 154 of file cap.c.
References _CAP_Obj_::ECCTL1.
| void CAP_setCapEvtReset | ( | CAP_Handle | capHandle, |
| const CAP_Event_e | event, | ||
| const CAP_Reset_e | reset | ||
| ) |
Sets the capture event counter reset configuration.
| [in] | capHandle | The capture (CAP) object handle |
| [in] | event | The event to configure |
| [in] | reset | Whether the event should reset the counter or not |
Definition at line 167 of file cap.c.
References _CAP_Obj_::ECCTL1.
| void CAP_setCapOneShot | ( | CAP_Handle | capHandle | ) |
Sets up for one-shot Capture.
| [in] | capHandle | The capture (CAP) object handle |
Definition at line 191 of file cap.c.
References CAP_ECCTL2_CONTONESHOT_BITS, and _CAP_Obj_::ECCTL2.
| void CAP_setModeApwm | ( | CAP_Handle | capHandle | ) |
Sets capture peripheral up for APWM mode.
| [in] | capHandle | The capture (CAP) object handle |
Definition at line 213 of file cap.c.
References CAP_ECCTL2_CAPAPWM_BITS, and _CAP_Obj_::ECCTL2.
| void CAP_setModeCap | ( | CAP_Handle | capHandle | ) |
Sets capture peripheral up for capture mode.
| [in] | capHandle | The capture (CAP) object handle |
Definition at line 202 of file cap.c.
References CAP_ECCTL2_CAPAPWM_BITS, and _CAP_Obj_::ECCTL2.
| void CAP_setStopWrap | ( | CAP_Handle | capHandle, |
| const CAP_Stop_Wrap_e | stopWrap | ||
| ) |
Set the stop/wrap mode.
| [in] | capHandle | The capture (CAP) object handle |
| [in] | stopWrap | The stop/wrap mode to set |
Definition at line 224 of file cap.c.
References CAP_ECCTL2_STOP_WRAP_BITS, and _CAP_Obj_::ECCTL2.
| void CAP_setSyncOut | ( | CAP_Handle | capHandle, |
| const CAP_SyncOut_e | syncOut | ||
| ) |
Set the sync out mode.
| [in] | capHandle | The capture (CAP) object handle |
| [in] | syncOut | The sync out mode to set |
Definition at line 238 of file cap.c.
References CAP_ECCTL2_SYNCOSEL_BITS, and _CAP_Obj_::ECCTL2.
1.8.9.1