MotorWare f2806x Driver API Documentation
Functions
timer.c File Reference

Contains the various functions related to the timer (TIMER) object. More...

#include "sw/drivers/timer/src/32b/f28x/f2806x/timer.h"

Go to the source code of this file.

Functions

void TIMER_clearFlag (TIMER_Handle timerHandle)
 Clears the timer (TIMER) flag. More...
 
void TIMER_disableInt (TIMER_Handle timerHandle)
 Disables the timer (TIMER) interrupt. More...
 
void TIMER_enableInt (TIMER_Handle timerHandle)
 Enables the timer (TIMER) interrupt. More...
 
TIMER_Status_e TIMER_getStatus (TIMER_Handle timerHandle)
 Gets the timer (TIMER) status. More...
 
TIMER_Handle TIMER_init (void *pMemory, const size_t numBytes)
 Initializes the timer (TIMER) object handle. More...
 
void TIMER_setDecimationFactor (TIMER_Handle timerHandle, const uint16_t decFactor)
 Sets the timer (TIMER) decimation factor. More...
 
void TIMER_setEmulationMode (TIMER_Handle timerHandle, const TIMER_EmulationMode_e mode)
 Sets the timer (TIMER) emulation mode. More...
 
void TIMER_setPreScaler (TIMER_Handle timerHandle, const uint16_t preScaler)
 Sets the timer (TIMER) prescaler. More...
 

Detailed Description

Contains the various functions related to the timer (TIMER) object.

(C) Copyright 2015, Texas Instruments, Inc.

Definition in file timer.c.