|
MotorWare f2806x Module API Documentation
|
Contains the public interface to the first-order filter (FILTER_FO) module routines. More...
Go to the source code of this file.
Data Structures | |
| struct | _FILTER_FO_ |
| Defines the first-order filter (FILTER_FO) object. More... | |
Typedefs | |
| typedef struct _FILTER_FO_ | FILTER_FO_Obj |
| Defines the first-order filter (FILTER_FO) object. More... | |
| typedef struct _FILTER_FO_Obj_ * | FILTER_FO_Handle |
| Defines the first-order filter (FILTER_FO) handle. More... | |
Functions | |
| static _iq | FILTER_FO_get_a1 (FILTER_FO_Handle handle) |
| Gets the first-order filter denominator coefficient a1. More... | |
| static _iq | FILTER_FO_get_b0 (FILTER_FO_Handle handle) |
| Gets the first-order filter numerator coefficient b0. More... | |
| static _iq | FILTER_FO_get_b1 (FILTER_FO_Handle handle) |
| Gets the first-order filter numerator coefficient b1. More... | |
| static _iq | FILTER_FO_get_x1 (FILTER_FO_Handle handle) |
| Gets the first-order filter input value at time sample n=-1. More... | |
| static _iq | FILTER_FO_get_y1 (FILTER_FO_Handle handle) |
| Gets the first-order filter output value at time sample n=-1. More... | |
| void | FILTER_FO_getDenCoeffs (FILTER_FO_Handle handle, _iq *pa1) |
| Gets the first-order filter denominator coefficients. More... | |
| void | FILTER_FO_getInitialConditions (FILTER_FO_Handle handle, _iq *px1, _iq *py1) |
| Gets the initial conditions of the first-order filter. More... | |
| void | FILTER_FO_getNumCoeffs (FILTER_FO_Handle handle, _iq *pb0, _iq *pb1) |
| Gets the first-order filter numerator coefficients. More... | |
| FILTER_FO_Handle | FILTER_FO_init (void *pMemory, const size_t numBytes) |
| Initializes the first-order filter. More... | |
| static _iq | FILTER_FO_run (FILTER_FO_Handle handle, const _iq inputValue) |
| Runs a first-order filter of the form y[n] = b0*x[n] + b1*x[n-1] - a1*y[n-1]. More... | |
| static _iq | FILTER_FO_run_form_0 (FILTER_FO_Handle handle, const _iq inputValue) |
| Runs a first-order filter of the form y[n] = b0*x[n] - a1*y[n-1]. More... | |
| static void | FILTER_FO_set_a1 (FILTER_FO_Handle handle, const _iq a1) |
| Sets the first-order filter denominator coefficient a1. More... | |
| static void | FILTER_FO_set_b0 (FILTER_FO_Handle handle, const _iq b0) |
| Sets the first-order filter numerator coefficient b0. More... | |
| static void | FILTER_FO_set_b1 (FILTER_FO_Handle handle, const _iq b1) |
| Sets the first-order filter numerator coefficient b1. More... | |
| static void | FILTER_FO_set_x1 (FILTER_FO_Handle handle, const _iq x1) |
| Sets the first-order filter input value at time sample n=-1. More... | |
| static void | FILTER_FO_set_y1 (FILTER_FO_Handle handle, const _iq y1) |
| Sets the first-order filter output value at time sample n=-1. More... | |
| void | FILTER_FO_setDenCoeffs (FILTER_FO_Handle handle, const _iq a1) |
| Sets the first-order filter denominator coefficients. More... | |
| void | FILTER_FO_setInitialConditions (FILTER_FO_Handle handle, const _iq x1, const _iq y1) |
| Sets the initial conditions of the first-order filter. More... | |
| void | FILTER_FO_setNumCoeffs (FILTER_FO_Handle handle, const _iq b0, const _iq b1) |
| Sets the first-order filter numerator coefficients. More... | |
Contains the public interface to the first-order filter (FILTER_FO) module routines.
(C) Copyright 2012, Texas Instruments, Inc.
Definition in file 32b/filter_fo.h.
1.8.9.1