MotorWare f2806x Module API Documentation
src Directory Reference

Directories

directory  32b
 
directory  float
 

Files

file  est_Flux_states.h [code]
 Contains the states for the flux estimator (EST_Flux) module routines.
 
file  est_Ls_states.h [code]
 Contains the states for the stator inductance estimator (EST_Ls) module routines.
 
file  est_Rr_states.h [code]
 Contains the public interface to the rotor resistance estimator (EST_Rr) module routines.
 
file  est_Rs_states.h [code]
 Contains the public interface to the stator resistance estimator (EST_Rs) module routines.
 
file  est_states.h [code]
 Contains the states for the estimator (EST) module routines.
 
file  est_Traj_states.h [code]
 Contains the states for the flux estimator (EST_Flux) module routines.