|
MotorWare f2806x Module API Documentation
|
Contains the public interface to the data logging (DLOG) module routines. More...
#include "sw/modules/types/src/types.h"Go to the source code of this file.
Data Structures | |
| struct | _DLOG_4CH_ |
| Defines the data logging (DLOG) object. More... | |
Macros | |
| #define | DLOG_4CH_DEFAULTS |
| Defines the default initalization for the DLOG object. More... | |
Typedefs | |
| typedef struct _DLOG_4CH_ | DLOG_4CH |
| Defines the data logging (DLOG) object. More... | |
| typedef struct _DLOG_4CH_Obj_ * | DLOG_4CH_handle |
| Defines the DLOG handle. More... | |
Functions | |
| void | DLOG_4CH_init (void *ptr) |
| Initializes the data logger. More... | |
| void | DLOG_4CH_update (void *ptr) |
| Updates the data logger. More... | |
Variables | |
| DLOG_4CH | dlog |
| Defines the DLOG object. More... | |
| int16_t | DlogCh1 |
| Defines DLOG channel 1. More... | |
| int16_t | DlogCh2 |
| Defines DLOG channel 2. More... | |
| int16_t | DlogCh3 |
| Defines DLOG channel 3. More... | |
| int16_t | DlogCh4 |
| Defines DLOG channel 4. More... | |
Contains the public interface to the data logging (DLOG) module routines.
(C) Copyright 2011, Texas Instruments, Inc.
Definition in file dlog4ch.h.
1.8.9.1