|
MotorWare f2806x Module API Documentation
|
Go to the source code of this file.
Functions | |
| void | HAL_AdcCalChanSelect (HAL_Handle handle, const ADC_SocChanNumber_e chanNumber) |
| Selects the analog channel used for calibration. More... | |
| uint16_t | HAL_AdcCalConversion (HAL_Handle handle) |
| Reads the converted value from the selected calibration channel. More... | |
| void | HAL_AdcOffsetSelfCal (HAL_Handle handle) |
| Executes the offset calibration of the ADC. More... | |
| void | HAL_cal (HAL_Handle handle) |
| Executes calibration routines. More... | |
| void | HAL_disableGlobalInts (HAL_Handle handle) |
| Disables global interrupts. More... | |
| void | HAL_disableWdog (HAL_Handle halHandle) |
| Disables the watch dog. More... | |
| void | HAL_enableAdcInts (HAL_Handle handle) |
| Enables the ADC interrupts. More... | |
| void | HAL_enableDebugInt (HAL_Handle handle) |
| Enables the debug interrupt. More... | |
| void | HAL_enableDrv (HAL_Handle handle) |
| Enables the 8301 device. More... | |
| void | HAL_enableGlobalInts (HAL_Handle handle) |
| Enables global interrupts. More... | |
| void | HAL_enablePwmInt (HAL_Handle handle) |
| Enables the PWM interrupt. More... | |
| HAL_Handle | HAL_init (void *pMemory, const size_t numBytes) |
| Initializes the hardware abstraction layer (HAL) object. More... | |
| void | HAL_OscTempComp (HAL_Handle handle) |
| Executes the oscillator 1 and 2 calibration functions. More... | |
| void | HAL_osc1Comp (HAL_Handle handle, const int16_t sensorSample) |
| Executes the oscillator 1 calibration based on input sample. More... | |
| void | HAL_osc2Comp (HAL_Handle handle, const int16_t sensorSample) |
| Executes the oscillator 2 calibration based on input sample. More... | |
| uint16_t | HAL_computeOscTrimValue (int16_t coarse, int16_t fine) |
| void | HAL_setParams (HAL_Handle handle, const USER_Params *pUserParams) |
| Sets the hardware abstraction layer parameters. More... | |
| void | HAL_setupAdcs (HAL_Handle handle) |
| Sets up the ADCs (Analog to Digital Converters) More... | |
| void | HAL_setupClks (HAL_Handle handle) |
| Sets up the clocks. More... | |
| void | HAL_setupFlash (HAL_Handle handle) |
| Sets up the FLASH. More... | |
| void | HAL_setupFaults (HAL_Handle handle) |
| Configures the fault protection logic. More... | |
| void | HAL_setupGate (HAL_Handle handle) |
| Sets up the GATE object. More... | |
| void | HAL_setupGpios (HAL_Handle handle) |
| Sets up the GPIO (General Purpose I/O) pins. More... | |
| void | HAL_setupPie (HAL_Handle handle) |
| Sets up the PIE (Peripheral Interrupt Expansion) More... | |
| void | HAL_setupPeripheralClks (HAL_Handle handle) |
| Sets up the peripheral clocks. More... | |
| void | HAL_setupPll (HAL_Handle handle, const PLL_ClkFreq_e clkFreq) |
| Sets up the PLL (Phase Lock Loop) More... | |
| void | HAL_setupPwms (HAL_Handle handle, const float_t systemFreq_MHz, const float_t pwmPeriod_usec, const uint_least16_t numPwmTicksPerIsrTick) |
| Sets up the PWMs (Pulse Width Modulators) More... | |
| void | HAL_setupSpiA (HAL_Handle handle) |
| Sets up the spiA peripheral. More... | |
| void | HAL_setupSpiB (HAL_Handle handle) |
| Sets up the spiB peripheral. More... | |
| void | HAL_setupPwmDacs (HAL_Handle handle, const float_t systemFreq_MHz, const float_t dacFreq_kHz) |
| Sets up the PWM DACs (Pulse Width Modulator Digital to Analof Converters) More... | |
| void | HAL_setupQEP (QEP_Handle qepHandle, const USER_Params *pUserParams, const uint32_t unitTimerFreq_Hz) |
| Sets up the QEP peripheral (Quadrature Encoder) More... | |
| void | HAL_setupTimers (HAL_Handle handle, const float_t systemFreq_MHz) |
| Sets up the timers. More... | |
| void | HAL_writeDrvData (HAL_Handle handle, DRV_SPI_8301_Vars_t *Spi_8301_Vars) |
| Writes data to the driver. More... | |
| void | HAL_readDrvData (HAL_Handle handle, DRV_SPI_8301_Vars_t *Spi_8301_Vars) |
| Reads data from the driver. More... | |
| void | HAL_setupDrvSpi (HAL_Handle handle, DRV_SPI_8301_Vars_t *Spi_8301_Vars) |
| Sets up the SPI interface for the driver. More... | |
1.8.9.1