|
| void | HAL_cal (HAL_Handle handle) |
| | Executes calibration routines. More...
|
| |
| void | HAL_OscTempComp (HAL_Handle handle) |
| | Executes the oscillator 1 and 2 calibration functions. More...
|
| |
| void | HAL_osc1Comp (HAL_Handle handle, const int16_t sensorSample) |
| | Executes the oscillator 1 calibration based on input sample. More...
|
| |
| void | HAL_osc2Comp (HAL_Handle handle, const int16_t sensorSample) |
| | Executes the oscillator 2 calibration based on input sample. More...
|
| |
| uint16_t | HAL_getOscTrimValue (int16_t coarse, int16_t fine) |
| | Converts coarse and fine oscillator trim values into a single 16bit word value. More...
|
| |
| void | HAL_AdcOffsetSelfCal (HAL_Handle handle) |
| | Executes the offset calibration of the ADC. More...
|
| |
| void | HAL_AdcCalChanSelect (HAL_Handle handle, const ADC_SocChanNumber_e chanNumber) |
| | Selects the analog channel used for calibration. More...
|
| |
| uint16_t | HAL_AdcCalConversion (HAL_Handle handle) |
| | Reads the converted value from the selected calibration channel. More...
|
| |
| void | HAL_disableWdog (HAL_Handle halHandle) |
| | Disables the watch dog. More...
|
| |
| void | HAL_disableGlobalInts (HAL_Handle handle) |
| | Disables global interrupts. More...
|
| |
| void | HAL_enableAdcInts (HAL_Handle handle) |
| | Enables the ADC interrupts. More...
|
| |
| void | HAL_enableDebugInt (HAL_Handle handle) |
| | Enables the debug interrupt. More...
|
| |
| void | HAL_enableGlobalInts (HAL_Handle handle) |
| | Enables global interrupts. More...
|
| |
| void | HAL_enablePwmInt (HAL_Handle handle) |
| | Enables the PWM interrupt. More...
|
| |
| void | HAL_setupFaults (HAL_Handle handle) |
| | Configures the fault protection logic. More...
|
| |
| HAL_Handle | HAL_init (void *pMemory, const size_t numBytes) |
| | Initializes the hardware abstraction layer (HAL) object. More...
|
| |
| void | HAL_setParams (HAL_Handle handle, const USER_Params *pUserParams) |
| | Sets the hardware abstraction layer parameters. More...
|
| |
| void | HAL_setupAdcs (HAL_Handle handle) |
| | Sets up the ADCs (Analog to Digital Converters) More...
|
| |
| void | HAL_setupClks (HAL_Handle handle) |
| | Sets up the clocks. More...
|
| |
| void | HAL_setupFlash (HAL_Handle handle) |
| | Sets up the FLASH. More...
|
| |
| void | HAL_setupGpios (HAL_Handle handle) |
| | Sets up the GPIO (General Purpose I/O) pins. More...
|
| |
| void | HAL_setupPie (HAL_Handle handle) |
| | Sets up the PIE (Peripheral Interrupt Expansion) More...
|
| |
| void | HAL_setupPeripheralClks (HAL_Handle handle) |
| | Sets up the peripheral clocks. More...
|
| |
| void | HAL_setupPll (HAL_Handle handle, const PLL_ClkFreq_e clkFreq) |
| | Sets up the PLL (Phase Lock Loop) More...
|
| |
| void | HAL_setupPwms (HAL_Handle handle, const float_t systemFreq_MHz, const float_t pwmPeriod_usec, const uint_least16_t numPwmTicksPerIsrTick) |
| | Sets up the PWMs (Pulse Width Modulators) More...
|
| |
| void | HAL_setupSpiA (HAL_Handle handle) |
| | Sets up the spiA peripheral. More...
|
| |
| void | HAL_setupPwmDacs (HAL_Handle handle) |
| | Sets up the PWM DACs (Pulse Width Modulator Digital to Analof Converters) More...
|
| |
| void | HAL_setupTimers (HAL_Handle handle, const float_t systemFreq_MHz) |
| | Sets up the timers. More...
|
| |