1 #ifndef _EST_LS_STATES_H_
2 #define _EST_LS_STATES_H_
71 #endif // end of _EST_LS_STATES_H_ definition
the number of estimator error codes
inductance shift overflow error code
the fine estimation state
the number of stator inductance estimator states
the coarse estimation state
EST_Ls_ErrorCode_e
Enumeration for the stator inductance estimator error codes.
EST_Ls_State_e
Enumeration for the stator inductance estimator states.