MotorWare f2806x Module API Documentation
Enumerations
est_Rr_states.h File Reference

Contains the public interface to the rotor resistance estimator (EST_Rr) module routines. More...

Go to the source code of this file.

Enumerations

enum  EST_Rr_State_e {
  EST_Rr_State_Error =0, EST_Rr_State_Idle, EST_Rr_State_RampUp, EST_Rr_State_Coarse,
  EST_Rr_State_Fine, EST_Rr_State_Done, EST_Rr_numStates
}
 Enumeration for the rotor resistance estimator states. More...
 

Detailed Description

Contains the public interface to the rotor resistance estimator (EST_Rr) module routines.

(C) Copyright 2014, Texas Instruments, Inc.

Definition in file est_Rr_states.h.