|
MotorWare f2806x Module API Documentation
|
Contains the public interface to the calibrator (CAL) module routines. More...
#include "sw/modules/types/src/types.h"#include "sw/modules/cal/src/cal_states.h"#include "sw/modules/hal/src/float/hal_data.h"#include "sw/modules/math/src/float/math.h"#include "sw/modules/offset/src/float/offset.h"#include "sw/modules/user/src/float/userParams.h"#include "user.h"Go to the source code of this file.
Data Structures | |
| struct | _CAL_Obj_ |
| Defines the calibrator (CAL) object. More... | |
Typedefs | |
| typedef struct _CAL_Obj_ | CAL_Obj |
| Defines the calibrator (CAL) object. More... | |
| typedef struct _CAL_Obj_ * | CAL_Handle |
| Defines the CAL handle. More... | |
Functions | |
| static void | CAL_disable (CAL_Handle handle) |
| Disables the calibrator (CAL) module. More... | |
| static void | CAL_enable (CAL_Handle handle) |
| Enables the calibrator (CAL) module. More... | |
| static int_least32_t | CAL_getCount_state (CAL_Handle handle) |
| Gets the state count value. More... | |
| static bool | CAL_getFlag_enable (CAL_Handle handle) |
| Gets the value of the enable flag. More... | |
| static bool | CAL_getFlag_enableAdcOffset (CAL_Handle handle) |
| Gets the value of the enable ADC offset flag. More... | |
| static OFFSET_Handle * | CAL_getOffsetHandleAddr_I (CAL_Handle handle) |
| Gets the current offset handle address. More... | |
| static OFFSET_Handle * | CAL_getOffsetHandleAddr_V (CAL_Handle handle) |
| Gets the voltage offset handle address. More... | |
| static float_t | CAL_getOffsetValue_I (CAL_Handle handle, const uint_least8_t sensorNumber) |
| Gets the current offset value. More... | |
| static float_t | CAL_getOffsetValue_V (CAL_Handle handle, const uint_least8_t sensorNumber) |
| Gets the voltage offset value. More... | |
| static CAL_State_e | CAL_getState (CAL_Handle handle) |
| Gets the calibration state. More... | |
| static int_least32_t | CAL_getWaitTime (CAL_Handle handle, const CAL_State_e state) |
| Gets the wait time for a given state. More... | |
| static void | CAL_incrCounter_state (CAL_Handle handle) |
| Increments the state count value. More... | |
| CAL_Handle | CAL_init (void *pMemory, const size_t numBytes) |
| Initializes the calibrator (CAL) module. More... | |
| static bool | CAL_isEnabled (CAL_Handle handle) |
| Returns a boolean value denoting if the module is enabled (true) or not (false) More... | |
| static bool | CAL_isError (CAL_Handle handle) |
| Determines if there is a calibrator error. More... | |
| static bool | CAL_isIdle (CAL_Handle handle) |
| Determines if the calibrator is in the idle state. More... | |
| static bool | CAL_isNotIdle (CAL_Handle handle) |
| Determines if the calibrator is not in the idle state. More... | |
| void | CAL_reset (CAL_Handle handle) |
| Resets the calibrator. More... | |
| static void | CAL_resetCounter_state (CAL_Handle handle) |
| Resets the state count value. More... | |
| static void | CAL_setCount_state (CAL_Handle handle, const int_least32_t count) |
| Sets the state count value. More... | |
| static void | CAL_setFlag_enable (CAL_Handle handle, const bool value) |
| Sets the value of the enable flag. More... | |
| static void | CAL_setFlag_enableAdcOffset (CAL_Handle handle, const bool value) |
| Sets the value of the enable ADC offset flag. More... | |
| void | CAL_setParams (CAL_Handle handle, const USER_Params *pUserParams) |
| Sets the parameters. More... | |
| static void | CAL_setState (CAL_Handle handle, const CAL_State_e state) |
| Sets the calibration state. More... | |
| static void | CAL_setWaitTime (CAL_Handle handle, const CAL_State_e state, const int_least32_t waitTime) |
| Sets the wait time for a given state. More... | |
| void | CAL_setWaitTimes (CAL_Handle handle, const int_least32_t *pWaitTimes) |
| Sets the wait times. More... | |
| static void | CAL_setup (CAL_Handle handle) |
| Sets up the calibrator (CAL) module. More... | |
| static void | CAL_run (CAL_Handle handle, const HAL_AdcData_t *pAdcData) |
| Runs the calibrator (CAL) module. More... | |
| bool | CAL_updateState (CAL_Handle handle) |
| Updates the calibrator (CAL) state. More... | |
Contains the public interface to the calibrator (CAL) module routines.
(C) Copyright 2014, Texas Instruments, Inc.
Definition in file float/cal.h.
|
inlinestatic |
Disables the calibrator (CAL) module.
| [in] | handle | The calibrator (CAL) handle |
Definition at line 86 of file float/cal.h.
References _CAL_Obj_::flag_enable.
|
inlinestatic |
Enables the calibrator (CAL) module.
| [in] | handle | The calibrator (CAL) handle |
Definition at line 98 of file float/cal.h.
References _CAL_Obj_::flag_enable.
|
inlinestatic |
Gets the state count value.
| [in] | handle | The calibrator (CAL) handle |
Definition at line 111 of file float/cal.h.
References _CAL_Obj_::counter_state.
|
inlinestatic |
Gets the value of the enable flag.
| [in] | handle | The calibrator (CAL) handle |
Definition at line 122 of file float/cal.h.
References _CAL_Obj_::flag_enable.
|
inlinestatic |
Gets the value of the enable ADC offset flag.
| [in] | handle | The calibrator (CAL) handle |
Definition at line 133 of file float/cal.h.
References _CAL_Obj_::flag_enableAdcOffset.
|
inlinestatic |
Gets the current offset handle address.
| [in] | handle | The calibrator (CAL) handle |
Definition at line 144 of file float/cal.h.
References _CAL_Obj_::offsetHandle_I.
|
inlinestatic |
Gets the voltage offset handle address.
| [in] | handle | The calibrator (CAL) handle |
Definition at line 155 of file float/cal.h.
References _CAL_Obj_::offsetHandle_V.
|
inlinestatic |
Gets the current offset value.
| [in] | handle | The calibrator (CAL) handle |
| [in] | sensorNumber | The sensor number |
Definition at line 167 of file float/cal.h.
References OFFSET_getOffset(), and _CAL_Obj_::offsetHandle_I.
|
inlinestatic |
Gets the voltage offset value.
| [in] | handle | The calibrator (CAL) handle |
| [in] | sensorNumber | The sensor number |
Definition at line 182 of file float/cal.h.
References OFFSET_getOffset(), and _CAL_Obj_::offsetHandle_V.
|
inlinestatic |
Gets the calibration state.
| [in] | handle | The calibrator (CAL) handle |
Definition at line 196 of file float/cal.h.
References _CAL_Obj_::state.
Referenced by CAL_isError(), CAL_isIdle(), CAL_isNotIdle(), and CAL_run().
|
inlinestatic |
Gets the wait time for a given state.
| [in] | handle | The calibrator (CAL) handle |
| [in] | state | The state |
Definition at line 208 of file float/cal.h.
References _CAL_Obj_::waitTimes.
|
inlinestatic |
Increments the state count value.
| [in] | handle | The calibrator (CAL) handle |
Definition at line 218 of file float/cal.h.
References _CAL_Obj_::counter_state.
Referenced by CAL_run().
|
inlinestatic |
Returns a boolean value denoting if the module is enabled (true) or not (false)
| [in] | handle | The calibrator (CAL) handle |
Definition at line 249 of file float/cal.h.
References _CAL_Obj_::flag_enable.
|
inlinestatic |
Determines if there is a calibrator error.
| [in] | handle | The calibrator (CAL) handle |
Definition at line 260 of file float/cal.h.
References CAL_getState(), CAL_State_Error, and _CAL_Obj_::state.
|
inlinestatic |
Determines if the calibrator is in the idle state.
| [in] | handle | The calibrator (CAL) handle |
Definition at line 279 of file float/cal.h.
References CAL_getState(), CAL_State_Idle, and _CAL_Obj_::state.
|
inlinestatic |
Determines if the calibrator is not in the idle state.
| [in] | handle | The calibrator (CAL) handle |
Definition at line 296 of file float/cal.h.
References CAL_getState(), CAL_State_Idle, and _CAL_Obj_::state.
|
inlinestatic |
Resets the state count value.
| [in] | handle | The calibrator (CAL) handle |
Definition at line 317 of file float/cal.h.
References _CAL_Obj_::counter_state.
|
inlinestatic |
Runs the calibrator (CAL) module.
| [in] | handle | The calibrator (CAL) handle |
Definition at line 417 of file float/cal.h.
References CAL_getState(), CAL_incrCounter_state(), CAL_State_AdcOffset, _HAL_AdcData_t_::I_A, OFFSET_run(), _CAL_Obj_::offsetHandle_I, _CAL_Obj_::offsetHandle_V, _CAL_Obj_::state, _HAL_AdcData_t_::V_V, and _MATH_vec3_::value.
|
inlinestatic |
Sets the value of the enable flag.
| [in] | handle | The calibrator (CAL) handle |
| [in] | value | The desired flag value |
Definition at line 343 of file float/cal.h.
References _CAL_Obj_::flag_enable.
|
inlinestatic |
Sets the value of the enable ADC offset flag.
| [in] | handle | The calibrator (CAL) handle |
| [in] | value | The desired flag value |
Definition at line 356 of file float/cal.h.
References _CAL_Obj_::flag_enableAdcOffset.
|
inlinestatic |
Sets the calibration state.
| [in] | handle | The calibrator (CAL) handle |
| [in] | state | The calibration state |
Definition at line 376 of file float/cal.h.
References _CAL_Obj_::state.
|
inlinestatic |
Sets up the calibrator (CAL) module.
| [in] | handle | The calibrator (CAL) handle |
Definition at line 408 of file float/cal.h.
1.8.9.1