|
MotorWare f2806x Module API Documentation
|
Portable C fixed point code. These functions define the Clarke transform module routines. More...
#include "sw/modules/clarke/src/float/clarke.h"Go to the source code of this file.
Functions | |
| CLARKE_Handle | CLARKE_init (void *pMemory, const size_t numBytes) |
| Initializes the Clarke transform module. More... | |
Portable C fixed point code. These functions define the Clarke transform module routines.
(C) Copyright 2014, Texas Instruments, Inc.
Definition in file float/clarke.c.
1.8.9.1