|
MotorWare f2806x Module API Documentation
|
Defines the structures for the CTRL object. More...
#include "sw/modules/types/src/types.h"#include "sw/modules/ctrl/src/ctrl_states.h"#include "sw/modules/math/src/float/math.h"#include "sw/modules/motor/src/float/motor.h"#include "sw/modules/pi/src/float/pi.h"Go to the source code of this file.
Data Structures | |
| struct | _CTRL_Version_ |
| Defines the controller (CTRL) version number. More... | |
| struct | _CTRL_Obj_ |
| Defines the controller (CTRL) object. More... | |
Macros | |
| #define | CTRL_MAJOR_RELEASE_NUMBER (2u) |
| Defines the major release number. More... | |
| #define | CTRL_MINOR_RELEASE_NUMBER (0u) |
| Defines the major release number. More... | |
| #define | CTRL_NUM_CONTROLLERS (2) |
| Defines the number of controllers. More... | |
Typedefs | |
| typedef struct _CTRL_Version_ | CTRL_Version |
| Defines the controller (CTRL) version number. More... | |
| typedef struct _CTRL_Obj_ | CTRL_Obj |
| Defines the controller (CTRL) object. More... | |
| typedef struct _CTRL_Obj_ * | CTRL_Handle |
| Defines the CTRL handle. More... | |
Enumerations | |
| enum | CTRL_ErrorCode_e { CTRL_ErrorCode_NoError =0, CTRL_ErrorCode_IdClip, CTRL_ErrorCode_EstError, CTRL_numErrorCodes, CTRL_ErrorCode_NoError =0, CTRL_ErrorCode_IdClip, CTRL_ErrorCode_EstError, CTRL_numErrorCodes } |
| Enumeration for the error codes. More... | |
| enum | CTRL_TargetProc_e { CTRL_TargetProc_2806x =0, CTRL_TargetProc_2805x, CTRL_TargetProc_2803x, CTRL_TargetProc_2802x, CTRL_TargetProc_Unknown, CTRL_TargetProc_2806x =0, CTRL_TargetProc_2805x, CTRL_TargetProc_2803x, CTRL_TargetProc_2802x } |
| Enumeration for the target processors. More... | |
| enum | CTRL_Type_e { CTRL_Type_PID_spd =0, CTRL_Type_PID_Id, CTRL_Type_PID_Iq, CTRL_Type_PI_spd =0, CTRL_Type_PI_Id, CTRL_Type_PI_Iq } |
| Enumeration for the controller (CTRL) types. More... | |
Defines the structures for the CTRL object.
(C) Copyright 2014, Texas Instruments, Inc.
Definition in file float/ctrl_obj.h.
1.8.9.1