Go to the source code of this file.
|
| static float_t | IPARK_getCosTh (IPARK_Handle handle) |
| | Gets the cosine of the angle between the d,q and the alpha,beta coordinate systems. More...
|
| |
| static void | IPARK_getPhasor (IPARK_Handle handle, MATH_vec2 *pPhasor) |
| | Gets the cosine/sine phasor for the inverse Park transform. More...
|
| |
| static float_t | IPARK_getSinTh (IPARK_Handle handle) |
| | Gets the sine of the angle between the d,q and the alpha,beta coordinate systems. More...
|
| |
| IPARK_Handle | IPARK_init (void *pMemory, const size_t numBytes) |
| | Initializes the inverse Park transform module. More...
|
| |
| static void | IPARK_run (IPARK_Handle handle, const MATH_vec2 *pInVec, MATH_vec2 *pOutVec) |
| | Runs the inverse Park transform module. More...
|
| |
| static void | IPARK_setCosTh (IPARK_Handle handle, const float_t cosTh) |
| | Sets the cosine of the angle between the d,q and the alpha,beta coordinate systems. More...
|
| |
| static void | IPARK_setPhasor (IPARK_Handle handle, const MATH_vec2 *pPhasor) |
| | Sets the cosine/sine phasor for the inverse Park transform. More...
|
| |
| static void | IPARK_setSinTh (IPARK_Handle handle, const float_t sinTh) |
| | Sets the sine of the angle between the d,q and the alpha,beta coordinate systems. More...
|
| |
| static void | IPARK_setup (IPARK_Handle handle, const float_t Th) |
| | Sets up the inverse Park transform module. More...
|
| |
Gets the cosine of the angle between the d,q and the alpha,beta coordinate systems.
- Parameters
-
| [in] | handle | The inverse Park transform handle |
- Returns
- The cosine of the angle
Definition at line 98 of file float/ipark.h.
References _IPARK_Obj_::cosTh.
Gets the sine of the angle between the d,q and the alpha,beta coordinate systems.
- Parameters
-
| [in] | handle | The inverse Park transform handle return The sine of the angle |
Definition at line 123 of file float/ipark.h.
References _IPARK_Obj_::sinTh.