104 const float_t iqFullScaleVoltage_V,
105 const float_t iqFullScaleFreq_Hz,
114 #endif // end of _FSTART_H_ definition
struct _FStart_Handle_ * FStart_Handle
Defines the FStart handle.
Contains the public interface to the types definitions.
_iq FStart_run(FStart_Handle handle, const _iq fm_Hz, const _iq flux_VpHz)
Runs the flying start module.
FStart_Handle FStart_init(void)
Initializes the flying start module.
void FStart_setParams(FStart_Handle handle, const float_t iqFullScaleVoltage_V, const float_t iqFullScaleFreq_Hz, const float_t estFreq_Hz, const float_t maxFlux_VpHz)
Sets the parameters for the flying start module.
float float_t
Defines the portable data type for 32 bit, signed floating-point data.