|
MotorWare f2806x Module API Documentation
|
Public interface, object, and function definitions related to the SpinTAC Position Plan component. More...
#include "spintac_version.h"Go to the source code of this file.
Data Structures | |
| struct | ST_PlanError_t |
| Defines the ST_PlanError_t data. More... | |
| struct | ST_PosPlan_t |
| Defines the ST_PosPlan_t data. More... | |
Macros | |
| #define | ST_POS_PLAN_ACT_DWORDS (5) |
| Defines the amount of memory that needs to be allocated for each component. More... | |
| #define | ST_POS_PLAN_COND_DWORDS (3) |
| Each configured Condition takes 3 double words of memory. More... | |
| #define | ST_POS_PLAN_VAR_DWORDS (2) |
| Each configured Variable takes 2 double words of memory. More... | |
| #define | ST_POS_PLAN_TRAN_DWORDS (7) |
| Each configured Transition takes 7 double words of memory. More... | |
| #define | ST_POS_PLAN_STATE_DWORDS (7) |
| Each configured State takes 7 double words of memory. More... | |
| #define | __ST_PLAN_ENUM__ |
| #define | __ST_PLAN_ERROR__ |
Typedefs | |
| typedef struct _ST_POSPLAN_Handle_ * | ST_POSPLAN_Handle |
Functions | |
| static void | STPOSPLAN_getPositionStep_mrev (ST_POSPLAN_Handle handle, int32_t *posStepInt_mrev, _iq24 *posStepFrac_mrev) |
| Gets the Position Step (posStepInt_mrev, posStepFrac_mrev) for SpinTAC Position Plan. More... | |
| static _iq24 | STPOSPLAN_getVelocityLimit (ST_POSPLAN_Handle handle) |
| Gets the Velocity Limit (VelLim) for SpinTAC Position Plan. More... | |
| static _iq24 | STPOSPLAN_getAccelerationLimit (ST_POSPLAN_Handle handle) |
| Gets the Acceleration Limit (AccLim) for SpinTAC Position Plan. More... | |
| static _iq24 | STPOSPLAN_getDecelerationLimit (ST_POSPLAN_Handle handle) |
| Gets the Deceleration Limit (DecLim) for SpinTAC Position Plan. More... | |
| static _iq20 | STPOSPLAN_getJerkLimit (ST_POSPLAN_Handle handle) |
| Gets the Jerk Limit (JrkLim) for SpinTAC Position Plan. More... | |
| static void | STPOSPLAN_setEnable (ST_POSPLAN_Handle handle, bool enb) |
| Sets the Enable signal (ENB) for SpinTAC Position Plan. More... | |
| static bool | STPOSPLAN_getEnable (ST_POSPLAN_Handle handle) |
| Gets the Enable signal (ENB) for SpinTAC Position Plan. More... | |
| static void | STPOSPLAN_setReset (ST_POSPLAN_Handle handle, bool res) |
| Sets the Reset signal (RES) for SpinTAC Position Plan. More... | |
| static bool | STPOSPLAN_getReset (ST_POSPLAN_Handle handle) |
| Gets the Reset signal (RES) for SpinTAC Position Plan. More... | |
| static ST_PlanStatus_e | STPOSPLAN_getStatus (ST_POSPLAN_Handle handle) |
| Gets the Status value (STATUS) for SpinTAC Position Plan. More... | |
| static uint16_t | STPOSPLAN_getCurrentState (ST_POSPLAN_Handle handle) |
| Gets the Current State (CurState) for SpinTAC Position Plan. More... | |
| static uint16_t | STPOSPLAN_getCurrentTransition (ST_POSPLAN_Handle handle) |
| Gets the Current Transition (CurTran) for SpinTAC Position Plan. More... | |
| static ST_PlanFsmState_e | STPOSPLAN_getFsmState (ST_POSPLAN_Handle handle) |
| Gets the State Machine State (FsmState) for SpinTAC Position Plan. More... | |
| static int32_t | STPOSPLAN_getCurrentTimerValue_tick (ST_POSPLAN_Handle handle) |
| Gets the Current Time Value (Timer_tick) for SpinTAC Position Plan. More... | |
| static uint16_t | STPOSPLAN_getCfgError (ST_POSPLAN_Handle handle, uint16_t *ERR_idx, uint16_t *ERR_code) |
| Gets the Configuration Error for SpinTAC Position Plan. More... | |
| static uint16_t | STPOSPLAN_getErrorID (ST_POSPLAN_Handle handle) |
| Gets the Error value (ERR_ID) for SpinTAC Position Plan. More... | |
| void | STPOSPLAN_getCfgStateNum (ST_POSPLAN_Handle handle, uint16_t *StateNum) |
| Returns the number of configured States in SpinTAC Position Plan. More... | |
| void | STPOSPLAN_getCfgVarNum (ST_POSPLAN_Handle handle, uint16_t *VarNum) |
| Returns the number of configured Variables in SpinTAC Position Plan. More... | |
| void | STPOSPLAN_getCfgCondNum (ST_POSPLAN_Handle handle, uint16_t *CondNum) |
| Returns the number of configured Conditions in SpinTAC Position Plan. More... | |
| void | STPOSPLAN_getCfgTranNum (ST_POSPLAN_Handle handle, uint16_t *TranNum) |
| Returns the number of configured Transitions in SpinTAC Position Plan. More... | |
| void | STPOSPLAN_getCfgActNum (ST_POSPLAN_Handle handle, uint16_t *ActNum) |
| Returns the number of configured Actions in SpinTAC Position Plan. More... | |
| void | STPOSPLAN_addCfgCond (ST_POSPLAN_Handle handle, uint16_t VarIdx, ST_PlanComp_e Comp, _iq24 Value1, _iq24 Value2) |
| Adds a Condition to the SpinTAC Position Plan configuration. More... | |
| void | STPOSPLAN_delCfgCond (ST_POSPLAN_Handle handle, uint16_t CondIdx) |
| Deletes a Condition from the SpinTAC Position Plan configuration. More... | |
| void | STPOSPLAN_setCfgCond (ST_POSPLAN_Handle handle, uint16_t CondIdx, uint16_t VarIdx, ST_PlanComp_e Comp, _iq24 Value1, _iq24 Value2) |
| Modifies a Condition in the SpinTAC Position Plan configuration. More... | |
| void | STPOSPLAN_getCfgCond (ST_POSPLAN_Handle handle, uint16_t CondIdx, uint16_t *VarIdx, ST_PlanComp_e *Comp, _iq24 *Value1, _iq24 *Value2) |
| Returns a Condition from the SpinTAC Position Plan configuration. More... | |
| void | STPOSPLAN_addCfgVarCond (ST_POSPLAN_Handle handle, uint16_t VarIdx1, uint16_t VarIdx2, ST_PlanComp_e Comp) |
| Adds a Variable Condition to the SpinTAC Position Plan configuration. More... | |
| void | STPOSPLAN_delCfgVarCond (ST_POSPLAN_Handle handle, uint16_t CondIdx) |
| Deletes a Variable Condition from the SpinTAC Position Plan configuration. More... | |
| void | STPOSPLAN_setCfgVarCond (ST_POSPLAN_Handle handle, uint16_t CondIdx, uint16_t VarIdx1, uint16_t VarIdx2, ST_PlanComp_e Comp) |
| Modifies a Variable Condition to the SpinTAC Position Plan configuration. More... | |
| void | STPOSPLAN_getCfgVarCond (ST_POSPLAN_Handle handle, uint16_t CondIdx, uint16_t *VarIdx1, uint16_t *VarIdx2, ST_PlanComp_e *Comp) |
| Returns a Variable Condition from the SpinTAC Position Plan configuration. More... | |
| void | STPOSPLAN_addCfgTran (ST_POSPLAN_Handle handle, uint16_t FromState, uint16_t ToState, ST_PlanCond_e AndOr, uint16_t CondIdx1, uint16_t CondIdx2, _iq24 VelLim, _iq24 AccLim, _iq24 DecLim, _iq20 JrkLim) |
| Adds a Transition to the SpinTAC Position Plan configuration. More... | |
| void | STPOSPLAN_delCfgTran (ST_POSPLAN_Handle handle, uint16_t TranIdx) |
| Deletes a Transition from the SpinTAC Position Plan configuration. More... | |
| void | STPOSPLAN_setCfgTran (ST_POSPLAN_Handle handle, uint16_t TranIdx, uint16_t FromState, uint16_t ToState, ST_PlanCond_e AndOr, uint16_t CondIdx1, uint16_t CondIdx2, _iq24 VelLim, _iq24 AccLim, _iq24 DecLim, _iq20 JrkLim) |
| Modifies a Transition in the SpinTAC Position Plan configuration. More... | |
| void | STPOSPLAN_getCfgTran (ST_POSPLAN_Handle handle, uint16_t TranIdx, uint16_t *FromState, uint16_t *ToState, ST_PlanCond_e *AndOr, uint16_t *CondIdx1, uint16_t *CondIdx2, _iq24 *VelLim, _iq24 *AccLim, _iq24 *DecLim, _iq20 *JrkLim) |
| Get a Transition from the SpinTAC Position Plan configuration. More... | |
| void | STPOSPLAN_addCfgAct (ST_POSPLAN_Handle handle, uint16_t State, ST_PlanCond_e AndOr, uint16_t CondIdx1, uint16_t CondIdx2, uint16_t VarIdx, ST_PlanActOptn_e Opt, _iq24 Value, ST_PlanActTrgr_e EnterExit) |
| Adds an action to the SpinTAC Position Plan configuration. More... | |
| void | STPOSPLAN_delCfgAct (ST_POSPLAN_Handle handle, uint16_t ActIdx) |
| Deletes an action from the SpinTAC Position Plan configuration. More... | |
| void | STPOSPLAN_setCfgAct (ST_POSPLAN_Handle handle, uint16_t ActIdx, uint16_t State, ST_PlanCond_e AndOr, uint16_t CondIdx1, uint16_t CondIdx2, uint16_t VarIdx, ST_PlanActOptn_e Opt, _iq24 Value, ST_PlanActTrgr_e EnterExit) |
| Modifies an action in the SpinTAC Position Plan configuration. More... | |
| void | STPOSPLAN_getCfgAct (ST_POSPLAN_Handle handle, uint16_t ActIdx, uint16_t *State, ST_PlanCond_e *AndOr, uint16_t *CondIdx1, uint16_t *CondIdx2, uint16_t *VarIdx, ST_PlanActOptn_e *Opt, _iq24 *Value, ST_PlanActTrgr_e *EnterExit) |
| Returns an action from the SpinTAC Position Plan configuration. More... | |
| void | STPOSPLAN_addCfgVar (ST_POSPLAN_Handle handle, ST_PlanVar_e Type, _iq24 Value) |
| Adds a variable to the SpinTAC Position Plan configuration. More... | |
| void | STPOSPLAN_delCfgVar (ST_POSPLAN_Handle handle, uint16_t VarIdx) |
| Deletes a Variable from the SpinTAC Position Plan configuration. More... | |
| void | STPOSPLAN_setCfgVar (ST_POSPLAN_Handle handle, uint16_t VarIdx, ST_PlanVar_e Type, _iq24 Value) |
| Modifies a variable in the SpinTAC Position Plan configuration. More... | |
| void | STPOSPLAN_getCfgVar (ST_POSPLAN_Handle handle, uint16_t VarIdx, ST_PlanVar_e *Type, _iq24 *Value) |
| Returns a variable from the SpinTAC Position Plan configuration. More... | |
| void | STPOSPLAN_setVar (ST_POSPLAN_Handle handle, uint16_t VarIdx, _iq24 Value) |
| Sets the value of a SpinTAC Position Plan variable. More... | |
| void | STPOSPLAN_getVar (ST_POSPLAN_Handle handle, uint16_t VarIdx, _iq24 *Value) |
| Gets the value of a SpinTAC Position Plan variable. More... | |
| void | STPOSPLAN_setUnitProfDone (ST_POSPLAN_Handle handle, bool ProDON) |
| Sets a flag in SpinTAC Position Plan to indicate if the unit profile is complete. More... | |
| void | STPOSPLAN_setCfg (ST_POSPLAN_Handle handle, _iq24 T_sec, bool LoopENB) |
| Configures SpinTAC Position Plan. More... | |
| void | STPOSPLAN_getCfg (ST_POSPLAN_Handle handle, _iq24 *T_sec, bool *LoopENB) |
| Gets the SpinTAC Position Plan configuration. More... | |
| void | STPOSPLAN_setCfgHaltState (ST_POSPLAN_Handle handle, int32_t PosStepInt_mrev, _iq24 PosStepFrac_mrev, _iq24 VelLim, _iq24 AccLim, _iq20 JrkLim, int32_t Timer_tick) |
| Configures the SpinTAC Position Plan Halt state. More... | |
| void | STPOSPLAN_getCfgHaltState (ST_POSPLAN_Handle handle, int32_t *PosStepInt_mrev, _iq24 *PosStepFrac_mrev, _iq24 *VelLim, _iq24 *AccLim, _iq20 *JrkLim, int32_t *Timer_tick) |
| Gets the SpinTAC Position Plan Halt state. More... | |
| void | STPOSPLAN_addCfgState (ST_POSPLAN_Handle handle, int32_t PosStepInt_mrev, _iq24 PosStep_Fracmrev, int32_t Timer_tick) |
| Adds a State to the SpinTAC Position Plan configuration. More... | |
| void | STPOSPLAN_delCfgState (ST_POSPLAN_Handle handle, uint16_t StateIdx) |
| Deletes a state from the SpinTAC Position Plan configuration. More... | |
| void | STPOSPLAN_setCfgState (ST_POSPLAN_Handle handle, uint16_t StateIdx, int32_t PosStepInt_mrev, _iq24 PosStepFrac_mrev, int32_t Timer_tick) |
| Modifies a state in the SpinTAC Position Plan configuration. More... | |
| void | STPOSPLAN_getCfgState (ST_POSPLAN_Handle handle, uint16_t StateIdx, int32_t *PosStepInt_mrev, _iq24 *PosStepFrac_mrev, int32_t *Timer_tick) |
| Returns a state from the SpinTAC Position Plan configuration. More... | |
| void | STPOSPLAN_reset (ST_POSPLAN_Handle handle) |
| Resets the SpinAC Position Plan component. More... | |
| ST_POSPLAN_Handle | STPOSPLAN_init (void *pMemory, const size_t numBytes) |
| Initializes the SpinTAC Position Plan component. More... | |
| void | STPOSPLAN_run (ST_POSPLAN_Handle handle) |
| Runs SpinTAC Position Plan calculation. More... | |
| void | STPOSPLAN_runTick (ST_POSPLAN_Handle handle) |
| Runs SpinTAC Position Plan Timing. Call this only from an ISR. More... | |
| void | STPOSPLAN_setCfgArray (ST_POSPLAN_Handle handle, uint32_t *cfgArray, const size_t numBytes, uint16_t MaxActNum, uint16_t MaxCondNum, uint16_t MaxVarNum, uint16_t MaxTranNum, uint16_t MaxStateNum) |
| Prepares SpinTAC Position Plan data structure. More... | |
Public interface, object, and function definitions related to the SpinTAC Position Plan component.
(C) Copyright 2012, LineStream Technologies, Inc. (C) Copyright 2011, Texas Instruments, Inc.
Definition in file spintac_pos_plan.h.
1.8.9.1