MotorWare f2806x Module API Documentation
Data Structures | Typedefs
user/src/float/userParams.h File Reference

Contains the user related definitions. More...

#include "sw/modules/types/src/types.h"
#include "sw/modules/math/src/float/math.h"
#include "sw/modules/motor/src/float/motor.h"
#include "sw/modules/cal/src/cal_states.h"
#include "sw/modules/ctrl/src/ctrl_states.h"
#include "sw/modules/est/src/est_Flux_states.h"
#include "sw/modules/est/src/est_Ls_states.h"
#include "sw/modules/est/src/est_Rr_states.h"
#include "sw/modules/est/src/est_Rs_states.h"
#include "sw/modules/est/src/est_Traj_states.h"
#include "sw/modules/est/src/est_states.h"

Go to the source code of this file.

Data Structures

struct  _USER_Params_
 Defines a structure for the user parameters. More...
 

Typedefs

typedef struct _USER_Params_ USER_Params
 Defines a structure for the user parameters. More...
 

Detailed Description

Contains the user related definitions.

(C) Copyright 2014, Texas Instruments, Inc.

Definition in file user/src/float/userParams.h.