//###########################################################################
//
// FILE:   usb_dev_serial.c
//
// TITLE:  USB Serial Device example. 
//
// ASSUMPTIONS:
//
//    This program requires:
//        - the F2806x header files 
//        - Driverlib (/ControlSUITE/lib/MWare/f2806x/driverlib/)
//        - Usblib (/ControlSUITE/lib/MWare/f2806x/usblib/)
//        - USB Capable F2806x
//
// Description:
//
//! \addtogroup f2806x_example_list
//! <h1>USB Serial Device (usb_dev_serial)</h1>
//!
//! This example application turns the evaluation kit into a virtual serial
//! port when connected to the USB host system.  The application supports the
//! USB Communication Device Class, Abstract Control Model to redirect UART0
//! traffic to and from the USB host system.
//!
//! A driver information (INF) file for use with Windows XP, Windows Vista and
//! Windows7 can be found in MWare/f2806x/windows_drivers. For Windows
//! 2000, the required INF file is in /MWare/f2806x/windows_drivers/win2K.
//
//  Section .ebss was initialized to 0x0000 in
//  F2806x_CodeStartBranch_ebss_init.asm. This was to ensure that all global
//  variables of the usblib are initialized to 0x0000 on the F2806x.
//		
//###########################################################################	
// $TI Release: F2806x Support Library v2.02.00.00 $ 
// $Release Date: Sat Sep 16 15:27:43 CDT 2017 $ 
// $Copyright:
// Copyright (C) 2009-2017 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without 
// modification, are permitted provided that the following conditions 
// are met:
// 
//   Redistributions of source code must retain the above copyright 
//   notice, this list of conditions and the following disclaimer.
// 
//   Redistributions in binary form must reproduce the above copyright
//   notice, this list of conditions and the following disclaimer in the 
//   documentation and/or other materials provided with the   
//   distribution.
// 
//   Neither the name of Texas Instruments Incorporated nor the names of
//   its contributors may be used to endorse or promote products derived
//   from this software without specific prior written permission.
// 
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT 
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE 
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//#############################################################################

//
// Included Files
//
#include "DSP28x_Project.h"
#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "inc/hw_uart.h"
#include "driverlib/debug.h"
#include "driverlib/interrupt.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "driverlib/usb.h"
#include "inc/hw_usb.h"
#include "include/usblib.h"
#include "include/usbcdc.h"
#include "driverlib/usb_hal.h"
#include "include/device/usbdevice.h"
#include "include/device/usbdcdc.h"
#include "usb_serial_structs.h"
#include "themis_io_definitions.h"
#include "F2806x_GlobalPrototypes.h"

extern void Gpio_select(void);
extern void delay_loop(void);

// Configure if ePWM timer interrupt is enabled at the PIE level:
// 1 = enabled,  0 = disabled
//
#define PWM7_INT_ENABLE  1
// #define PWM7_TIMER_TBPRD   0x1FFF       // Configure the period for the timer
#define PWM7_TIMER_TBPRD   0x5FFF           // close to 2 kHz
//
// Function Prototypes
//
__interrupt void epwm7_timer_isr(void);
void InitEPwmTimer(void);

//
// Globals
//
Uint32  EPwm7TimerIntCount;     //counts entries into PWM1 Interrupt

typedef struct
{
    volatile struct EPWM_REGS *EPwmRegHandle;
    Uint16 EPwm_CMPA_Direction;
    Uint16 EPwm_CMPB_Direction;
    Uint16 EPwmTimerIntCount;
    Uint16 EPwmMaxCMPA;
    Uint16 EPwmMinCMPA;
    Uint16 EPwmMaxCMPB;
    Uint16 EPwmMinCMPB;
} EPWM_INFO;

//
// Globals
//
EPWM_INFO epwm7_info;
//
// Defines to keep track of which way the compare value is moving
//

#define EPWM_CMP_UP   1
#define EPWM_CMP_DOWN 0
#define DAC_PWM
#define USE_USB

//
//
// Defines that configure the period for each timer
//
#define EPWM7_TIMER_TBPRD  1000000  // Period register
#define EPWM7_MAX_CMPA     1950
#define EPWM7_MIN_CMPA       50
#define EPWM7_MAX_CMPB     1950
#define EPWM7_MIN_CMPB       50


//
// Flag indicating whether or not a Break condition is currently being sent.
//
static tBoolean g_bSendingBreak = false;

//
// __error__ - The error routine that is called if the driver library 
// encounters an error.
//
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
	__asm(" ESTOP0");
}
#endif

//
// CheckForSerialStateChange - This function is called whenever serial data is 
// received from the UART. It is passed the accumulated error flags from each 
// character received in this interrupt and determines from them whether or not
// an interrupt notification to the host is required.
//
// If a notification is required and the control interrupt endpoint is idle,
// send the notification immediately.  If the endpoint is not idle, accumulate
// the errors in a global variable which will be checked on completion of the
// previous notification and used to send a second one if necessary.
//
static void
CheckForSerialStateChange(const tUSBDCDCDevice *psDevice, uint32_t lErrors)
{
    unsigned short usSerialState;

    //
    // Clear the USB serial state.  Since handshakes are being faked, always
    // set the TXCARRIER (DSR) and RXCARRIER (DCD) bits.
    //
    usSerialState = USB_CDC_SERIAL_STATE_TXCARRIER |
                    USB_CDC_SERIAL_STATE_RXCARRIER;

    //
    // Are any error bits set?
    //
    if(lErrors & (UART_RXST_BRKDT | UART_RXST_FE | UART_RXST_OE | UART_RXST_PE))
    {
        //
        // At least one error is being notified so translate from the hardware
        // error bits into the correct state markers for the USB notification.
        //
        if(lErrors & UART_RXST_OE)
        {
            usSerialState |= USB_CDC_SERIAL_STATE_OVERRUN;
        }

        if(lErrors & UART_RXST_PE)
        {
            usSerialState |= USB_CDC_SERIAL_STATE_PARITY;
        }

        if(lErrors & UART_RXST_FE)
        {
            usSerialState |= USB_CDC_SERIAL_STATE_FRAMING;
        }

        if(lErrors & UART_RXST_BRKDT)
        {
            usSerialState |= USB_CDC_SERIAL_STATE_BREAK;
        }

        //
        // Call the CDC driver to notify the state change.
        //
        USBDCDCSerialStateChange((void *)psDevice, usSerialState);
    }
}

//
// ReadUARTData - Read as many characters from the UART FIFO as possible and 
// move them into the CDC transmit buffer.
//
// \return Returns UART error flags read during data reception.
//
static long
ReadUARTData(void)
{
    int32_t i32Char, i32Errors;
    uint8_t ui8Char;
    uint32_t ui32Space;

    //
    // Clear the error indicator.
    //
    i32Errors = 0;

    //
    // How much space is available in the buffer?
    //
    ui32Space = USBBufferSpaceAvailable(&g_sTxBuffer);

    //
    // Read data from the UART FIFO until there is none left or there is no
    // more space in the receive buffer.
    //
    while(ui32Space && UARTCharsAvail(UART1_BASE))
    {
        //
        // Read a character from the UART FIFO into the ring buffer if no
        // errors are reported.
        //
        i32Char = UARTCharGetNonBlocking(UART1_BASE);

        //
        // If the character did not contain any error notifications,
        // copy it to the output buffer.
        //
        if(!(i32Char & ~0xFF))
        {
            ui8Char = (unsigned char)(i32Char & 0xFF);
            USBBufferWrite(&g_sTxBuffer, &ui8Char, 1);

            //
            // Decrement the number of bytes the buffer can accept.
            //
            ui32Space--;
        }
        else
        {
            //
            // Update the error accumulator.
            //
            i32Errors |= i32Char;
        }
    }

    //
    // Pass back the accumulated error indicators.
    //
    return(i32Errors);
}

//
// USBUARTPrimeTransmit - Take as many bytes from the transmit buffer as there
// is space for and move them into the USB UART's transmit FIFO.
//
static void
USBUARTPrimeTransmit(void)
{
    uint32_t ui32Read;
    uint8_t ui8Char;

    //
    // If a break condition is currently being sent, don't receive any more
    // data.  Transmission will resume once the break is turned off.
    //
    if(g_bSendingBreak)
    {
        return;
    }

    //
    // If there is space in the UART FIFO, try to read some characters
    // from the receive buffer to fill it again.
    //
    while(UARTSpaceAvail(UART1_BASE))
    {
        //
        // Get a character from the buffer.
        //
        ui32Read = USBBufferRead(&g_sRxBuffer, &ui8Char, 1);

        //
        // Was a character read?
        //
        if(ui32Read)
        {
            //
            // Place the character in the UART transmit FIFO.
            //
            UARTCharPutNonBlocking(UART1_BASE, ui8Char);
        }
        else
        {
            //
            // There are no more characters so exit the function.
            //
            return;
        }
    }
}

//
// USBUARTTXIntHandler- Interrupt handler for the UART TX which is being 
// redirected via USB.
//
__interrupt void
USBUARTTXIntHandler(void)
{
    uint32_t ui32Ints;

    ui32Ints = UARTIntStatus(UART1_BASE, true);
    //
    // Handle transmit interrupts.
    //
    if(ui32Ints & UART_INT_TXRDY)
    {
        //
        // Move as many bytes as possible into the transmit FIFO.
        //
        USBUARTPrimeTransmit();

        //
        // If the output buffer is empty, turn off the transmit interrupt.
        //
        if(!USBBufferDataAvailable(&g_sRxBuffer))
        {
            UARTIntDisable(UART1_BASE, UART_INT_TXRDY);
        }
    }

    PieCtrlRegs.PIEACK.bit.ACK9 = 1;
}

//
// USBUARTRXIntHandler - Interrupt handler for the UART RX which is being 
// redirected via USB.
//
__interrupt void
USBUARTRXIntHandler(void)
{
    uint32_t ui32Ints;

    ui32Ints = UARTIntStatus(UART1_BASE, true);
    
    //
    // Handle receive interrupts.
    //
    if(ui32Ints & UART_INT_RXRDY_BRKDT)
    {
        //
        // Read the UART's characters into the buffer.
        //
        ReadUARTData();

    }
    else if(ui32Ints & UART_INT_RXERR)
    {
        //
        //Notify Host of our error
        //
        CheckForSerialStateChange(&g_sCDCDevice, UARTRxErrorGet(UART1_BASE));

        //
        //Clear the error and continue
        //
        UARTRxErrorClear(UART1_BASE);
    }

    PieCtrlRegs.PIEACK.bit.ACK9 = 1;

}

//
// SetLineCoding - Set the communication parameters to use on the UART.
//
static tBoolean
SetLineCoding(tLineCoding *psLineCoding)
{
    uint32_t ui32Config;
    tBoolean bRetcode;

    //
    // Assume everything is OK until a problem is detected.
    //
    bRetcode = true;

    //
    // Word length.  For invalid values, the default is to set 8 bits per
    // character and return an error.
    //
    switch(psLineCoding->ui8Databits)
    {
        case 5:
        {
            ui32Config = UART_CONFIG_WLEN_5;
            break;
        }

        case 6:
        {
            ui32Config = UART_CONFIG_WLEN_6;
            break;
        }

        case 7:
        {
            ui32Config = UART_CONFIG_WLEN_7;
            break;
        }

        case 8:
        {
            ui32Config = UART_CONFIG_WLEN_8;
            break;
        }

        default:
        {
            ui32Config = UART_CONFIG_WLEN_8;
            bRetcode = false;
            break;
        }
    }

    //
    // Parity.  For any invalid values, set no parity and return an error.
    //
    switch(psLineCoding->ui8Parity)
    {
        case USB_CDC_PARITY_NONE:
        {
            ui32Config |= UART_CONFIG_PAR_NONE;
            break;
        }

        case USB_CDC_PARITY_ODD:
        {
            ui32Config |= UART_CONFIG_PAR_ODD;
            break;
        }

        case USB_CDC_PARITY_EVEN:
        {
            ui32Config |= UART_CONFIG_PAR_EVEN;
            break;
        }

        default:
        {
            ui32Config |= UART_CONFIG_PAR_NONE;
            bRetcode = false;
            break;
        }
    }

    //
    // Stop bits.  The hardware only supports 1 or 2 stop bits whereas CDC
    // allows the host to select 1.5 stop bits.  If passed 1.5 (or any other
    // invalid or unsupported value of ucStop, set up for 1 stop bit but return
    // an error in case the caller needs to Stall or otherwise report this back
    // to the host.
    //
    switch(psLineCoding->ui8Stop)
    {
        //
        // One stop bit requested.
        //
        case USB_CDC_STOP_BITS_1:
        {
            ui32Config |= UART_CONFIG_STOP_ONE;
            break;
        }

        //
        // Two stop bits requested.
        //
        case USB_CDC_STOP_BITS_2:
        {
            ui32Config |= UART_CONFIG_STOP_TWO;
            break;
        }

        //
        // Other cases are either invalid values of ucStop or values that are
        // not supported, so set 1 stop bit but return an error.
        //
        default:
        {
            ui32Config = UART_CONFIG_STOP_ONE;
            bRetcode = false;
            break;
        }
    }

    //
    // Set the UART mode appropriately.
    //
    UARTConfigSetExpClk(UART1_BASE, SysCtlClockGet(SYSTEM_CLOCK_SPEED)/4,
    		            readusb32_t(&(psLineCoding->ui32Rate)), ui32Config);

    //
    // Let the caller know if a problem was encountered.
    //
    return(bRetcode);
}

//
// GetLineCoding - Get the communication parameters in use on the UART.
//
static void
GetLineCoding(tLineCoding *psLineCoding)
{
    uint32_t ui32Config;
    uint32_t ui32Rate;

    //
    // Get the current line coding set in the UART.
    //
    UARTConfigGetExpClk(UART1_BASE, SysCtlClockGet(SYSTEM_CLOCK_SPEED)/4,
                        &ui32Rate, &ui32Config);
    writeusb32_t(&(psLineCoding->ui32Rate), ui32Rate);

    //
    // Translate the configuration word length field into the format expected
    // by the host.
    //
    switch(ui32Config & UART_CONFIG_WLEN_MASK)
    {
        case UART_CONFIG_WLEN_8:
        {
            psLineCoding->ui8Databits = 8;
            break;
        }

        case UART_CONFIG_WLEN_7:
        {
            psLineCoding->ui8Databits = 7;
            break;
        }

        case UART_CONFIG_WLEN_6:
        {
            psLineCoding->ui8Databits = 6;
            break;
        }

        case UART_CONFIG_WLEN_5:
        {
            psLineCoding->ui8Databits = 5;
            break;
        }
    }

    //
    // Translate the configuration parity field into the format expected
    // by the host.
    //
    switch(ui32Config & UART_CONFIG_PAR_MASK)
    {
        case UART_CONFIG_PAR_NONE:
        {
            psLineCoding->ui8Parity = USB_CDC_PARITY_NONE;
            break;
        }

        case UART_CONFIG_PAR_ODD:
        {
            psLineCoding->ui8Parity = USB_CDC_PARITY_ODD;
            break;
        }

        case UART_CONFIG_PAR_EVEN:
        {
            psLineCoding->ui8Parity = USB_CDC_PARITY_EVEN;
            break;
        }
    }

    //
    // Translate the configuration stop bits field into the format expected
    // by the host.
    //
    switch(ui32Config & UART_CONFIG_STOP_MASK)
    {
        case UART_CONFIG_STOP_ONE:
        {
            psLineCoding->ui8Stop = USB_CDC_STOP_BITS_1;
            break;
        }

        case UART_CONFIG_STOP_TWO:
        {
            psLineCoding->ui8Stop = USB_CDC_STOP_BITS_2;
            break;
        }
    }
}

//
// SendBreak - This function sets or clears a break condition on the redirected
// UART RX line.  A break is started when the function is called with \e bSend 
// set to \b true and persists until the function is called again with \e bSend
// set to \b false.
//
static void
SendBreak(tBoolean bSend)
{
    //
    //C28x SCI cannot send break conditions
    //
    return;
}

//
// ControlHandler - Handles CDC driver notifications related to control and 
// setup of the device.
//
// \param pvCBData is the client-supplied callback pointer for this channel.
// \param ui32Event identifies the notification event.
// \param ui32MsgValue is an event-specific value.
// \param pvMsgData is an event-specific pointer.
//
// This function is called by the CDC driver to perform control-related
// operations on behalf of the USB host.  These functions include setting
// and querying the serial communication parameters, setting handshake line
// states and sending break conditions.
//
// \return The return value is event-specific.
//
unsigned long
ControlHandler(void *pvCBData, uint32_t ui32Event, uint32_t ui32MsgValue,
               void *pvMsgData)
{
    //
    // Which event was sent?
    //
    switch(ui32Event)
    {
        //
        // The host has connected.
        //
        case USB_EVENT_CONNECTED:
        {
            //
            // Flush the buffers.
            //
            USBBufferFlush(&g_sTxBuffer);
            USBBufferFlush(&g_sRxBuffer);

            break;
        }

        //
        // The host has disconnected.
        //
        case USB_EVENT_DISCONNECTED:
        {
            break;
        }

        //
        // Return the current serial communication parameters.
        //
        case USBD_CDC_EVENT_GET_LINE_CODING:
        {
            GetLineCoding(pvMsgData);
            break;
        }

        //
        // Set the current serial communication parameters.
        //
        case USBD_CDC_EVENT_SET_LINE_CODING:
        {
            SetLineCoding(pvMsgData);
            break;
        }

        //
        // Set the current serial communication parameters.
        //
        case USBD_CDC_EVENT_SET_CONTROL_LINE_STATE:
        {
            break;
        }

        //
        // Send a break condition on the serial line.
        //
        case USBD_CDC_EVENT_SEND_BREAK:
        {
            SendBreak(true);
            break;
        }

        //
        // Clear the break condition on the serial line.
        //
        case USBD_CDC_EVENT_CLEAR_BREAK:
        {
            SendBreak(false);
            break;
        }

        //
        // Ignore SUSPEND and RESUME for now.
        //
        case USB_EVENT_SUSPEND:
        case USB_EVENT_RESUME:
        {
            break;
        }

        //
        // Other events can be safely ignored.
        //
        default:
        {
            break;
        }
    }
    return(0);
}

//
// TxHandler - Handles CDC driver notifications related to the transmit channel
// (data to the USB host).
//
// \param ui32CBData is the client-supplied callback pointer for this channel.
// \param ui32Event identifies the notification event.
// \param ui32MsgValue is an event-specific value.
// \param pvMsgData is an event-specific pointer.
//
// This function is called by the CDC driver to notify us of any events
// related to operation of the transmit data channel (the IN channel carrying
// data to the USB host).
//
// \return The return value is event-specific.
//
unsigned long
TxHandler(void *pvCBData, uint32_t ui32Event, uint32_t ui32MsgValue,
          void *pvMsgData)
{
    //
    // Which event was sent?
    //
    switch(ui32Event)
    {
        case USB_EVENT_TX_COMPLETE:
        {
            //
            // There is nothing to do here since it is handled by the
            // USBBuffer.
            //
            break;
        }

        //
        // Other events can be safely ignored.
        //
        default:
        {
            break;
        }
    }

    return(0);
}

//
// RxHandler - Handles CDC driver notifications related to the receive channel 
// (data from the USB host).
//
// \param ui32CBData is the client-supplied callback data value for this channel.
// \param ui32Event identifies the notification event.
// \param ui32MsgValue is an event-specific value.
// \param pvMsgData is an event-specific pointer.
//
// This function is called by the CDC driver to notify us of any events
// related to operation of the receive data channel (the OUT channel carrying
// data from the USB host).
//
// \return The return value is event-specific.
//
unsigned long
RxHandler(void *pvCBData, uint32_t ui32Event, uint32_t ui32MsgValue,
          void *pvMsgData)
{
    uint32_t ui32Count;

    //
    // Which event was sent?
    //
    switch(ui32Event)
    {
        //
        // A new packet has been received.
        //
        case USB_EVENT_RX_AVAILABLE:
        {
            //
            // Feed some characters into the UART TX FIFO and enable the
            // interrupt.
            //
            USBUARTPrimeTransmit();
            UARTIntEnable(UART1_BASE, UART_INT_TXRDY);
            break;
        }

        //
        // This is a request for how much unprocessed data is still waiting to
        // be processed.  Return 0 if the UART is currently idle or 1 if it is
        // in the process of transmitting something.  The actual number of
        // bytes in the UART FIFO is not important here, merely whether or
        // not everything previously sent to us has been transmitted.
        //
        case USB_EVENT_DATA_REMAINING:
        {
            //
            // Get the number of bytes in the buffer and add 1 if some data
            // still has to clear the transmitter.
            //
            ui32Count = UARTBusy(UART1_BASE) ? 1 : 0;
            return(ui32Count);
        }

        //
        // This is a request for a buffer into which the next packet can be
        // read.  This mode of receiving data is not supported so let the
        // driver know by returning 0.  The CDC driver should not be sending
        // this message but this is included just for illustration and
        // completeness.
        //
        case USB_EVENT_REQUEST_BUFFER:
        {
            return(0);
        }

        //
        // Other events can be safely ignored.
        //
        default:
        {
            break;
        }
    }

    return(0);
}

//
// SysCtrlInit - 
//
void
SysCtrlInit(void)
{
    EALLOW;
    
    //
    // Disable Watchdog
    //
    SysCtrlRegs.WDCR = 0x68;

    //
    // Setup Clock
    // 20MHz ->PLL->80MHz->C28
    //      ->PLL2->120MHz->USB
    //
    SysCtrlRegs.CLKCTL.bit.XCLKINOFF = 0;
    SysCtrlRegs.CLKCTL.bit.XTALOSCOFF = 0;
    SysCtrlRegs.CLKCTL.bit.OSCCLKSRC2SEL = 0;
    SysCtrlRegs.CLKCTL.bit.OSCCLKSRCSEL = 1;

    while(SysCtrlRegs.PLLSTS.bit.MCLKSTS);
    SysCtrlRegs.PLLSTS.bit.DIVSEL = 0;
    SysCtrlRegs.PLLSTS.bit.MCLKOFF = 1;
    SysCtrlRegs.PLLCR.bit.DIV = 4;
    while(!SysCtrlRegs.PLLSTS.bit.PLLLOCKS);
    SysCtrlRegs.PLLSTS.bit.MCLKOFF = 1;
    SysCtrlRegs.PLLSTS.bit.DIVSEL = 3;

    SysCtrlRegs.PLL2CTL.bit.PLL2CLKSRCSEL = 1;
    SysCtrlRegs.PLL2CTL.bit.PLL2EN = 1;
    SysCtrlRegs.PLL2MULT.bit.PLL2MULT = 6;
    while(!SysCtrlRegs.PLL2STS.bit.PLL2LOCKS);


#ifdef USE_USB

    //
    // Enable USB Clock
    //
    SysCtrlRegs.PCLKCR3.bit.USB0ENCLK = 1;
    
    //
    // Enable PHY
    //
    GpioCtrlRegs.GPACTRL2.bit.USB0IOEN = 1;
#endif
    EDIS;
}

//
// main - This is the main application entry function.
//
int
main(void)
{
	//
    // Section .ebss was initialized to 0x0000 in
	// F2806x_CodeStartBranch_ebss_init.asm. This was to ensure that all global
	// variables of the usblib are initialized to 0x0000 on the F2806x.
	//

    //
    // Set the clocking to run from the PLL
    //
    DINT;

    //
    // Disable CPU interrupts and clear all CPU interrupt flags
    //
    IER = 0x0000;
    IFR = 0x0000;

//     InitAdc();         // For this example, init the ADC
//     AdcOffsetSelfCal();


    themis_gpio_init();			// initilize themis gpio
    
    SysCtrlInit();
    InitPieCtrl();
    InitPieVectTable();
    
#ifdef DAC_PWM
    EALLOW;  // This is needed to write to EALLOW protected registers
    PieVectTable.EPWM7_INT = &epwm7_timer_isr;
    EDIS;    // This is needed to disable write to EALLOW protected registers
#endif

 //   InitEPwmTimer();    // For this example, only initialize the ePWM Timer


    // InitAdc();         // For this example, init the ADC
    // AdcOffsetSelfCal();

    //
    // Enable Device Mode
    //

 //   Gpio_select();                          // init GPIO


    themis_usb_gpio_init();
    //
    // Enable the UART.
    //
    SysCtlPeripheralEnable(SYSCTL_PERIPH_UART1);

    //
    // Enable and configure the UART RX and TX pins
    //

    themis_uart_gpio_init();
    
    //
      EALLOW;
      SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;
      EDIS;

      InitEPwmTimer();    // For this example, only initialize the ePWM Timer();

      EALLOW;
      SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;
      EDIS;

        //

//      USBGPIOEnable();
#ifdef USE_USB
    //
    // Register interrupt handlers
    //
    IntRegister(INT_SCITXINTB, USBUARTTXIntHandler);
    IntRegister(INT_SCIRXINTB, USBUARTRXIntHandler);

    //
    // Configure the required pins for USB operation.
    //
    USBGPIOEnable();
    USBIntRegister(USB0_BASE, f28x_USB0DeviceIntHandler);

    //
    // Set the default UART configuration.
    //
    UARTConfigSetExpClk(UART1_BASE, SysCtlClockGet(SYSTEM_CLOCK_SPEED)/4,
                        115200, UART_CONFIG_WLEN_8 | UART_CONFIG_PAR_NONE |
                        UART_CONFIG_STOP_ONE);
    UARTFIFOLevelSet(UART1_BASE, UART_FIFO_TX4_8, UART_FIFO_RX4_8);

    //
    // Configure and enable UART interrupts.
    //
    UARTIntClear(UART1_BASE, UARTIntStatus(UART1_BASE, false));
    UARTIntEnable(UART1_BASE, (UART_INT_RXERR | UART_INT_RXRDY_BRKDT |
                  UART_INT_TXRDY ));

    //
    // Initialize the transmit and receive buffers.
    //
    USBBufferInit(&g_sTxBuffer);
    USBBufferInit(&g_sRxBuffer);

    //
    // Set the USB stack mode to Device mode with VBUS monitoring.
    //
    USBStackModeSet(0, eUSBModeForceDevice, 0);

    //
    // Pass the device information to the USB library and place the device
    // on the bus.
    //
    USBDCDCInit(0, &g_sCDCDevice);

    //
    // Enable interrupts now that the application is ready to start.
    //
    IntEnable(INT_SCITXINTB);
    IntEnable(INT_SCIRXINTB);

    IntMasterEnable();
    // Enable CPU INT3 which is connected to EPWM1-6 INT
     //
#endif
#ifdef DAC_PWM
     IER |= M_INT3;

     //
      // Enable EPWM INTn in the PIE: Group 3 interrupt 1-6
      //
      PieCtrlRegs.PIEIER3.bit.INTx7 = PWM7_INT_ENABLE;

    //
    // Initalize counters
    //
    EPwm7TimerIntCount = 0;


     //
     // Initially disable time-critical interrupts
     //
     SetDBGIER(0x0000);          // PIE groups time-critical designation

     //
     // Enable global Interrupts and higher priority real-time debug events
     //
     EINT;   // Enable Global interrupt INTM
     ERTM;   // Enable Global realtime interrupt DBGM
#endif

    //
    // Main application loop.
    //
    while(1)
    {
#if 0
            EALLOW;
            GpioCtrlRegs.GPAMUX1.bit.GPIO8 = ENABLE;                // ENABLE MEMS OSC - 90 MHz
            GpioCtrlRegs.GPAPUD.bit.GPIO8 = DISABLE;
            GpioCtrlRegs.GPADIR.bit.GPIO8 = ENABLE;
            EDIS;
#endif
 //           EALLOW;
 //           GpioDataRegs.GPASET.bit.GPIO8 = ENABLE;
 //           GpioCtrlRegs.GPADIR.bit.GPIO8 = ENABLE;
 //           EDIS;
            delay_loop();
#if 0
            EALLOW;
                       GpioCtrlRegs.GPAMUX1.bit.GPIO8 = ENABLE;                // ENABLE MEMS OSC - 90 MHz
                       GpioCtrlRegs.GPAPUD.bit.GPIO8 = DISABLE;
                       GpioCtrlRegs.GPADIR.bit.GPIO8 = DISABLE;
                       EDIS;
#endif
                       delay_loop();
    }
}

//
// InitEPwmTimer -
//
#if 1
void
InitEPwmTimer()
{
    EALLOW;
    SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;      // Stop all the TB clocks
    EDIS;

    //
    // Disable Sync
    //
    EPwm7Regs.TBCTL.bit.SYNCOSEL = 11;  // Pass through

    //
    // Initally disable Free/Soft Bits
    //
    EPwm7Regs.TBCTL.bit.FREE_SOFT = 0;

    EPwm7Regs.TBPRD = PWM7_TIMER_TBPRD;          // Set up PWM1 Period
    EPwm7Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;   // Count up mode
    EPwm7Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO;    // Select INT on Zero event
    EPwm7Regs.ETSEL.bit.INTEN = PWM7_INT_ENABLE; // Enable INT
    EPwm7Regs.ETPS.bit.INTPRD = ET_1ST;          // Generate INT on 1st event
    EPwm7Regs.TBCTR = 0x0000;                    // Clear timer counter

    //
    // CompareA event at half of period
    //
    EPwm7Regs.CMPA.half.CMPA = PWM7_TIMER_TBPRD/2;

    //
    // Action-qualifiers, Set on CMPA, Clear on PRD
    //
    EPwm7Regs.AQCTLA.all = 0x0024;

    EALLOW;
    SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;       // Start all the timers synced
    EDIS;
}
#endif

//
// InitEPwm1Example -
//
#if 0
void
InitEPwmTimer()
{
    //
    // Setup TBCLK
    //

    EPwm7Regs.TBCTL.bit.PRDLD = TB_IMMEDIATE;     // set Immediate load
    EPwm7Regs.TBPRD = EPWM7_TIMER_TBPRD - 1;                   // PWM frequency = 1 / period
    EPwm7Regs.CMPA.half.CMPA = EPWM7_TIMER_TBPRD / 2;        // set duty 50% initially
    EPwm7Regs.CMPA.half.CMPAHR = (1 << 8);        // initialize HRPWM extension
    EPwm7Regs.CMPB = EPWM7_TIMER_TBPRD / 2;                  // set duty 50% initially
    EPwm7Regs.TBPHS.all = 0;
    EPwm7Regs.TBCTR = 0;


    EPwm7Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP; // Count up
    EPwm7Regs.TBPRD = EPWM7_TIMER_TBPRD;       // Set timer period
    EPwm7Regs.TBCTL.bit.PHSEN = TB_DISABLE;    // Disable phase loading
    EPwm7Regs.TBPHS.half.TBPHS = 0x0000;       // Phase is 0
    EPwm7Regs.TBCTR = 0x0000;                  // Clear counter
    EPwm7Regs.TBCTL.bit.HSPCLKDIV = TB_DIV2;   // Clock ratio to SYSCLKOUT
    EPwm7Regs.TBCTL.bit.CLKDIV = TB_DIV2;

    //
    // Setup shadow register load on ZERO
    //
    EPwm7Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
    EPwm7Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
    EPwm7Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
    EPwm7Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;

    //
    // Set Compare values
    //
    EPwm7Regs.CMPA.half.CMPA = EPWM7_MIN_CMPA;    // Set compare A value
    EPwm7Regs.CMPB = EPWM7_MIN_CMPB;              // Set Compare B value

    //
    // Set actions
    //
    EPwm7Regs.AQCTLA.bit.ZRO = AQ_CLEAR;      // Set PWM1A on Zero
    EPwm7Regs.AQCTLA.bit.CAU = AQ_SET;    // Clear PWM1A on event A, up count

    EPwm7Regs.AQCTLB.bit.ZRO = AQ_CLEAR;      // Set PWM1B on Zero
    EPwm7Regs.AQCTLB.bit.CBU = AQ_SET;    // Clear PWM1B on event B, up count

    //
    // Interrupt where we will change the Compare Values
    //
    EPwm7Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO;     // Select INT on Zero event
    EPwm7Regs.ETSEL.bit.INTEN = 1;                // Enable INT
    EPwm7Regs.ETPS.bit.INTPRD = ET_1ST;           // Generate INT on 3rd event

    //
    // Information this example uses to keep track of the direction the
    // CMPA/CMPB values are moving, the min and max allowed values and
    // a pointer to the correct ePWM registers
    //

    //
    // Start by increasing CMPA & CMPB
    //
    epwm7_info.EPwm_CMPA_Direction = EPWM_CMP_UP;
    epwm7_info.EPwm_CMPB_Direction = EPWM_CMP_UP;

    epwm7_info.EPwmTimerIntCount = 0;         // Zero the interrupt counter
    epwm7_info.EPwmRegHandle = &EPwm7Regs;// Set the pointer to the ePWM module
    epwm7_info.EPwmMaxCMPA = EPWM7_MAX_CMPA;  // Setup min/max CMPA/CMPB values
    epwm7_info.EPwmMinCMPA = EPWM7_MIN_CMPA;
    epwm7_info.EPwmMaxCMPB = EPWM7_MAX_CMPB;
    epwm7_info.EPwmMinCMPB = EPWM7_MIN_CMPB;
}
#endif
//
// epwm1_timer_isr - Interrupt routines uses in this example
//
__interrupt void
epwm7_timer_isr(void)
{
    EPwm7TimerIntCount++;
//    LEDcount++;

    //
    // Clear INT flag for this timer
    //
    EPwm7Regs.ETCLR.bit.INT = 1;
#if 0
    if (LEDcount==500)
    {
        //
        // turn on/off LED3 on the controlCARD
        //
        GpioDataRegs.GPBTOGGLE.bit.GPIO34 = 1;
        LEDcount=0;
    }
#endif
    //
    // Acknowledge this interrupt to receive more interrupts from group 3
    //
    PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
}



//
// End of File
//





//
// End of File
//