Version.txt
                                      ===========

This is Build 10a of Serial Port Flash Programming Utilities for the TMS320LF240x-A silicon.

This programs the flash over the serial communications interface (SCI).


Revision History	

April 11, 2002:
	Commented out in the clear.asm the line which wrote to the SCSR1 to set up the
	PLL. The PLL is set up in the boot ROM code, and there is a selection mechanism
	to select x2 or x4 mode for the PLL. (only on the -A parts) This over-wrote 
	that selection causing the programmer to fail when the x2 option was selected,
	since only the pll register got changed, while the baud rate register in the 
	SCI remained the same.



March 27, 2002
	1. Updated for the security and documented this.



November 14, 2000

	1. Updated timing information files. Added support for configuration
	   for different frequencies.
	2. NOTE: The Boot ROM loader still puts in X4 for the PLL mutiplier.
		 This means that the CLKIN must be 7.5 MHZ or less per documentation
		 in the SPRU357 ( LF240x Users guide).
	3. Updated f240_hex.exe version with the v2.0b. This version handles
	   separate run and load adresses correctly.



April  10, 2000	                

        1. Fixed a bug in the programming algorithm where section on a boundary 
        not divisible by 8 would fail.