READ-ME FILE ****IMPORTANT**** READ THIS CAREFULLY

320F2XX Flash Programming Utility Rev2.0b Beta    12/5/97
**********************************************************
This revision includes changes to the 'F2XX algorithm code only. The user
interface and all other files are identical to Rev2.0. Note that since the 
user interface is the same, it will still report Rev2.0 rather than Rev2.0b
when using this beta revision of the software.  It is therefore important 
to know which version of the complete utility package is being used. Please 
give the correct revision number with letter when contacting TI for any 
support questions.