Changes:

VIF: 
	Unchunked Supported set -> YES : JSON has Unchunked Supported in PD3 Config register
	Responds to Discov SOP_UFP -> YES
	Updated SOP Discover ID tab with correct values
	VIF 9-V PDO had 0-A current, changing to 3 to match JSON

JSON: 
	Number of batteries (in TX source cap extended-> Battries, set fixed batteries to 1)
		The sink cap extended uses the field in source extended. A little confusing, but done because we never expect them to be different
	PD3 Config -> Suport Sink cap extended bit -> yes (Required for Sinks)
	Sink caps extended:
		battery powered -> yes
		TX sink capabilities extended data block group 1 -> max PDP set to 45-W
			Here you can set the min power you want



Re


Discover SOP as UFP
SOP_P capable
Unchunked


Responds to discov UFP
	If never being UFP, disable

Same for DFP