/* USER CODE BEGIN Header */
/**
  ******************************************************************************
  * @file           : main.c
  * @brief          : Main program body
  ******************************************************************************
  * @attention
  *
  * <h2><center>&copy; Copyright (c) 2020 STMicroelectronics.
  * All rights reserved.</center></h2>
  *
  * This software component is licensed by ST under BSD 3-Clause license,
  * the "License"; You may not use this file except in compliance with the
  * License. You may obtain a copy of the License at:
  *                        opensource.org/licenses/BSD-3-Clause
  *
  ******************************************************************************
  */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include <stdio.h>
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define MAX_BUFFER_SIZE     10
/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
SPI_HandleTypeDef hspi1;

TIM_HandleTypeDef htim1;

UART_HandleTypeDef huart2;

/* USER CODE BEGIN PV */
uint8_t spiData [2];
uint8_t spiRxData [2];
uint8_t rxdata [2];
uint8_t busyData [2] = {0xFF, 0xFF};

uint8_t TX_2Byte [2] = {0x00, 0x00};
uint8_t TX_3Byte [3] = {0x00, 0x00, 0x00};
uint8_t TX_4Byte [4] = {0x00, 0x00, 0x00, 0x00};
uint8_t TX_Buffer [MAX_BUFFER_SIZE] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};

uint8_t RX_2Byte [2] = {0x00, 0x00};
uint8_t RX_3Byte [3] = {0x00, 0x00, 0x00};
uint8_t RX_4Byte [4] = {0x00, 0x00, 0x00, 0x00};
uint8_t RX_12Byte [12] = {0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};
uint8_t RX_Buffer [MAX_BUFFER_SIZE] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};
unsigned int RX_CRC_Check = 0;

// Variables for cell voltages, temperatures, CC2 current, Stack voltage, PACK Pin voltage, LD Pin voltage
uint16_t CellVoltage [16] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};
float Temperature [3] = {0,0,0};
float FET_Temperature = 0;
uint16_t Stack_Voltage = 0x00;
uint16_t LD_Voltage = 0x00;
uint16_t PACK_Voltage = 0x00;
uint16_t PACK_Current = 0x00;
uint16_t AlarmBits = 0x00;

uint8_t SafetyStatusA;  // Safety Status Register A
uint8_t SafetyStatusB;  // Safety Status Register B
uint8_t SafetyStatusC;  // Safety Status Register C
uint8_t PFStatusA;   // Permanent Fail Status Register A
uint8_t PFStatusB;   // Permanent Fail Status Register B
uint8_t PFStatusC;   // Permanent Fail Status Register C
uint8_t FET_Status;  // FET Status register contents See TRM Section 12.2.20  - Shows states of FETs

uint16_t CB_ActiveCells;  // Cell Balancing Active Cells
uint16_t DEVICE_NUMBER;

uint8_t	UV_Fault = 0;   // under-voltage fault state
uint8_t	OV_Fault = 0;   // over-voltage fault state
uint8_t	SCD_Fault = 0;  // short-circuit fault state
uint8_t	OCD_Fault = 0;  // over-current fault state
uint8_t LD_ON = 0;							// Load Detect status bit
uint8_t DCHG = 0;   // discharge FET state
uint8_t CHG = 0;   // charge FET state
uint8_t PCHG = 0;  // pre-charge FET state
uint8_t PDSG = 0;  // pre-discharge FET state

uint32_t AccumulatedCharge_Int;
uint32_t AccumulatedCharge_Frac;
uint32_t AccumulatedCharge_Time;

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_SPI1_Init(void);
static void MX_USART2_UART_Init(void);
static void MX_TIM1_Init(void);

/* USER CODE BEGIN PFP */

void delayUS(uint32_t us) {   // Sets the delay in microseconds. 
	__HAL_TIM_SET_COUNTER(&htim1,0);  // set the counter value a 0
	while (__HAL_TIM_GET_COUNTER(&htim1) < us);  // wait for the counter to reach the us input in the parameter
}

void delay_ticks(uint32_t ticks)
{
    SysTick->LOAD = ticks;
    SysTick->VAL = 0;
    SysTick->CTRL = SysTick_CTRL_ENABLE_Msk;
    // COUNTFLAG is a bit that is set to 1 when counter reaches 0.
    // It's automatically cleared when read.
    while ((SysTick->CTRL & SysTick_CTRL_COUNTFLAG_Msk) == 0);
    SysTick->CTRL = 0;
}

unsigned char Checksum(unsigned char *ptr, unsigned char len)
	// Calculates the checksum when writing to a RAM register. The checksum is the inverse of the sum of the bytes.
{
	unsigned char i;
	unsigned char checksum = 0;
	
	for(i=0; i<len; i++)
		checksum += ptr[i];

	checksum = 0xff & ~checksum;

	return(checksum);
}



void SPI_WriteReg(uint8_t reg_addr, uint8_t *reg_data, uint8_t count) {
	// SPI Write. Includes retries in case HFO has not started or if wait time is needed. See BQ76952 Software Development Guide for examples
  uint8_t addr; 
  unsigned int i;
	unsigned int match;
	unsigned int retries = 10;
    
	match = 0;
  addr = 0x80 | reg_addr;
    
  for(i=0; i<count; i++) {
		TX_Buffer[0] = addr;
		TX_Buffer[1] = reg_data[i];
		
		HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_RESET);
		HAL_SPI_TransmitReceive(&hspi1, TX_Buffer, rxdata, 2, 1);
		HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_SET); 
        
		while ((match == 0) & (retries > 0)) {
			delayUS(500);
			HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_RESET);
			HAL_SPI_TransmitReceive(&hspi1, TX_Buffer, rxdata, 2, 1);
			HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_SET); 
			if ((rxdata[0] == addr) & (rxdata[1] == reg_data[i]))
				match = 1;
			retries --;
		}    
    match = 0;
    addr += 1;
		delayUS(500);
  }
}


void SPI_ReadReg(uint8_t reg_addr, uint8_t *reg_data, uint8_t count) {
	// SPI Read. Includes retries in case HFO has not started or if wait time is needed. See BQ76952 Software Development Guide for examples
  uint8_t addr; 
  unsigned int i;
	unsigned int match;
	unsigned int retries = 10;
    
	match = 0;
  addr = reg_addr;
    
  for(i=0; i<count; i++) {
		TX_Buffer[0] = addr;
		TX_Buffer[1] = 0xFF;
		
		HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_RESET);
		HAL_SPI_TransmitReceive(&hspi1, TX_Buffer, rxdata, 2, 1);
		HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_SET); 
        
		while ((match == 0) & (retries > 0)) {
			delayUS(500);
			HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_RESET);
			HAL_SPI_TransmitReceive(&hspi1, TX_Buffer, rxdata, 2, 1);
			HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_SET); 
			if (rxdata[0] == addr) {
				match = 1;
				reg_data[i] = rxdata[1];
			}
			retries --;
		}    
    match = 0;
    addr += 1;
		delayUS(500);
  }
}
void AFE_Reset() {
	// Reset command. Resets all registers to default values or the values programmed in OTP.
	TX_2Byte[0] = 0x12; TX_2Byte[1] = 0x00;
	SPI_WriteReg(0x3E,TX_2Byte,2);
}

void AFE_Init() {
	// Configures all parameters in device RAM
	
	// Enter CONFIGUPDATE mode (Subcommand 0x0090) - It is required to be in CONFIG_UPDATE mode to program the device RAM settings
	// See TRM Section 7.6 for full description of CONFIG_UPDATE mode
	TX_2Byte[0] = 0x90; TX_2Byte[1] = 0x00;
	SPI_WriteReg(0x3E,TX_2Byte,2);
	
	delayUS(2000);
	
	// After entering CONFIG_UPDATE mode, RAM registers can be programmed. When programming RAM, checksum and length must also be
	// programmed for the change to take effect. All of the RAM registers are described in detail in Chapter 13 of the BQ76952 TRM.
	// An easier way to find the descriptions is in the BQStudio Data Memory screen. When you move the mouse over the register name, 
	// a full description of the register and the bits will pop up on the screen.
	// A summary of the Data Memory is also in Section 13.9 of the TRM.
	
	// 'Power Config' - Set DSLP_LDO  - 0x9234 = 0x2D80  (See TRM section 13.3.2)
	// Setting the DSLP_LDO bit allows the LDOs to remain active when the device goes into Deep Sleep mode
  TX_4Byte[0] = 0x34; TX_4Byte[1] = 0x92; TX_4Byte[2] = 0x80; TX_4Byte[3] = 0x2D;
  SPI_WriteReg(0x3E, TX_4Byte, 4); 
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_4Byte, 4); TX_2Byte[1] = 0x06;  // Checksum and Length
  SPI_WriteReg(0x60, TX_2Byte, 2);	
	delayUS(1000);
	
	// 'VCell Mode' - Enable 16 cells - 0x9304 = 0x0000  (See TRM section 13.3.2.19)
	// 0x0000 sets the default value of 16 cells.
  TX_4Byte[0] = 0x04; TX_4Byte[1] = 0x93; TX_4Byte[2] = 0x00; TX_4Byte[3] = 0x00;
  SPI_WriteReg(0x3E, TX_4Byte, 4); 
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_4Byte, 4); TX_2Byte[1] = 0x06;  // Checksum and Length
  SPI_WriteReg(0x60, TX_2Byte, 2);	
	delayUS(1000);
	
	// Enable protections in 'Enabled Protections A' 0x9261 = 0xBC (See TRM section 13.3.3.2)
	// Enables SCD (short-circuit), OCD1 (over-current in discharge), OCC (over-current in charge), 
	// COV (over-voltage), CUV (under-voltage)
	TX_3Byte[0] = 0x61; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0xFC;
  SPI_WriteReg(0x3E, TX_3Byte, 3); 
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  SPI_WriteReg(0x60, TX_2Byte, 2);	
	delayUS(1000);
	
	// Enable all protections in 'Enabled Protections B' 0x9262 = 0xF7 (See TRM section 13.3.3.3)
	// Enables OTF (over-temperature FET), OTINT (internal over-temperature), OTD (over-temperature in discharge), 
	// OTC (over-temperature in charge), UTINT (internal under-temperature), UTD (under-temperature in discharge), UTC (under-temperature in charge)
	TX_3Byte[0] = 0x62; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0xF7;
  SPI_WriteReg(0x3E, TX_3Byte, 3); 
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  SPI_WriteReg(0x60, TX_2Byte, 2);	
	delayUS(1000);
	
	// Set TS1 to measure Cell Temperature - 0x92FD = 0x07   (See TRM Section 13.3.2.12)
	TX_3Byte[0] = 0xFD; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x07;
  SPI_WriteReg(0x3E, TX_3Byte, 3); 
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  SPI_WriteReg(0x60, TX_2Byte, 2);	
	delayUS(1000);
	
	// Set TS3 to measure FET Temperature - 0x92FF = 0x0F   (See TRM Section 13.3.2.14)
	TX_3Byte[0] = 0xFF; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x0F;
  SPI_WriteReg(0x3E, TX_3Byte, 3); 
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  SPI_WriteReg(0x60, TX_2Byte, 2);	
	delayUS(1000);
	
	// Set DFETOFF pin to control BOTH CHG and DSG FET - 0x92FB = 0x42 (set to 0x00 to disable) 
	// See TRM section 13.3.2.10, Table 13-7
	TX_3Byte[0] = 0xFB; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x42;
  SPI_WriteReg(0x3E, TX_3Byte, 3); 
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  SPI_WriteReg(0x60, TX_2Byte, 2);	
	delayUS(1000);
	
	// Set up Alert Pin - 0x92FC = 0x2A  - See TRM Section 13.3.2.11, Table 13-8
	// This configures the Alert pin to drive high (REG1 voltage) when enabled. 
	// Other options available include active-low, drive HiZ, drive using REG18 (1.8V), weak internal pull-up and pull-down
	TX_3Byte[0] = 0xFC; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x2A;
  SPI_WriteReg(0x3E, TX_3Byte, 3); 
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  SPI_WriteReg(0x60, TX_2Byte, 2);	
	delayUS(1000);
	
	// Set up Cell Balancing Configuration - 0x9335 = 0x03   -  Automated balancing while in Relax or Charge modes
	// See TRM Section 13.3.11. Chapter 10 of TRM describes Cell Balancing in detail
	// Also see "Cell Balancing with BQ76952, BQ76942 Battery Monitors" document on ti.com
	TX_3Byte[0] = 0x35; TX_3Byte[1] = 0x93; TX_3Byte[2] = 0x03;
  SPI_WriteReg(0x3E, TX_3Byte, 3); 
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  SPI_WriteReg(0x60, TX_2Byte, 2);	
	delayUS(1000);
	
	// Set up COV (over-voltage) Threshold - 0x9278 = 0x55 (4301 mV) 
	// COV Threshold is this value multiplied by 50.6mV  See TRM section 13.6.2
	TX_3Byte[0] = 0x78; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x55;
  SPI_WriteReg(0x3E, TX_3Byte, 3); 
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  SPI_WriteReg(0x60, TX_2Byte, 2);	
	delayUS(1000);
	
	// Set up SCD Threshold - 0x9286 = 0x05 (100 mV = 100A across 1mOhm sense resistor)  
	// See TRM section 13.6.7    0x05=100mV
	TX_3Byte[0] = 0x86; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x05;
  SPI_WriteReg(0x3E, TX_3Byte, 3); 
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  SPI_WriteReg(0x60, TX_2Byte, 2);	
	delayUS(1000);	
	
	// Set up SCD Delay - 0x9287 = 0x03 (30 us)    See TRM section 13.6.7
	// Units of 15us
	TX_3Byte[0] = 0x87; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x03;
  SPI_WriteReg(0x3E, TX_3Byte, 3); 
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  SPI_WriteReg(0x60, TX_2Byte, 2);	
	delayUS(1000);	
	
	// Set up SCDL Latch Limit to 1 to set SCD recovery only with load removal 0x9295 = 0x01  
	// If this is not set, then SCD will recover based on time (SCD Recovery Time parameter).
	// See TRM section 13.6.11.1
	TX_3Byte[0] = 0x95; TX_3Byte[1] = 0x92; TX_3Byte[2] = 0x01;
  SPI_WriteReg(0x3E, TX_3Byte, 3); 
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  SPI_WriteReg(0x60, TX_2Byte, 2);	
	delayUS(1000);	
	

	// Exit CONFIGUPDATE mode  - Subcommand 0x0092
	TX_2Byte[0] = 0x92; TX_2Byte[1] = 0x00;
	SPI_WriteReg(0x3E,TX_2Byte,2);
	delayUS(1000);
}

//  ********************************* FET Control Commands  ***************************************

void AFE_FET_ENABLE() {
	// Toggles the FET_EN bit in the Manufacturing Status register. So this command can be used to enable or disable the FETs. 
	TX_2Byte[0] = 0x22; TX_2Byte[1] = 0x00;
	SPI_WriteReg(0x3E,TX_2Byte,2);
}

void AFE_FET_Control(uint8_t FET_states) {  // Bit3 = PCHG_OFF, Bit 2 = CHG_OFF, Bit1 = PDSG_OFF, Bit 0 = DSG_OFF
	TX_3Byte[0] = 0x97; TX_3Byte[1] = 0x00; TX_3Byte[2] = FET_states;
	SPI_WriteReg(0x3E,TX_3Byte,3);
	delayUS(1000);
	TX_2Byte[0] = Checksum(TX_3Byte, 3); TX_2Byte[1] = 0x05;
  SPI_WriteReg(0x60, TX_2Byte, 2);		
}

void DSG_PDSG_OFF() {  
	// Disable discharge (and pre-discharge) FETs  
	// Subcommand 0x0093  See TRM Table 5-8  (DSG_PDSG_OFF())
	TX_2Byte[0] = 0x93; TX_2Byte[1] = 0x00; 
	SPI_WriteReg(0x3E,TX_2Byte,2);
}

void CHG_PCHG_OFF() {  
	// Disable charge (and pre-charge) FETs  
	// Subcommand 0x0094  See TRM Table 5-8  (CHG_PCHG_OFF())
	TX_2Byte[0] = 0x94; TX_2Byte[1] = 0x00; 
	SPI_WriteReg(0x3E,TX_2Byte,2);
}

void AFE_ALL_FETS_OFF() {
	// Disable all FETs with command 0x0095  See TRM Table 5-8
	TX_2Byte[0] = 0x95; TX_2Byte[1] = 0x00;
	SPI_WriteReg(0x3E,TX_2Byte,2);
}

void AFE_ALL_FETS_ON() {
	// All all FETs to be enabled with command 0x0096  See TRM Table 5-8
	TX_2Byte[0] = 0x96; TX_2Byte[1] = 0x00;
	SPI_WriteReg(0x3E,TX_2Byte,2);
}

void AFE_BOTHOFF () {
	// Disables all FETs using the DFETOFF (BOTHOFF) pin
	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_SET);  // DFETOFF pin (BOTHOFF) set low
}

void AFE_RESET_BOTHOFF () {
	// Resets DFETOFF (BOTHOFF) pin
	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_RESET);  // DFETOFF pin (BOTHOFF) set low
}

void AFE_ReadFETStatus() { 
	// Read FET Status to see which FETs are enabled
	SPI_ReadReg(0x7F, RX_2Byte, 2);
  FET_Status = (RX_2Byte[1]*256 + RX_2Byte[0]);
	DCHG = 0x4 & RX_2Byte[0];   // discharge FET state
	CHG = 0x1 & RX_2Byte[0];   // charge FET state
	PCHG = 0x2 & RX_2Byte[0];  // pre-charge FET state
	PDSG = 0x8 & RX_2Byte[0];  // pre-discharge FET state
}



// ********************************* End of FET Control Commands *********************************


// ********************************* AFE Cell Balancing Commands   *****************************************

void CB_ACTIVE_CELLS() { 
	// Check status of which cells are balancing
	TX_2Byte[0] = 0x83; TX_2Byte[1] = 0x00;
	SPI_WriteReg(0x3E,TX_2Byte,2);
	SPI_ReadReg(0x40, RX_2Byte, 2);
  CB_ActiveCells = (RX_2Byte[1]*256 + RX_2Byte[0]);
}


// ********************************* End of AFE Cell Balancing Commands   *****************************************


// ********************************* AFE Power Commands   *****************************************
void AFE_DeepSleep() {
	// Puts the device into DEEPSLEEP mode. See TRM section 7.4
	TX_2Byte[0] = 0x0F; TX_2Byte[1] = 0x00;
	SPI_WriteReg(0x3E,TX_2Byte,2);
	SPI_WriteReg(0x3E,TX_2Byte,2);
}

void AFE_ExitDeepSleep() {
	// Exits DEEPSLEEP mode. See TRM section 7.4
	TX_2Byte[0] = 0x0E; TX_2Byte[1] = 0x00;
	SPI_WriteReg(0x3E,TX_2Byte,2);
}

void AFE_ShutdownCommand() { 
	// Puts the device into SHUTDOWN mode. See TRM section 7.5
	TX_2Byte[0] = 0x10; TX_2Byte[1] = 0x00;
	SPI_WriteReg(0x3E,TX_2Byte,2);
}

void AFE_ShutdownPin() { 
	// Puts the device into SHUTDOWN mode using the RST_SHUT pin
	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_SET);  // Sets RST_SHUT pin 
}

void AFE_ReleaseShutdownPin() { 
	// Releases the RST_SHUT pin
	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_RESET);  // Resets RST_SHUT pin 
}

void AFE_SLEEP_ENABLE() { // SLEEP_ENABLE 0x0099
	// Allows the device to enter Sleep mode if current is below Sleep Current. See TRM section 7.3
	TX_2Byte[0] = 0x99; TX_2Byte[1] = 0x00;
	SPI_WriteReg(0x3E,TX_2Byte,2);
}

void AFE_SLEEP_DISABLE() { // SLEEP_DISABLE 0x009A
	// Takes the device out of sleep mode. See TRM section 7.3
	TX_2Byte[0] = 0x9A; TX_2Byte[1] = 0x00;
	SPI_WriteReg(0x3E,TX_2Byte,2);
}

// ********************************* End of AFE Power Commands   *****************************************


// ********************************* AFE Status and Fault Commands   *****************************************

uint16_t AFE_ReadAlarmStatus() { 
	// Read this register to find out why the Alert pin was asserted. See section 6.6 of the TRM for full description.
	SPI_ReadReg(0x62, RX_2Byte, 2);
	return (RX_2Byte[1]*256 + RX_2Byte[0]);
}

void AFE_ReadSafetyStatus() { 
	// Read Safety Status A/B/C and find which bits are set
	// This shows which primary protections have been triggered
	SPI_ReadReg(0x03, RX_2Byte, 2);
	SafetyStatusA = (RX_2Byte[1]*256 + RX_2Byte[0]);
	UV_Fault = 0x4 & RX_2Byte[0];
	OV_Fault = 0x8 & RX_2Byte[0];
	SCD_Fault = 0x8 & RX_2Byte[1];
	OCD_Fault = 0x2 & RX_2Byte[1];
	SPI_ReadReg(0x05, RX_2Byte, 2);
	SafetyStatusB = (RX_2Byte[1]*256 + RX_2Byte[0]);
	SPI_ReadReg(0x07, RX_2Byte, 2);
	SafetyStatusC = (RX_2Byte[1]*256 + RX_2Byte[0]);
}

void AFE_ReadPFStatus() { 
	// Read Permanent Fail Status A/B/C and find which bits are set
	// This shows which permanent failures have been triggered
	SPI_ReadReg(0x0B, RX_2Byte, 2);
	PFStatusA = (RX_2Byte[1]*256 + RX_2Byte[0]);
	SPI_ReadReg(0x0D, RX_2Byte, 2);
	PFStatusB = (RX_2Byte[1]*256 + RX_2Byte[0]);
	SPI_ReadReg(0x0F, RX_2Byte, 2);
	PFStatusC = (RX_2Byte[1]*256 + RX_2Byte[0]);
}


void AFE_ControlStatus() { 
	// Control status register - Bit0 - LD_ON (load detected)
	// See TRM Table 6-1
	SPI_ReadReg(0x00, RX_2Byte, 2);
  LD_ON = 0x1 & RX_2Byte[0];
}

void AFE_BatteryStatus() { 
	// Battery status register - See TRM Table 6-2
	SPI_ReadReg(0x12, RX_2Byte, 2);
}

void AFE_ClearFaults() { 
	TX_2Byte[0] = 0x00; TX_2Byte[1] = 0xF8;
	SPI_WriteReg(0x62,TX_2Byte,2);
}

void AFE_PFReset() { 
	TX_2Byte[0] = 0x29; TX_2Byte[1] = 0x00;
	SPI_WriteReg(0x3E,TX_2Byte,2);
}

uint16_t AFE_DeviceID() { 
	// Read Device ID using Subcommand 0x0001
	TX_2Byte[0] = 0x01; TX_2Byte[1] = 0x00;
	SPI_WriteReg(0x3E,TX_2Byte,2);
	delayUS(500);
	SPI_ReadReg(0x40, RX_2Byte, 2);
	return (RX_2Byte[1]*256 + RX_2Byte[0]);
}
// ********************************* End of AFE Status and Fault Commands   *****************************************


// ********************************* AFE Measurement Commands   *****************************************

uint16_t AFE_ReadCellVoltage(uint8_t channel) {
	SPI_ReadReg(channel*2+0x12, RX_2Byte, 2);
	return (RX_2Byte[1]*256 + RX_2Byte[0]);     // cell voltage is reported in mV
}

uint16_t AFE_ReadStackVoltage() {
	SPI_ReadReg(0x34, RX_2Byte, 2);
	return 10 * (RX_2Byte[1]*256 + RX_2Byte[0]);  // voltage is reported in 0.01V units
}

uint16_t AFE_ReadPackVoltage() {
	SPI_ReadReg(0x36, RX_2Byte, 2);
	return 10 * (RX_2Byte[1]*256 + RX_2Byte[0]);  // voltage is reported in 0.01V units
}

uint16_t AFE_ReadLDVoltage() {
	SPI_ReadReg(0x38, RX_2Byte, 2);
	return 10 * (RX_2Byte[1]*256 + RX_2Byte[0]);  // voltage is reported in 0.01V units
}

uint16_t AFE_ReadCurrent() {
	SPI_ReadReg(0x3A, RX_2Byte, 2);
	return (RX_2Byte[1]*256 + RX_2Byte[0]);  // current is reported in mA
}



float AFE_ReadTemperature(uint8_t channel) {
	switch(channel)
	{
		case 0: 
			SPI_ReadReg(0x70, RX_2Byte, 2);  // TS1 pin
			break;
		case 1: 
			SPI_ReadReg(0x74, RX_2Byte, 2);  // TS3 pin, FET temperature
			break;
		default: break;
	}
	return (0.1 * (float)(RX_2Byte[1]*256 + RX_2Byte[0])) - 273.15;  // convert from 0.1K to Celcius
}
	

void AFE_ReadPassQ() {
	// Read Accumulated Charge and Time from DASTATUS6 (See TRM Table 4-6)
	TX_2Byte[0] = 0x76; TX_2Byte[1] = 0x00;
	SPI_WriteReg(0x3E,TX_2Byte,2);
	delayUS(1000);
	SPI_ReadReg(0x40, RX_12Byte, 12);
	AccumulatedCharge_Int = ((RX_12Byte[3]<<24) + (RX_12Byte[2]<<16) + (RX_12Byte[1]<<8) + RX_12Byte[0]);
	AccumulatedCharge_Frac = ((RX_12Byte[7]<<24) + (RX_12Byte[6]<<16) + (RX_12Byte[5]<<8) + RX_12Byte[4]);
	AccumulatedCharge_Time = ((RX_12Byte[11]<<24) + (RX_12Byte[10]<<16) + (RX_12Byte[9]<<8) + RX_12Byte[8]);
}

void AFE_ClearPassQ() {
	// Clear Accumulated Charge and Time, command 0x0082
	TX_2Byte[0] = 0x82; TX_2Byte[1] = 0x00;
	SPI_WriteReg(0x3E,TX_2Byte,2);
}

// ********************************* End of AFE Measurement Commands   *****************************************



/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
  * @brief  The application entry point.
  * @retval int
  */
int main(void)
{
  /* USER CODE BEGIN 1 */
  char uart_buf[50];
	int uart_buf_len;
	// uint16_t timer_val;
	
  /* USER CODE END 1 */

  /* MCU Configuration--------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();

  /* USER CODE BEGIN Init */

  /* USER CODE END Init */

  /* Configure the system clock */
  SystemClock_Config();

  /* USER CODE BEGIN SysInit */

  /* USER CODE END SysInit */

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_SPI1_Init();
  MX_USART2_UART_Init();
  MX_TIM1_Init();
	
  /* USER CODE BEGIN 2 */
	
	// Start timer
	HAL_TIM_Base_Start(&htim1);
	HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_SET);  // SPI_CS pin set high
	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_RESET);  // RST_SHUT pin set low
	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_RESET);  // DFETOFF pin (BOTHOFF) set low
  delayUS(10000);


	AFE_Reset();
	delayUS(60000);
	AFE_Init();
	delayUS(10000);
	AFE_FET_ENABLE();
	delayUS(60000); delayUS(60000); delayUS(60000); delayUS(60000);  //wait to start measurements after FETs close
	CellVoltage[1] = AFE_ReadCellVoltage(1);
	CellVoltage[5] = AFE_ReadCellVoltage(5);
	CellVoltage[10] = AFE_ReadCellVoltage(10);
	Stack_Voltage = AFE_ReadStackVoltage();
	PACK_Voltage = AFE_ReadPackVoltage();
	LD_Voltage = AFE_ReadLDVoltage();
	PACK_Current = AFE_ReadCurrent();
	Temperature[0] = AFE_ReadTemperature(0);
	FET_Temperature = AFE_ReadTemperature(1);


	
  /* USER CODE END 2 */

  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
	
  while (1)
  {
		
    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */
	  /* delayUS(50000); */
		CellVoltage[1] = AFE_ReadCellVoltage(1);
		
		/* Debug code - prints the Cell1 Voltage to a terminal window
		uart_buf_len = sprintf(uart_buf, "%u mV\r\n", CellVoltage[1]);
		HAL_UART_Transmit(&huart2, (uint8_t *)uart_buf, uart_buf_len, 100); */
		
		CellVoltage[2] = AFE_ReadCellVoltage(2);
		CellVoltage[3] = AFE_ReadCellVoltage(3);
		CellVoltage[4] = AFE_ReadCellVoltage(4);
		CellVoltage[5] = AFE_ReadCellVoltage(5);
		CellVoltage[6] = AFE_ReadCellVoltage(6);
		CellVoltage[7] = AFE_ReadCellVoltage(7);
		CellVoltage[8] = AFE_ReadCellVoltage(8);		
		CellVoltage[9] = AFE_ReadCellVoltage(9);
		CellVoltage[10] = AFE_ReadCellVoltage(10);
		Stack_Voltage = AFE_ReadStackVoltage();
		PACK_Voltage = AFE_ReadPackVoltage();
		LD_Voltage = AFE_ReadLDVoltage();
		PACK_Current = AFE_ReadCurrent();
		Temperature[0] = AFE_ReadTemperature(0);
		FET_Temperature = AFE_ReadTemperature(1);
		
		AlarmBits = AFE_ReadAlarmStatus(); 
		if (AlarmBits & 0xC000)
			AFE_ReadSafetyStatus();
			AFE_ReadPFStatus();
			AFE_ClearFaults();
			AFE_PFReset();
  }
  /* USER CODE END 3 */
}

/**
  * @brief System Clock Configuration
  * @retval None
  */
void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

  /** Initializes the RCC Oscillators according to the specified parameters
  * in the RCC_OscInitTypeDef structure.
  */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
  RCC_OscInitStruct.HSEState = RCC_HSE_ON;
  RCC_OscInitStruct.HSEPredivValue = RCC_HSE_PREDIV_DIV1;
  RCC_OscInitStruct.HSIState = RCC_HSI_ON;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
  RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL8;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }
  /** Initializes the CPU, AHB and APB buses clocks
  */
  RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
                              |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
  {
    Error_Handler();
  }
}

/**
  * @brief SPI1 Initialization Function
  * @param None
  * @retval None
  */
static void MX_SPI1_Init(void)
{

  /* USER CODE BEGIN SPI1_Init 0 */

  /* USER CODE END SPI1_Init 0 */

  /* USER CODE BEGIN SPI1_Init 1 */

  /* USER CODE END SPI1_Init 1 */
  /* SPI1 parameter configuration*/
  hspi1.Instance = SPI1;
  hspi1.Init.Mode = SPI_MODE_MASTER;
  hspi1.Init.Direction = SPI_DIRECTION_2LINES;
  hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
  hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
  hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
  hspi1.Init.NSS = SPI_NSS_SOFT;
  hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_64;
  hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
  hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
  hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_ENABLE;
  hspi1.Init.CRCPolynomial = 7;
  if (HAL_SPI_Init(&hspi1) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN SPI1_Init 2 */

  /* USER CODE END SPI1_Init 2 */

}

/**
  * @brief TIM1 Initialization Function
  * @param None
  * @retval None
  */
static void MX_TIM1_Init(void)
{

  /* USER CODE BEGIN TIM1_Init 0 */

  /* USER CODE END TIM1_Init 0 */

  TIM_ClockConfigTypeDef sClockSourceConfig = {0};
  TIM_MasterConfigTypeDef sMasterConfig = {0};

  /* USER CODE BEGIN TIM1_Init 1 */

  /* USER CODE END TIM1_Init 1 */
  htim1.Instance = TIM1;
  htim1.Init.Prescaler = 63;
  htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
  htim1.Init.Period = 65535;
  htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
  htim1.Init.RepetitionCounter = 0;
  htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
  if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
  {
    Error_Handler();
  }
  sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
  if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
  {
    Error_Handler();
  }
  sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
  sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
  if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN TIM1_Init 2 */

  /* USER CODE END TIM1_Init 2 */

}

/**
  * @brief USART2 Initialization Function
  * @param None
  * @retval None
  */
static void MX_USART2_UART_Init(void)
{

  /* USER CODE BEGIN USART2_Init 0 */

  /* USER CODE END USART2_Init 0 */

  /* USER CODE BEGIN USART2_Init 1 */

  /* USER CODE END USART2_Init 1 */
  huart2.Instance = USART2;
  huart2.Init.BaudRate = 115200;
  huart2.Init.WordLength = UART_WORDLENGTH_8B;
  huart2.Init.StopBits = UART_STOPBITS_1;
  huart2.Init.Parity = UART_PARITY_NONE;
  huart2.Init.Mode = UART_MODE_TX_RX;
  huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
  huart2.Init.OverSampling = UART_OVERSAMPLING_16;
  if (HAL_UART_Init(&huart2) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN USART2_Init 2 */

  /* USER CODE END USART2_Init 2 */

}

/**
  * @brief GPIO Initialization Function
  * @param None
  * @retval None
  */
static void MX_GPIO_Init(void)
{
  GPIO_InitTypeDef GPIO_InitStruct = {0};

  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOC_CLK_ENABLE();
  __HAL_RCC_GPIOD_CLK_ENABLE();
  __HAL_RCC_GPIOA_CLK_ENABLE();
  __HAL_RCC_GPIOB_CLK_ENABLE();

  /*Configure GPIO pin Output Level */
  HAL_GPIO_WritePin(GPIOA, LD2_Pin|GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10, GPIO_PIN_RESET);

  /*Configure GPIO pin Output Level */
  HAL_GPIO_WritePin(GPIOB, GPIO_PIN_6, GPIO_PIN_RESET);

  /*Configure GPIO pin : B1_Pin */
  GPIO_InitStruct.Pin = B1_Pin;
  GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct);

  /*Configure GPIO pins : LD2_Pin PA8 PA9 PA10 */
  GPIO_InitStruct.Pin = LD2_Pin|GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

  /*Configure GPIO pin : PB6 */
  GPIO_InitStruct.Pin = GPIO_PIN_6;
  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
  GPIO_InitStruct.Pull = GPIO_NOPULL;
  GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
  HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

  /* EXTI interrupt init*/
  HAL_NVIC_SetPriority(EXTI15_10_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(EXTI15_10_IRQn);

}

/* USER CODE BEGIN 4 */
void HAL_GPIO_EXTI_Callback ( uint16_t GPIO_Pin )
{
	if ( GPIO_Pin == GPIO_PIN_10 ) {
		AlarmBits = AFE_ReadAlarmStatus();
		AFE_ReadSafetyStatus();
		AFE_ReadPFStatus();
		HAL_GPIO_TogglePin (GPIOA, GPIO_PIN_5 );
	}
	else {
		__NOP ();
	}
}
/* USER CODE END 4 */

/**
  * @brief  This function is executed in case of error occurrence.
  * @retval None
  */
void Error_Handler(void)
{
  /* USER CODE BEGIN Error_Handler_Debug */
  /* User can add his own implementation to report the HAL error return state */

  /* USER CODE END Error_Handler_Debug */
}

#ifdef  USE_FULL_ASSERT
/**
  * @brief  Reports the name of the source file and the source line number
  *         where the assert_param error has occurred.
  * @param  file: pointer to the source file name
  * @param  line: assert_param error line source number
  * @retval None
  */
void assert_failed(uint8_t *file, uint32_t line)
{
  /* USER CODE BEGIN 6 */
  /* User can add his own implementation to report the file name and line number,
     tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
  /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/