Resistance temperature compensation optimizer, rev=3.5		
		
Optimized Impedance Track parameters:		
		
Qmax, mAh : 8088		
		
Ra table normalized to 25C, uncompressed, unscaled		
		
DOD, %	Ra, mOhm	
		
0	37	
11.11	37	
22.22	37	
33.33	17	
44.44	31	
55.56	41	
66.67	30	
77.78	24	
80.95	24	
84.13	26	
87.3	27	
90.48	28	
93.65	44	
96.83	87	
100	152	
		
Ra0_ch, mOhm : 235	This firmware is not explicitly supporting Ra0_ch, FCC drop could occur at low temperatures if used	
		
Thermal parameters:		
		
Temp a	1000	
Temp k	0.4	
Res Relax Time	4	
		
Optimized resistance temperature compensation parameters saved in chemdat12		
		
		
Due to GG file format issues, GG values have not been updated		
		
		
Warning: Automatic firmware properties detection failed. Rb_select defaults to 2. Please make sure that chem ID loaded in the GG file is the same as ID specified in the config.txt		
Warning: Automatic firmware properties detection failed. basescale defaults to 1. Please make sure that chem ID loaded in the GG file is the same as ID specified in the config.txt		
Error: negative room temperature resistance observed	 R=-0.0189703994155302 usually caused by wrong chem ID selection