Resistance temperature compensation optimizer, rev=3.57		
		
Optimized Impedance Track parameters:		
		
Qmax, mAh : 3660		
		
Ra table normalized to 25C, uncompressed, unscaled		
		
DOD, %	Ra, mOhm	
		
0	100	
11.11	100	
22.22	237	
33.33	191	
44.44	124	
55.56	119	
66.67	92	
77.78	11	
80.95	10	
84.13	70	
87.3	111	
90.48	160	
93.65	292	
96.83	550	
100	764	
		
Ra0_ch, mOhm : 75	This firmware is not explicitly supporting Ra0_ch, FCC drop could occur at low temperatures if used	
		
Thermal parameters:		
		
T Time Constant type undefined	509	
T Rise type undefined	73	
Res Relax Time	363	
		
Optimized resistance temperature compensation parameters saved in *.chem file		
		
		
Due to GG file format issues, GG values have not been updated		
		
		
Error: Terminate Voltage or Term Voltage not found in GG file. Term k didiver uncertain. Make sure that gg.csv file is not corrupted		
Warning: GG file could not be processed. Please check that it is unmodified	 as exported by EV Software or BM Studio	
Warning: Automatic firmware properties detection failed. Rb_select defaults to 2. Please make sure that chem ID loaded in the GG file is the same as ID specified in the config.txt		
Warning: Automatic firmware properties detection failed. basescale defaults to 1. Please make sure that chem ID loaded in the GG file is the same as ID specified in the config.txt		
Error: negative room temperature resistance observed	 R=-0.000895545062019996 usually caused by wrong chem ID selection