TimeTypeSeverityExtraMessage
11:00:09.065CUSTOMERGENERALnoneFactory version: TI Digital Power Production Tool Version: 2.0.13.0
11:00:09.068INTERNALGENERALnoneRunning Script: UCD3138UpdateFactoryScript.xml @ C:\Users\Jack Tan\Desktop\1005 debug\ucd3138llc-200319\UCD3138\UCD3138UpdateFactoryScript.xml
11:00:09.068INTERNALGENERALnoneOperator: 1
11:00:09.074CUSTOMERGENERALnoneWrote: SAA Settings: Speed400KHz, Serial, Alert: 2.2 k?; Clock: 2.2 k?; Data: 2.2 k?
11:00:09.110INTERNALGENERALnone************************************************************
11:00:09.111INTERNALGENERALnoneFactory Script START attempt: 0/0
11:00:09.112INTERNALGENERALnone************************************************************
11:00:09.116INTERNALGENERALnoneUCD3100ISO1@71(1) START attempt: 0/0
11:00:09.116INTERNALGENERALnone************************************************************
11:00:09.121INTERNALGENERALnoneFactory Script INITIALIZING attempt: 0/0
11:00:09.124INTERNALGENERALnoneFactory Script INITIALIZED attempt: 0/0
11:00:09.126INTERNALGENERALnone************************************************************
11:00:09.128INTERNALGENERALnoneFactory Script Device VALIDATING attempt: 0/0
11:00:09.129PMBUSGENERALnoneMisc: Starting device discovery
11:00:09.129PMBUSGENERALnoneMisc: Starting device scan on SAA #1
11:00:09.133PMBUSGENERALnoneDiscovery @ 71d: DEVICE_ID [MFR 45,0xFD]: read UCD3100ISO1|0.0.11.0106|200319 [0x5543443331303049534F317C302E302E31312E303130367C32303033313900]
11:00:09.144PMBUSGENERALnoneDiscovery @ 71d: SETUP_ID [MFR 23,0xE7]: read VERSION1|LLC001 [0x56455253494F4E317C4C4C4330303100]
11:00:09.150PMBUSGENERALnoneDC-DC LLC @ 71d: CMDS_DCDC_PAGED [MFR 20,0xE4]: read No commands write protected [0x0000000000000000000000000000000000000000000000000000000000000000]
11:00:09.152PMBUSGENERALnoneDC-DC LLC @ 71d: CMDS_DCDC_NONPAGED [MFR 21,0xE5]: read Write protected: 0x01, 0x02, 0x03, 0x11, 0x12, 0x19, 0x20, 0x21, 0x23, 0x25, 0x26, 0x27, 0x35, 0x36, 0x38, 0x39, 0x40, 0x42, 0x43, 0x44, 0x45, 0x46, 0x47, 0x4A, 0x4F, 0x51, 0x55, 0x57, 0x58, 0x59, 0x5B, 0x5D, 0x5E, 0x5F, 0x60, 0x61, 0x78, 0x79, 0x7A, 0x7B, 0x7C, 0x7D, 0x7E, 0x88, 0x8B, 0x8C, 0x8D, 0x8E, 0x95, 0x96, 0x98, 0x99, 0x9A, 0x9B, 0x9C, 0x9D, 0x9E, 0xAD, 0xAE, 0xD1, 0xD2, 0xD3, 0xD5, 0xD9, 0xDA, 0xE2, 0xE3, 0xE4, 0xE5, 0xE7, 0xEA, 0xF0, 0xF2, 0xF4, 0xF7, 0xFA, 0xFB, 0xFC, 0xFD [0x70006040D70006C0BF2145D7C00000FE009E06FE00060000000074603D20A93C]
11:00:09.156PMBUSGENERALnoneDC-DC LLC @ 71d: DEVICE_ID [MFR 45,0xFD]: read UCD3100ISO1|0.0.11.0106|200319 [0x5543443331303049534F317C302E302E31312E303130367C32303033313900]
11:00:09.164PMBUSGENERALnoneDC-DC LLC @ 71d: PMBUS_REVISION [0x98]: read 0.0,1.2 - Part I: 0.0, Part II: 1.2 [0x42]
11:00:09.166PMBUSGENERALnoneDC-DC LLC @ 71d: PARM_INFO [MFR 18,0xE2]: wrote Base: 1 (HardwarePeripherals), Offset: 0x07D0, Count: 1, Size: 4 [0x01D0070104] to RAM
11:00:09.168PMBUSGENERALnoneDC-DC LLC @ 71d: PARM_VALUE [MFR 19,0xE3]: read 0x0103FFFF
11:00:09.169INTERNALGENERALnoneFactory Script Device VALIDATED PASS
11:00:09.170INTERNALGENERALnone************************************************************
11:00:09.189INTERNALGENERALnoneUCD3100ISO1@71(1).Update Firmware on Device(1) START attempt: 0/0
11:00:09.194INTERNALGENERALnone************************************************************
11:00:09.205INTERNALGENERALnoneUCD3100ISO1@71(1).Update Firmware on Device(1).Firmware_Update(1) START attempt: 0/0
11:00:09.210CUSTOMERGENERALSummaryPMBUS: Firmware_Update Description: This task downloads the specified firmware to the device(non-volatile memory). You can avoid downloading firmware already loaded onto the device by setting the parameter Condition_For_Flash to DeviceVersionIsLower or DeviceVersionDiffers and specifying the version of the x0 file in the Version_Number parameter. If you always want to download no matter what is on the device, then set Condition_For_Flash to "AlwaysFlash" . Refer to the User Guide - Script Writer in the help menu for more complex examples of downloading firmware. Technical Description: The "Condition_For_Flash" parameter is a great way to speed up your script if you need to re-run. This task should be placed in an Activity of type Normal. Inputs(22): (FileLocation=C:\Users\Jack Tan\Desktop\1005 debug\ucd3138-test\UCD3138_LLC_HB.x0) (Condition_For_Flash=DeviceVersionIsLower) (Version_Number=N/A) (Verify_Device_Has_Been_Trimmed=True) (Data_Flash_Option=Download) (Restore_Current_Config=False) (Display_PFLASH_Checkum_After_Download=False) (Boot_Needed=False) (Boot_Size=-1) (Multi_Flash=False) (PFlash_Block=Block0) (PFlash_Checksum_From=EntireBlockIncludingBoot) (Checksum_Mode=CalculateAndWrite) (Validate_PFlash_Checksum_With_User_Checksum=False) (User_PFlash_Checksum=0) (Validate_2K_BFlash_Checksum_With_User_Checksum=False) (Validate_Above_2K_BFlash_Checksum_With_User_Checksum=False) (User_2K_BFlash_Checksum=0) (User_Above_2K_BFlash_Checksum=0) (Data_Flash_Option_Begin_Page=0) (Data_Flash_Option_Final_Page=63) (Split_Boot=False) Retry on failure: 0 Namespace: TIDP.Factory.TaskLibrary Class: Manufacturing Assembly: TIDP.Factory.TaskLibrary Version: 1.0.10 **Dependencies**:
11:00:09.218CUSTOMERGENERALSummaryTIDP.Factory.TaskLibrary, Version=3.0.8.0, Culture=neutral, PublicKeyToken=null
11:00:09.229CUSTOMERGENERALnoneFirmware currently on device: 0.0.11.106
11:00:09.230CUSTOMERERRORSummary?????????????
11:00:09.364CUSTOMER_LOGONLYERRORSummary ????????????? ? System.Version.VersionResult.SetFailure(ParseFailureKind failure, String argument) ? System.Version.TryParseVersion(String version, VersionResult& result) ? System.Version.Parse(String input) ? System.Version..ctor(String version) ? TIDP.Factory.TaskLibrary.UCD9XXX.UCD9XXX_Firmware_Update(PMBusDevice device, String fileName, String version, ConditionForFlash condition_for_flash, Boolean Verify_Device_Has_Been_Trimmed, DataFlashOptions Data_Flash_Option, Boolean restore_current_config, Boolean display_pflash_checkum_after_download, Boolean is_boot_needed, Int32 boot_size, Boolean is_multi_flash, ProgramFlashBlockSelection pflash_block, ProgramFlashChecksumCalculation pflash_checksum_from, ProgramChecksumMode pflash_checksum_mode, Boolean Validate_PFlash_Checksum_With_User_Checksum, UInt64 User_Pflash_Checksum, Boolean Validate_2K_BFlash_Checksum_With_User_Checksum, UInt64 User_2K_BFlash_Checksum, Boolean Validate_Above_2K_BFlash_Checksum_With_User_Checksum, UInt64 User_Above_2K_BFlash_Checksum, UInt32 Data_Flash_Start_Page, UInt32 Data_Flash_Final_Page, Boolean is_split_boot) ?? C:\Workspaces\IsolatedGUI-Branch-Git\Libraries\TIDP\TIDP.Factory.TaskLibrary\UCD9XXX.cs:?? 1729 ? TIDP.Factory.TaskLibrary.Manufacturing.Firmware_Update(String FileLocation, ConditionForFlash Condition_For_Flash, String Version_Number, Boolean Verify_Device_Has_Been_Trimmed, DataFlashOptions Data_Flash_Option, Boolean Restore_Current_Config, Boolean Display_PFLASH_Checkum_After_Download, Boolean Boot_Needed, Int32 Boot_Size, Boolean Multi_Flash, ProgramFlashBlockSelection PFlash_Block, ProgramFlashChecksumCalculation PFlash_Checksum_From, ProgramChecksumMode Checksum_Mode, Boolean Validate_PFlash_Checksum_With_User_Checksum, UInt64 User_PFlash_Checksum, Boolean Validate_2K_BFlash_Checksum_With_User_Checksum, Boolean Validate_Above_2K_BFlash_Checksum_With_User_Checksum, UInt64 User_2K_BFlash_Checksum, UInt64 User_Above_2K_BFlash_Checksum, UInt32 Data_Flash_Option_Begin_Page, UInt32 Data_Flash_Option_Final_Page, Boolean Split_Boot) ?? C:\Workspaces\IsolatedGUI-Branch-Git\Libraries\TIDP\TIDP.Factory.TaskLibrary\Manufacturing.cs:?? 1010
11:00:09.369CUSTOMERGENERALnone[message] Title:Failure occured... - Prompt: ?????????????
11:00:11.148INTERNALGENERALnoneUCD3100ISO1@71(1).Update Firmware on Device(1).Firmware_Update(1) END attempt: 0/0 (19.9472ms) FAIL
11:00:11.149INTERNALGENERALnoneUCD3100ISO1@71(1).Update Firmware on Device(1) END attempt: 0/0 (19.9472ms) FAIL
11:00:11.153INTERNALGENERALnoneUCD3100ISO1@71(1) END attempt: 0/0 (59.841ms) FAIL
11:00:11.159INTERNALGENERALnoneFactory Script END attempt: 0/0 (59.841ms) FAIL