Resistance temperature compensation optimizer, rev=3.48		
		
Optimized Impedance Track parameters:		
		
Qmax, mAh : 6718		
		
Ra table normalized to 25C, uncompressed, unscaled		
		
DOD, %	Ra, mOhm	
		
0	7	
11.11	79	
22.22	88	
33.33	94	
44.44	81	
55.56	87	
66.67	99	
77.78	102	
80.95	106	
84.13	103	
87.3	167	
90.48	305	
93.65	386	
96.83	421	
100	623	
		
Ra0_ch, mOhm : 2784	This firmware is not explicitly supporting Ra0_ch, FCC drop could occur at low temperatures if used	
		
Thermal parameters:		
		
T Time Constant	1996	
T Rise	38.41	
		
Optimized resistance temperature compensation parameters saved in chemdat12		
		
		
Due to GG file format issues, GG values have not been updated		
		
		
Warning: Automatic firmware properties detection failed. Rb_select defaults to 2. Please make sure that chem ID loaded in the GG file is the same as ID specified in the config.txt		
Warning: Automatic firmware properties detection failed. basescale defaults to 1. Please make sure that chem ID loaded in the GG file is the same as ID specified in the config.txt