/*******************************************************************************
  MPLAB Harmony Application Header File

  Company:
    Microchip Technology Inc.

  File Name:
    app_i2c.h

  Summary:
    This header file provides prototypes and definitions for the application.

  Description:
    This header file provides function prototypes and data type definitions for
    the application.  Some of these are required by the system (such as the
    "APP_I2C_Initialize" and "APP_I2C_Tasks" prototypes) and some of them are only used
    internally by the application (such as the "APP_I2C_STATES" definition).  Both
    are defined here for convenience.
*******************************************************************************/

#ifndef _APP_I2C_H
#define _APP_I2C_H

// *****************************************************************************
// *****************************************************************************
// Section: Included Files
// *****************************************************************************
// *****************************************************************************

#include "app.h"
//#include "driver/i2c/drv_i2c.h"

// DOM-IGNORE-BEGIN
#ifdef __cplusplus  // Provide C++ Compatibility

extern "C" {

#endif
// DOM-IGNORE-END
    
    
    
unsigned char APP_AT24MAC_DEVICE_ADDR  =    0x18;
#define APP_AT24MAC_MEMORY_ADDR             0x00
#define APP_AT24MAC_MEMORY_ADDR1            0x00
#define APP_TRANSMIT_DATA_LENGTH    3
unsigned char APP_ACK_DATA_LENGTH      =    1;
#define APP_RECEIVE_DUMMY_WRITE_LENGTH      2
#define APP_RECEIVE_DATA_LENGTH             4

static uint8_t testTxData[APP_TRANSMIT_DATA_LENGTH];
static uint8_t  testRxData[APP_RECEIVE_DATA_LENGTH];

typedef enum
{
    APP_STATE_EEPROM_STATUS_VERIFY,
    APP_STATE_EEPROM_WRITE,
    APP_STATE_EEPROM_WAIT_WRITE_COMPLETE,
    APP_STATE_EEPROM_CHECK_INTERNAL_WRITE_STATUS,
    APP_STATE_EEPROM_READ,
    APP_STATE_EEPROM_WAIT_READ_COMPLETE,
    APP_STATE_VERIFY,
    APP_STATE_IDLE,
    APP_STATE_XFER_SUCCESSFUL,
    APP_STATE_XFER_ERROR

} APP_STATES;

typedef enum
{
    APP_TRANSFER_STATUS_IN_PROGRESS,
    APP_TRANSFER_STATUS_SUCCESS,
    APP_TRANSFER_STATUS_ERROR,
    APP_TRANSFER_STATUS_IDLE,

} APP_TRANSFER_STATUS;

// *****************************************************************************
/* Application Data

  Summary:
    Holds application data

  Description:
    This structure holds the application's data.

  Remarks:
    Application strings and buffers are be defined outside this structure.
 */

// *****************************************************************************
// *****************************************************************************
// Section: I2C Applications and Callback Routines
// *****************************************************************************
// *****************************************************************************

void APP_I2C_Initialize( void );
void APP_I2C_Tasks( void );

// *****************************************************************************
// *****************************************************************************
// Section: Applications for BQ State Machine Functions
// *****************************************************************************
// *****************************************************************************

int I2CSendByte(unsigned char I2CSlaveAddress, unsigned char data);
int I2CSendBytes(unsigned char I2CSlaveAddress, unsigned char *DataBuffer, unsigned int ByteCount, unsigned int *SentByte);
int I2CWriteRegisterByte(unsigned char I2CSlaveAddress, unsigned char Register, unsigned char Data);
int I2CWriteRegisterByteWithCRC(unsigned char I2CSlaveAddress, unsigned char Register, unsigned char Data);
int I2CWriteRegisterWordWithCRC(unsigned char I2CSlaveAddress, unsigned char Register, unsigned int Data);
int I2CWriteBlockWithCRC(unsigned char I2CSlaveAddress, unsigned char StartAddress, unsigned char *Buffer, unsigned char Length);
int I2CWriteRegisterWord(unsigned char I2CSlaveAddress, unsigned char Register, unsigned int Data);
int I2CReadBytes(unsigned char I2CSlaveAddress, unsigned char *DataBuffer, unsigned int ExpectedByteNumber, unsigned int *NumberOfReceivedBytes);
int I2CReadRegisterByte(unsigned char I2CSlaveAddress, unsigned char Register, unsigned char *Data);
int I2CReadBlock(unsigned char I2CSlaveAddress, unsigned char StartRegisterAddress, unsigned char *Buffer, unsigned int BlockSize, unsigned int *NumberOfBytes);
unsigned char CRC8(unsigned char *ptr, unsigned char len,unsigned char key);
int I2CReadRegisterByteWithCRC(unsigned char I2CSlaveAddress, unsigned char Register, unsigned char *Data);
int I2CReadRegisterWordWithCRC(unsigned char I2CSlaveAddress, unsigned char Register, unsigned int *Data);
int I2CReadBlockWithCRC(unsigned char I2CSlaveAddress, unsigned char Register, unsigned char *Buffer, unsigned char Length);
int GetADCGainOffset();
int ConfigureBqMaximo();
int InitialisebqMaximo();
int UpdateVoltageFromBqMaximo();
int Read_BQ(void);

#endif /* _APP_H */

//DOM-IGNORE-BEGIN
#ifdef __cplusplus
}
#endif

//DOM-IGNORE-END
/*******************************************************************************
 End of File
 */